FPGA
  • Technologies
  • More
FPGA
Blog Go Go Speedtest®︎! Testing WiFi Internet Connection on Ultra96-V2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: narrucmot
  • Date Created: 11 Mar 2021 6:59 PM Date Created
  • Views 2266 views
  • Likes 9 likes
  • Comments 2 comments
  • ultra96-v2
  • wifi
  • internet
  • ultrazed
  • microzed
  • ethernet
  • speedtest
  • aarch64
  • petalinux
  • iperf3
  • ookla
  • picozed
  • designed by avnet
  • mbps
  • arm
  • throughput
  • linux
  • minized
Related
Recommended

Go Go Speedtest®︎! Testing WiFi Internet Connection on Ultra96-V2

narrucmot
narrucmot
11 Mar 2021

We've talked in this blog space and elsewhere about testing WiFi performance for the Ultra96-V2Ultra96-V2 board on a LAN using iperf3.  It is a very handy and useful test, but it only tests local (WLAN) throughput.  What about if you are developing an IoT product and your Ultra96-V2 needs to communicate with other devices or cloud services over the internet?  How do you test WiFi performance over the internet to the Ultra96-V2 board if you need to rely on command line access (no mouse, keyboard, or monitor connected)?  Sure, iperf3 can also be used to test WiFi performance over the internet via the command line, but public iperf3 servers are often geographically very far away and also not very reliable.

 

Ookla, the company behind the popular SpeedtestRegistered website (https://www.speedtest.net/), has free software applications to test the internet connection of anything from PCs to embedded Linux devices.  We can use this software application to examine the speed of the internet connection to the Ultra96-V2 board:

https://www.speedtest.net/apps/cli

image

 

Open a serial console or ssh connection command window to your Ultra96-V2 board.  Make a new folder to download the Speedtest application in:

# mkdir -p ~/speedtest

# cd ~/speedtest

 

Open a web browser on the same PC as the Ultra96-V2 command window and navigate to the Speedtest application webpage.  Select "Download for Linux" to reveal the Linux application options for all the supported CPU architectures.  The Ultra96-V2 has a Xilinx Zynq UltraScale+Registered MPSoC device with a 64-bit quad core Arm A53 APU, so download the application for the Arm aarch64 architecture.  Reveal the URL for the file download by hovering over the "aarch64" hyperlink and copy it to the clipboard.  Use the Linux curl command and paste the download link into the Linux command line in the Ultra96-V2 command window to download the file as follows (the exact file path and name may be different):

# curl -JLO https://bintray.com/ookla/download/download_file?file_path=ookla-speedtest-1.0.0-aarch64-linux.tgz

 

Extract the downloaded tarball (the exact file name may be different):

# tar xzvf ookla-speedtest-1.0.0-aarch64-linux.tgz

 

Run the Speedtest application:

$ ./speedtest

 

Accept the EULA and examine the results (my internet connection is capped at ~10Mbps upload, otherwise these results might have shown even higher Mbps throughput):

image

 

The application also has several command line options one can use to specify what server to connect to for the test, what device interface to bind to, and many others:

image

 

This Speedtest application can also be downloaded and run on the Xilinx Zynq-based Avnet MiniZed (SBC), MicroZed (SOM), or PicoZed (SOM) using the Speedtest application for arm CPUs.  The UltraZed SOMs will use the same aarch64 application as the Ultra96-V2.

 

What results will you achieve when you run Speedtest on your SOM or SBC?  Are they similar results to running an iperf3 test on your WLAN?  Leave your results in the comments below.

 

--Tom

  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 5 years ago +1
    Very cool Tom. I just got the Ultra96-V2 that I am testing up and running and recently connected to it's web server. I'll have to give this a test to see how it performs in my environment.
  • redcharly
    redcharly over 5 years ago +1
    Very interesting work!! Another application uing Ultra96-V2 thanks carlo
  • redcharly
    redcharly over 5 years ago

    Very interesting work!!

    Another application uing Ultra96-V2

     

    thanks

     

    carlo

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 5 years ago

    Very cool Tom.

     

    I just got the Ultra96-V2 that I am testing up and running and recently connected to it's web server.  I'll have to give this a test to see how it performs in my environment.