FPGA
  • Technologies
  • More
FPGA
Blog Creating a Custom Kria App - Part 7
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: albertabeef
  • Date Created: 12 Jan 2022 12:50 PM Date Created
  • Views 5414 views
  • Likes 3 likes
  • Comments 0 comments
  • firmware
  • kria
  • vvas
  • overlay
  • kv260
  • vitis-ai
  • app
  • dfx-mgr
  • kria app
  • smart_model_select
  • xmutil
Related
Recommended

Creating a Custom Kria App - Part 7

albertabeef
albertabeef
12 Jan 2022
Creating a Custom Kria App - Part 7

This blog is part of a series of blogs which describe the development steps for an in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-blog

This part of the tutorial describes how to perform final installation and execution of the custom Kria app.

image

 

Booting and Login

During first boot, you will be prompted for login credentials.

Start by login in as “petalinux” user, and specify “root” as password.

Next, switch to the “root” user, as shown below:

xilinx-k26-starterkit-2021_1 login: petalinux

You are required to change your password immediately (administrator enforced)

New password:

Retype new password:

xilinx-k26-starterkit-2021_1:~$ sudo su -l root

 

We trust you have received the usual lecture from the local System

Administrator. It usually boils down to these three things:

 

    #1) Respect the privacy of others.

    #2) Think before you type.

    #3) With great power comes great responsibility.

 

Password:

 

Updating the KV260 Firmware (optional)

If the SD card image does not boot, you may need to update the KV26 boot firmware (BOOT.BIN), as described in the following wiki page:

https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/1641152513/Kria+K26+SOM#Stand-alone-FW-Update-&-Recovery-Utility

image 

 

Run-time Installation

After first boot, the following components need to be installed on the system:

  • Install rpm packages 

Before installing the rpm packages, the ext4 partition needs to be extended with the following commands:

# parted /dev/mmcblk1 resizepart 2

 

Warning: Partition /dev/mmcblk1p2 is being used. Are you sure you want to continue?

Yes/No? yes

End?  [6442MB]? 100%

Information: You may need to update /etc/fstab.

 

# resize2fs /dev/mmcblk1p2

 

resize2fs 1.45.6 (20-Mar-2020)

Filesystem at /dev/mmcblk1p2 is mounted on /; on-line resizing required

old_desc_blocks = 1, new_desc_blocks = 4

The filesystem on /dev/mmcblk1p2 is now 7267455 (4k) blocks long.

 

#

 

To install the rpm packages, perform the following commands:

# cd ~/kv260-vvas-sms-2021-1/rpm

# dnf install kv260-vvas-sms-1.0-r0.0.zynqmp_generic.rpm

# dnf install kv260-vvas-sms-models-1.0-r0.0.cortexa72-cortexa53.rpm

# dnf install kv260-vvas-sms-app-1.0-r0.0.cortexa72-cortexa53.rpm

# dnf install packagegroup-kv260-vvas-sms-1.0-r0.0.noarch.rpm

 

This will take a significant amount of time, as several hundreds (900+) of dependencies will be installed.

 

 

Modify the contents of the /etc/vart.conf file:

# echo firmware: /lib/firmware/xilinx/kv260-vvas-sms/kv260-vvas-sms.xclbin > /etc/vart.conf

 

 

 

Loading the Custom App

After each boot, the KV260 Vision AI starter kit will be running the default app:

  • kv260-dp

This can be queried with the "xmutil listapps" command.

 

# xmutil listapps

   Accelerator                Base       Type   #slots   Active_slot

 

      kv260-dp            kv260-dp   XRT_FLAT        0            0,

kv260-vvas-sms      kv260-vvas-sms   XRT_FLAT        0            -1

 

Socket 9 closed by client

 

Before we can load our custom app, we first need to unload the kv260-dp app with the "xmutil unloadapp {app}" command:

 

# xmutil unloadapp kv260-dp

 

DFX-MGRD> daemon removing accel at slot 0

DFX-MGRD> Removing accel kv260-dp from slot 0

 

Accelerator successfully removed.

 

Socket 9 closed by client

 

# xmutil listapps

   Accelerator                Base       Type   #slots   Active_slot

 

      kv260-dp            kv260-dp   XRT_FLAT        0            -1

kv260-vvas-sms      kv260-vvas-sms   XRT_FLAT        0            -1

 

Socket 9 closed by client

 

We then load the custom app with the "xmutil loadapp {app}" command:

 

# xmutil loadapp kv260-vvas-sms

DFX-MGRD> daemon loading accel kv260-vvas-sms

DFX-MGRD> Successfully loaded base design.

 

Accelerator loaded to slot 0

 

Socket 6 closed by client

 

 

# xmutil listapps

   Accelerator                Base       Type   #slots   Active_slot

 

      kv260-dp            kv260-dp   XRT_FLAT        0            -1

kv260-vvas-sms      kv260-vvas-sms   XRT_FLAT        0            0,

 

Socket 9 closed by client

 

Launching the smart_model_select example

With the kv260-vvas-sms app loaded, we can run the smart_model_select example application.

 

The application is located in the "/opt/avnet/kv260-vvas-sms/app" directory:

 

# cd /opt/avnet/kv260-vvas-sms/app

 

 

First, we need to configure our monitor for 1080P resolution:

 

# source ./setup.sh

setting mode 1920x1080-60.00Hz on connectors 43, crtc 41

testing 1920x1080@NV12 overlay plane 39

 

[1]+  Stopped(SIGTTIN)        modetest -M xlnx -s 43@41:1920x1080-60@AR24 -P 39@41:1920x1080@NV12 -w 40:alpha:0

 

 

This will display a diagonal color bar pattern on the monitor as show below:

image

With our monitor configured for 1080P resolution, we can launch the application:

 

# ./smart_model_select

############################################

################## WELCOME #################

############################################

 

DEBUG: Got the cmd: gst-launch-1.0 multifilesrc location=templates/welcome_1080.jpg ! \

        jpegparse ! jpegdec ! \

        queue ! fpsdisplaysink video-sink="kmssink driver-name=xlnx sync=false" text-overlay=false sync=false

 

Setting pipeline to PAUSED ...

Pipeline is PREROLLING ...

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

 

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

Menu displayed on the monitor shows various options available

for input source, ML model, output sink. Each option carry an

index number along side.

Select elements to be used in the pipeline in the sequence of

"input source, ML model, output sink and performance

mode flag" seperated by commas.

eg: 1,1,3,0

Above input will run "filesrc" input, "resnet50" model

"kmssink" used as output sink and performance mode disabled.

Enter 'q' to exit

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

 

This will display the following image on the monitor, which only acts as a visual reference for the choices that can be made on the command line:

image

Note that the original image was modified to reflect the two additional input sources that were added to the application:

  • USB camera
  • MIPI sensor

Hardware Setup

The examples described below were performed with the following setup:

image

I do not have the very cool stand that was provided with some of the initial KV260 units, so simply placed the KV260 against the monitor.

 

In addition to the video files, I have the following two input sources connected to the board:

  • USB camera - Logitech BRIO (with NV12 support)
  • MIPI sensor - IAS AR1335 module (http://avnet.me/ias-ar1335-datasheet)

 

Running the application with video file input

The SD card image comes with the following video files pre-installed:

videos

├── CLASSIFICATION.mp4

├── FACEDETECT.mp4

├── REFINEDET.mp4

├── SSD.mp4

├── YOLOV2.mp4

└── YOLOV3.mp4

 

 

 

In order to apply a model to the video files, use the "1, #, 3, 0" syntax, where # is a value from 1-16, representing one of the supported models.

 

For example, to apply model #6 to a video file, launch the example as follows:

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

Menu displayed on the monitor shows various options available

for input source, ML model, output sink. Each option carry an

index number along side.

Select elements to be used in the pipeline in the sequence of

"input source, ML model, output sink and performance

mode flag" seperated by commas.

eg: 1,1,3,0

Above input will run "filesrc" input, "resnet50" model

"kmssink" used as output sink and performance mode disabled.

Enter 'q' to exit

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

1,6,3,0

...

 >>>>> Enter any key to return to main menu <<<<<

 

The following animated image shows the expected output for this above example:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This launches the following GStreamer pipeline:

image

 

Running the application with USB camera input

In order to apply a model to a USB camera input, use the "3, #, 3, 0" syntax, where # is a value from 1-16, representing one of the supported models.

 

For example, to apply model #16 to the USB camera, launch the example as follows:

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

Menu displayed on the monitor shows various options available

for input source, ML model, output sink. Each option carry an

index number along side.

Select elements to be used in the pipeline in the sequence of

"input source, ML model, output sink and performance

mode flag" seperated by commas.

eg: 1,1,3,0

Above input will run "filesrc" input, "resnet50" model

"kmssink" used as output sink and performance mode disabled.

Enter 'q' to exit

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

3,16,3,0

...

 >>>>> Enter any key to return to main menu <<<<<

 

The following animated image shows the expected output for this above example:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Note that for real-time execution, the USB camera must support NV12 format. For this reason, I recommend to use the following USB camera:

  • Logitech BRIO

image

Other USB cameras that do not support NV12 format, will require software color space conversion, which will prevent achieving real-time performance.

image 

It is possible to accelerate this conversion, but this is beyond the scope of this project.

 

NOTE : If you get a green screen after a certain period, I found that stopping and re-starting the example will resolve this issue.

 

Running the application with MIPI sensor input

In order to apply a model to the MIPI sensor input, use the "4, #, 3, 0" syntax, where # is a value from 1-16, representing one of the supported models.

 

For example, to apply model #14 to the MIPI sensor, launch the example as follows:

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

Menu displayed on the monitor shows various options available

for input source, ML model, output sink. Each option carry an

index number along side.

Select elements to be used in the pipeline in the sequence of

"input source, ML model, output sink and performance

mode flag" seperated by commas.

eg: 1,1,3,0

Above input will run "filesrc" input, "resnet50" model

"kmssink" used as output sink and performance mode disabled.

Enter 'q' to exit

XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

4,14,3,0

...

 >>>>> Enter any key to return to main menu <<<<<

 

The following animated image shows the expected output for this above example:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This example launches the following GStreamer pipeline:

image

 

Deployment Fow

Using the pre-built package that we created in the previous sections, we can also deploy our custom Kria app, like any other Kria app, as shown below.

 image

Recall that we created rpm packages for our custom Kria app:

  • kv260-vvas-sms
  • kv260-vvas-sms-models
  • kv260-vvas-sms-app
  • packagegroup-kv260-vvas-sms

These rpm packages would have to be hosted to a server, and their location specified the /etc/yum.repos.d/*.repo

This has not been completed for this project tutorial, but may be in the near future Blush

 

Next Steps

The following blogs cover the previous development steps for this in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-part1
  • http://avnet.me/kv260-vvas-sms-2021-1-part2
  • http://avnet.me/kv260-vvas-sms-2021-1-part3
  • http://avnet.me/kv260-vvas-sms-2021-1-part4
  • http://avnet.me/kv260-vvas-sms-2021-1-part5
  • http://avnet.me/kv260-vvas-sms-2021-1-part6