FPGA
  • Technologies
  • More
FPGA
Blog Making a Vivado Development Board Reference Design Your Own
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ad0es
  • Date Created: 29 Dec 2022 4:04 PM Date Created
  • Views 2908 views
  • Likes 9 likes
  • Comments 2 comments
Related
Recommended

Making a Vivado Development Board Reference Design Your Own

ad0es
ad0es
29 Dec 2022

Decided to recreate the process of going from a vendor provided reference design to a first version of my project. I've literally gone thru more than a dozen iterations of this process to gain the knowledge of how to do it properly.

The vendor's reference design was done with Vivado 2019 on windoz. I am using Vivado 2022.2 on Ubuntu 22.04. This causes most of the IP to be "out of date". There is a vendor provided doc, which being run under windoz can be misleading...

The first step is to open the reference design, bring it up to date, and then save as our design.

$ file 32_pcie_ram_axilite_usr_bypass.rar
32_pcie_ram_axilite_usr_bypass.rar: RAR archive data, v4, os: Win32

$ unrar x 32_pcie_ram_axilite_usr_bypass.rar

UNRAR 6.11 beta 1 freeware      Copyright (c) 1993-2022 Alexander Roshal


Extracting from 32_pcie_ram_axilite_usr_bypass.rar

Creating    pcie_ram_axilite_usr_bypass                               OK
 ...
All OK

Start Vivado and select [Open Project]

image

This will display a splash screen:

image

Click [OK]

Then:

image

Click [Yes]

A splash screen warns of the "out of date" IP:

image
Click [Report IP Status]

At the bottom of the Vivado GUI an IP Status tab will be added:

image

Everything requiring update should be selected.

Click [Upgrade Selected]

Then this appears:

image

Click [OK]

image

Click [OK]

image

Click [Generate]

image

image

Click [OK]

This will grind along in the background for quite a while...

image


Ending with:

image

Click [details]

Causing this popup:

image

Click [Force up-to-date]

Which may display this:

image


If so, select the Messages tab at bottom of GUI:

image

I'm guessing this is a result of limiting the path to what windoz can handle, we'll clean it up when we "save as" to create out project.

At this point we have:

image

Time to "save as" our project.

Select [File > Project > Save As...]

image

I renamed the project to dfcSDR, and selected a location with the same name. Leave "Include run results" unchecked, we want to leave the windoz cruft behind us. Edit appropriately and then:

Click [OK]

Select [File > Close Project]

Re-open the new project, it should be at the top of Recent Projects on the right side of GUI. We now have:

image


As a result of Create project directory we have:

../dfcSDR$ ls -At
Blog/  Notes/  dfcSDR/
../dfcSDR$ ls -At dfcSDR
dfcSDR.runs           dfcSDR.cache  dfcSDR.gen   dfcSDR.hw
dfcSDR.ip_user_files  dfcSDR.sim    dfcSDR.srcs  dfcSDR.xpr


I added Blog and Notes directories for things I make associated with the project.


Add git version control.

../dfcSDR$ git init
 ...
Initialized empty Git repository in ../dfcSDR/.git/
../dfcSDR$ l
Blog/  dfcSDR/  Notes/
../dfcSDR$ l -a
./  ../  Blog/  dfcSDR/  .git/  .gitignore  Notes/
../dfcSDR$ git status
On branch master

No commits yet

Untracked files:
  (use "git add <file>..." to include in what will be committed)
	.gitignore
	Blog/
	dfcSDR/

nothing added to commit but untracked files present (use "git add" to track)
../dfcSDR$ l Blog
addtoBlog
../dfcSDR$ git add .
../dfcSDR$ git status
On branch master

No commits yet

Changes to be committed:
  (use "git rm --cached <file>..." to unstage)
	new file:   .gitignore
	new file:   Blog/addtoBlog
 ...
	new file:   dfcSDR/dfcSDR.xpr

../dfcSDR$ find . -type f | wc -l
1487

../dfcSDR$ git config user.email "foo@bar"
../dfcSDR$ git config user.name "Foo Bar"
../dfcSDR$ git commit -m "Initial commit."
[master (root-commit) cb09936] Initial commit.
 881 files changed, 3027609 insertions(+)
 create mode 100644 .gitignore
 ...
 create mode 100644 dfcSDR/dfcSDR.xpr
../dfcSDR$ git status
On branch master
nothing to commit, working tree clean

Now that the base files are under git control its time to synthesize the design:

Click [Run Synthesis]

image

Note that I had previously set "Number of jobs" to 14 (default is 8) as I have 16 cores.

Click [OK]

image

This takes awhile...

image

Click [OK]

Synthesis created a lot of new files for git:

../dfcSDR$ git status
On branch master
Changes not staged for commit:
  (use "git add <file>..." to update what will be committed)
  (use "git restore <file>..." to discard changes in working directory)
	modified:   Blog/addtoBlog
	modified:   dfcSDR/dfcSDR.cache/wt/synthesis.wdf
 ...
	modified:   dfcSDR/dfcSDR.xpr

Untracked files:
  (use "git add <file>..." to include in what will be committed)
	dfcSDR/dfcSDR.cache/ip/
	dfcSDR/dfcSDR.runs/

no changes added to commit (use "git add" and/or "git commit -a")
../dfcSDR$ git add -u
../dfcSDR$ git commit -m "After running initial synthesis."
[master 888c25b] After running initial synthesis.
 59 files changed, 924884 insertions(+), 924856 deletions(-)
 rewrite dfcSDR/dfcSDR.gen/sources_1/bd/PCIe/ip/PCIe_Reg_wrAXI4lite_0_2/PCIe_Reg_wrAXI4lite_0_2.dcp (95%)
 ...
 rewrite dfcSDR/dfcSDR.gen/sources_1/bd/PCIe/ip/PCIe_util_vector_logic_0_0/PCIe_util_vector_logic_0_0.dcp (88%)

Now we have to run the implementation.

Select [Run implementation]

image

Click [OK]

This takes even more time...

image

And finally finishes:

image

Click [OK]

Implementation also creates a lot of new files for git:

../dfcSDR$ git status
On branch master
Changes not staged for commit:
  (use "git add <file>..." to update what will be committed)
  (use "git restore <file>..." to discard changes in working directory)
	modified:   dfcSDR/dfcSDR.cache/wt/gui_handlers.wdf
	modified:   dfcSDR/dfcSDR.cache/wt/java_command_handlers.wdf
	modified:   dfcSDR/dfcSDR.cache/wt/webtalk_pa.xml
	modified:   dfcSDR/dfcSDR.xpr

Untracked files:
  (use "git add <file>..." to include in what will be committed)
	dfcSDR/dfcSDR.cache/ip/
	dfcSDR/dfcSDR.runs/

no changes added to commit (use "git add" and/or "git commit -a")
/dfcSDR$ git add -u
../dfcSDR$ git commit -m "After running initial implementation."
[master c50aaf1] After running initial implementation.
 5 files changed, 457 insertions(+), 413 deletions(-)
../D/dfcSDR$ git status
On branch master
Untracked files:
  (use "git add <file>..." to include in what will be committed)
	dfcSDR/dfcSDR.cache/ip/
	dfcSDR/dfcSDR.runs/

nothing added to commit but untracked files present (use "git add" to track)

Now we create the .bit and .bin files.

Select [Generate Bitstream]

image

Click [OK]

More churn...

image

All done.

image

Click [OK]

Update git:

../dfcSDR$ git status
On branch master
Changes not staged for commit:
  (use "git add <file>..." to update what will be committed)
  (use "git restore <file>..." to discard changes in working directory)
	modified:   dfcSDR/dfcSDR.cache/wt/project.wpc
	modified:   dfcSDR/dfcSDR.cache/wt/webtalk_pa.xml

Untracked files:
  (use "git add <file>..." to include in what will be committed)
	dfcSDR/dfcSDR.cache/ip/
	dfcSDR/dfcSDR.runs/

no changes added to commit (use "git add" and/or "git commit -a")
../dfcSDR$ git add -u
../dfcSDR$ git commit -m "After running Generate Bitstream."
[master ff74bde] After running Generate Bitstream.
 3 files changed, 52 insertions(+), 3 deletions(-)

Looking good:

image

A LOT of Warnings, but no Errors!

image

Time to test.

Select [Open Hardware Manager]

Select [Open Target > AutoConnect]

image

Select [Program Device > <your device>]

Select the correct .bit file:

image

Select [Program]

All looks good:

image

This step loaded the code directly to the FPGA. To test it we have to restart linux WITHOUT a power-cycle. Running the test immediately after the load fails.

The test:

#! /bin/sh
#

echo "Checking for device..."
lspci | grep Xilinx
if [ $? -eq 1 ]; then
    echo FAIL; sleep 50; exit
fi

echo "Loading driver"
cd ../LinuxPCIeDrivers/dma_ip_drivers/XDMA/linux-kernel/tests
./load_driver.sh
if [ $? -eq 1 ]; then
    echo FAIL; sleep 50; exit
fi

./run_test.sh

sleep 1000

The result:

Checking for device...
01:00.0 Memory controller: Xilinx Corporation Device 7024
Loading driver
interrupt_selection .
Loading driver...insmod xdma.ko interrupt_mode=2 ...

Error: The Kernel module installed correctly, but no devices were recognized.
 FAILED
FAIL

On Ubuntu select Poweroff > restart

Retest once Ubuntu has restarted:

Checking for device...
01:00.0 Memory controller: Xilinx Corporation Device 7024
Loading driver
interrupt_selection .
Loading driver...insmod xdma.ko interrupt_mode=2 ...

The Kernel module installed correctly and the xmda devices were recognized.
DONE
Info: Number of enabled h2c channels = 2
Info: Number of enabled c2h channels = 2
Info: The PCIe DMA core is memory mapped.
Info: Running PCIe DMA memory mapped write read test
	transfer size:  1024, count: 1
Info: Writing to h2c channel 0 at address offset 0.
Info: Writing to h2c channel 1 at address offset 1024.
Info: Wait for current transactions to complete.
/dev/xdma0_h2c_1 ** Average BW = 1024, 8.630716
/dev/xdma0_h2c_0 ** Average BW = 1024, 7.923673
Info: Writing to h2c channel 0 at address offset 2048.
Info: Writing to h2c channel 1 at address offset 3072.
Info: Wait for current transactions to complete.
/dev/xdma0_h2c_0 ** Average BW = 1024, 16.706366
/dev/xdma0_h2c_1 ** Average BW = 1024, 29.789957
Info: Reading from c2h channel 0 at  address offset 0.
Info: Reading from c2h channel 1 at  address offset 1024.
Info: Wait for current transactions to complete.
/dev/xdma0_c2h_0 ** Average BW = 1024, 15.247852
/dev/xdma0_c2h_1 ** Average BW = 1024, 46.265759
Info: Reading from c2h channel 0 at  address offset 2048.
Info: Reading from c2h channel 1 at  address offset 3072.
Info: Wait for current transactions to complete.
/dev/xdma0_c2h_0 ** Average BW = 1024, 7.360711
/dev/xdma0_c2h_1 ** Average BW = 1024, 14.372131
Info: Checking data integrity.
Info: Data check passed for address range  0 - 1024
Info: Data check passed for address range  1024 - 2048
Info: Data check passed for address range  2048 - 3072
Info: Data check passed for address range  3072 - 4096
Info: All PCIe DMA memory mapped tests passed.
Info: All tests in run_tests.sh passed.

Now we test the ability to load the .bin file to the board's flash. If its highlighted, you need to click the "Add Configuration Memory Device", and then create the appropriate device for your board. If its grayed out you should right-click the existing <flash device> field:

image

Then select "Program Memory Configuration Device..." from the popup menu.

image

Click [OK]

It first erases the part and then programs the flash part.

image

This warning may pop up. It can safely be ignored. It occurs because Labtools looses communication with the FPGA while the JPEG is connected to the flash.

image

Click [OK] to dismiss it.

This step loaded the code to the board's flash, which is used to load the FPGA on power-up of the box. To test this we stop Ubuntu with a power-off, followed by a power-on. I've found that having the JPEG attached during power-up sometimes prevents the FPGA from booting, so best to disconnect it before re-powering the box:

Checking for device...
01:00.0 Memory controller: Xilinx Corporation Device 7024
Loading driver
interrupt_selection .
Loading driver...insmod xdma.ko interrupt_mode=2 ...

The Kernel module installed correctly and the xmda devices were recognized.
DONE
Info: Number of enabled h2c channels = 2
Info: Number of enabled c2h channels = 2
Info: The PCIe DMA core is memory mapped.
Info: Running PCIe DMA memory mapped write read test
	transfer size:  1024, count: 1
Info: Writing to h2c channel 0 at address offset 0.
Info: Writing to h2c channel 1 at address offset 1024.
Info: Wait for current transactions to complete.
/dev/xdma0_h2c_1 ** Average BW = 1024, 8.630716
/dev/xdma0_h2c_0 ** Average BW = 1024, 7.923673
Info: Writing to h2c channel 0 at address offset 2048.
Info: Writing to h2c channel 1 at address offset 3072.
Info: Wait for current transactions to complete.
/dev/xdma0_h2c_0 ** Average BW = 1024, 16.706366
/dev/xdma0_h2c_1 ** Average BW = 1024, 29.789957
Info: Reading from c2h channel 0 at  address offset 0.
Info: Reading from c2h channel 1 at  address offset 1024.
Info: Wait for current transactions to complete.
/dev/xdma0_c2h_0 ** Average BW = 1024, 15.247852
/dev/xdma0_c2h_1 ** Average BW = 1024, 46.265759
Info: Reading from c2h channel 0 at  address offset 2048.
Info: Reading from c2h channel 1 at  address offset 3072.
Info: Wait for current transactions to complete.
/dev/xdma0_c2h_0 ** Average BW = 1024, 7.360711
/dev/xdma0_c2h_1 ** Average BW = 1024, 14.372131
Info: Checking data integrity.
Info: Data check passed for address range  0 - 1024
Info: Data check passed for address range  1024 - 2048
Info: Data check passed for address range  2048 - 3072
Info: Data check passed for address range  3072 - 4096
Info: All PCIe DMA memory mapped tests passed.
Info: All tests in run_tests.sh passed.

Our project is working!

image

  • Sign in to reply
Parents
  • flyingbean
    flyingbean over 3 years ago

    Great document for a Vivado flow, especially for IP flow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • flyingbean
    flyingbean over 3 years ago

    Great document for a Vivado flow, especially for IP flow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ad0es
    ad0es over 3 years ago in reply to flyingbean

    Knowing nothing about FPGA programming or Vivado, It took me several weeks of diddling to get the reference code to build properly.  I thought I might save some else the grief Stuck out tongue winking eye