FPGA
  • Technologies
  • More
FPGA
Blog Summer of FPGAs - Building an Embedded System on FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yesha98
  • Date Created: 16 Aug 2021 4:31 PM Date Created
  • Views 6543 views
  • Likes 11 likes
  • Comments 21 comments
Related
Recommended

Summer of FPGAs - Building an Embedded System on FPGA

yesha98
yesha98
16 Aug 2021

Introduction:

Back then in February when I roadtested the USB104-A7, I had learned to create block designs using MicroBlaze. I found it very interesting but the available online resources were limited, the tutorials were based on the older versions of Vivado (Uploaded 6 years back or so). So I thought of making a course on using MicroBlaze in block designs and programming it with Xilinx SDK. Finally, after my semester exams were over, I got some free time to record the tutorials and the course material.

 

The course is designed in such a way that basic knowledge on FPGA programming using Vivado would be sufficient to take up this course. Also, the learner will understand the design of hardware while making the custom Pmod (Pmod Character LCD) and the working of Rotary Encoder.

 

Also, in this course, the design will be modified as new modules are added according to the requirements. The quadrature decoder module described in Verilog will also be added to the design at a later stage in the course. Thus, the learner will be able to feel the essence of the term "Reconfigurable Hardware".

 

Course Contents:

Video 1 - Introduction to MicroBlaze and AXI

Video 2 -- Lab 1 - Creating a block design with MicroBlaze and AXI GPIOs

Video 3 -- Lab 2 - Writing code in Xilinx SDK to interface with user LED and Pushbutton

Video 4 - Working of Character LCD and making of the Pmod LCD

Video 5 -- Lab 3 - Modifying the block design to interface Pmod LCD

Video 6 -- Lab 4 - LCD Driver Code to display elapsed seconds in LCD

Video 7 - Working of Rotary Encoder and Quadrature Decoder

VIdeo 8 -- Lab 5 - Adding the Quadrature Decoder Module to the Design

Video 9 -- Lab 6 - Writing code in SDK to display count and direction to the LCD

VIdeo 10 - Final Assessment

 

 

About the Course:

All videos are available on YouTube, here's the link to Playlist: https://www.youtube.com/playlist?list=PL6jYIySXv7VhUjg95oP88ubxRrr9MQMfH

Complete the final assessment to earn a certificate!

 

Course Overview:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thanks for reading!

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +2
    Video 3 also worked perfectly on a Pynq-Z2 board with Zynq IC. www.youtube.com/watch
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to yesha98 +2
    yesha98 wrote: ... Btw, I have a doubt, so you added the onboard LEDs and Pushbuttons through AXI GPIO right. After adding the Zynq IP in block design, if we run the block automation, the Fixed IO and…
  • navadeepganeshu
    navadeepganeshu over 5 years ago +2
    Gave a try with ARTY S7 - 50. For this board, I skipped adding NOT logic for reset(lab video1) as it was active low with the onboard switch by default. Used GPIO0 and 1 for 4 x LEDs and 4 x pushbuttons…
  • navadeepganeshu
    navadeepganeshu over 5 years ago

    Gave a try with ARTY S7 - 50. For this board, I skipped adding NOT logic for reset(lab video1) as it was active low with the onboard switch by default. Used GPIO0 and 1 for 4 x LEDs and 4 x pushbuttons. The hello word is here: (I didn't believe it worked and suspected "hello world" was out-of-the-box demo serial prints. But ya, with "It works!" It works.
    All other steps are almost the same and were compatible with Vitis IDE(on 2020.1). Nice series,...following through.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yesha98
    yesha98 over 5 years ago in reply to Jan Cumps

    Oh right!

    Thanks again Jan Cumps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to yesha98

    yesha98  wrote:

    ...

    Btw, I have a doubt, so you added the onboard LEDs and Pushbuttons through AXI GPIO right.

    After adding the Zynq IP in block design, if we run the block automation, the Fixed IO and DDR get mapped right.

    So in that case, we use XGpiops.h, but in my code, I write 0xA or 0xC to the 4 bits of LEDs connected to AXI GPIO which uses XGpio.h.

    ...

    The LEDs and Buttons work exactly as in your example, and are linked the same.

     

    The 2 AXI GPIOs are attached to the Microblaze. They are not related to the Zynq.

    image

    The Zynq PS does not play a role - except as source for Clock and Reset for the whole PL FPGA design.

     

    And when creating an Application in Vitis, I select that MicroBlaze as target for my Application.

    image

    image

    The code is exacly yours:

     

    #include "xgpio.h"
    #include "xparameters.h"
    #include "sleep.h"
    
    // ...
    
        int val, toggle = 0;
        XGpio input, output;
        XGpio_Initialize(&input, XPAR_AXI_GPIO_0_DEVICE_ID);
        XGpio_Initialize(&output, XPAR_AXI_GPIO_1_DEVICE_ID);
        XGpio_SetDataDirection(&input, 1, 0x01);
        XGpio_SetDataDirection(&output, 1, 0x00);
        while(1) {
          val = XGpio_DiscreteRead(&input,  1);
          if(val == 1) {
            print("Button pressed\n\r");
            toggle = ~toggle;
          }
          if(toggle) {
            XGpio_DiscreteWrite(&output, 1, 0b1010);
            usleep(250000);
            XGpio_DiscreteWrite(&output, 1, 0b0101);
            usleep(250000);
          } else {
            XGpio_DiscreteWrite(&output, 1, 0b1100);
            usleep(250000);
            XGpio_DiscreteWrite(&output, 1, 0b0011);
            usleep(250000);
          }
        }

     

    yesha98  wrote:

     

    Can you tell me how XGpiops.h can be used without adding the AXI GPIO in block design only with Zynq? (Without using MicroBlaze)

    In that case you would connect an AXI Interconnect and the 2 AXI GPIOs to a Master AXI output of the Zynq. You don't see one in my block diagram because I didn't enable (need) it.

    In Vitis, you would then build your application against the Zynq ARM processors.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yesha98
    yesha98 over 5 years ago in reply to Jan Cumps

    That's great Jan Cumps.

    Btw, I have a doubt, so you added the onboard LEDs and Pushbuttons through AXI GPIO right.

    After adding the Zynq IP in block design, if we run the block automation, the Fixed IO and DDR get mapped right.

    So in that case, we use XGpiops.h, but in my code, I write 0xA or 0xC to the 4 bits of LEDs connected to AXI GPIO which uses XGpio.h.

    Can you tell me how XGpiops.h can be used without adding the AXI GPIO in block design only with Zynq? (Without using MicroBlaze)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    Video 3 also worked perfectly on a Pynq-Z2 board with Zynq IC.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>