FPGA
  • Technologies
  • More
FPGA
Blog The N64=>HDMI Conversion Project: Part 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: muddpup64
  • Date Created: 22 Oct 2018 6:03 AM Date Created
  • Views 1526 views
  • Likes 2 likes
  • Comments 3 comments
  • hardware
  • student
  • artix-7
  • computer engineering
  • fpga
  • n64
  • vhdl
  • saleae
Related
Recommended

The N64=>HDMI Conversion Project: Part 2

muddpup64
muddpup64
22 Oct 2018

This is an update of my on going N64 HDMI conversion project. The N64=>HDMI Conversion Project

As of right now I have identified that the RCP (or the GPU) have common outputs between board revisions for the video and audio. There is a seven bit word, Dsync, and clock that contribute to the digital video signal. These are connected to a DAC that outputs an RGB signal. The plan is to rob these signals on there way to the DAC in order to reduce complexity and latency of the FPGA design. I have acquired a Saleae Logic Pro 16 to analyze these signals in order to try and find a pattern. The hypothesis this that these seven bit words come in sets of three, one for blue, one for green, and one for red and that the Dsync weaves these signals together. I have yet to grab a clean signal off of the chip as the probes that came with the Saleae seem to also be shorting out the other pins. I plan on soldering on a ribbon cable using my campus's microscope and micro pencil to resolve this problem.

 

Simultaneously, I have gotten myself a Artix-7 dev board with an HDMI port and am teaching myself VHDL. I have decided to go with VHDL as it is what the overwhelming majority of my peers use and this will make it easier for me to ask questions, of which, I always have plenty.

 

This week I plan on doing some VHDL practice and to hopefully acquire a clean signal off of my board.

 

I have attached some photos of what I have done so far. I apologize for the poor lighting, my phone is having some issues.

Attachments:
image
image
image
image
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 7 years ago +1
    Bold use of the tiny clips on the logic analyser ! I usually solder tiny wires to the chip and connect these to a dual row 0.1" pitch connector (often glues to the chip) and then my logic analyser plugs…
  • genebren
    genebren over 7 years ago +1
    Interesting project. It looks like you are moving along smoothly so far. Good luck! Gene
  • muddpup64
    muddpup64 over 7 years ago

    I finally got around to doing some work on the project. Here is my latest peice: The N64=>HDMI Conversion Project: Part 3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    Interesting project.  It looks like you are moving along smoothly so far.

    Good luck!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago

    Bold use of the tiny clips on the logic analyser !

     

    I usually solder tiny wires to the chip and connect these to a dual row 0.1" pitch connector (often glues to the chip) and then my logic analyser plugs straight in.

    I get too many problems with the clips shorting or falling off.

     

    I'd be interested to see a screenshot of the logic analyser's capture of the signals.

     

    MK