FPGA
  • Technologies
  • More
FPGA
Blog Arty-S7-Rover (experiments)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dramoz
  • Date Created: 24 Jul 2022 4:57 AM Date Created
  • Views 759 views
  • Likes 7 likes
  • Comments 0 comments
  • 7 Ways to Leave Your Spartan-6
  • 7 Ways to Leave Your Spartan-6 FPGA: Arty S7 Activities
  • Spartan_Migration
Related
Recommended

Arty-S7-Rover (experiments)

dramoz
dramoz
24 Jul 2022

Trolleybus Arty-S7-Rover (experiments)

Disclaimer

An experiment with the Arty S7, 7 Ways to Leave Your Spartan-6 FPGA element14 Community challenge.

The Arty-S7-Rover is a small functional autonomous vehicle based on the Digilent Arty S7-50 board. The project was done for the 7 Ways to Leave Your Spartan-6 FPGA element14 Community challenge.

All the files are open-source, MIT license and can be downloaded from GitHub Logo-imgdramoz

Experiments

A collection of some experiments I tried while building this project

VexRiscv

How fast can I toggle a led?

  • RISC-V IO registers latency test

Toggling a bit from a microprocessor would require some instructions that add some latency to the event. The firmware in this case is a simple toggle operation on an IO register.

#include "memory_map.h"
int main(void) {
  for(;;) {
    WRITE_IO(LEDS_REG, 5);
    WRITE_IO(LEDS_REG, ~5);
  };
  return 0;
}

image

Arty-S7 VexRiscv LED toggle (1)

By checking the simulation, I saw that there was a latency - caused by the for(;;) loop, which caused a jump and a reload of the target register address in the RISCV CPU registers.

int main(void) {
  for(;;) {
    WRITE_IO(LEDS_REG, 5);
 14c:	800007b7          	lui	a5,0x80000
 150:	00500713          	li	a4,5
 154:	00e7a623          	sw	a4,12(a5) # 8000000c <__io_end+0xfffffc0c>
    WRITE_IO(LEDS_REG, ~5);
 158:	ffa00713          	li	a4,-6
 15c:	00e7a623          	sw	a4,12(a5)
  for(;;) {
 160:	fedff06f          	j	14c <main>

Another try

#include "memory_map.h"

int main(void) {
  for(;;) {
    WRITE_IO(LEDS_REG, 1);
    WRITE_IO(LEDS_REG, 2);
    WRITE_IO(LEDS_REG, 3);
    WRITE_IO(LEDS_REG, 4);
    WRITE_IO(LEDS_REG, 5);
    WRITE_IO(LEDS_REG, 6);
    WRITE_IO(LEDS_REG, 7);
    WRITE_IO(LEDS_REG, 8);
    WRITE_IO(LEDS_REG, 9);
    WRITE_IO(LEDS_REG, 0);
  };
  return 0;
}

image

Arty-S7 VexRiscv LED toggle (2)

Note that this case is misleading, as by checking the assembly file you can notice that the compiler did a good job and the target address is only loaded once.

int main(void) {
  for(;;) {
    WRITE_IO(LEDS_REG, 1);
 14c:	800007b7          	lui	a5,0x80000
 150:	00100713          	li	a4,1
 154:	00e7a623          	sw	a4,12(a5) # 8000000c <__io_end+0xfffffc0c>
    WRITE_IO(LEDS_REG, 2);
 158:	00200713          	li	a4,2
 15c:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 3);
 160:	00300713          	li	a4,3
 164:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 4);
 168:	00400713          	li	a4,4
 16c:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 5);
 170:	00500713          	li	a4,5
 174:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 6);
 178:	00600713          	li	a4,6
 17c:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 7);
 180:	00700713          	li	a4,7
 184:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 8);
 188:	00800713          	li	a4,8
 18c:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 9);
 190:	00900713          	li	a4,9
 194:	00e7a623          	sw	a4,12(a5)
    WRITE_IO(LEDS_REG, 0);
 198:	0007a623          	sw	zero,12(a5)
  for(;;) {
 19c:	fb1ff06f          	j	14c <main>

A final attempt produced the expected behaviour.

#include "memory_map.h"
int main(void) {
  for(;;) {
    WRITE_IO(LEDS_REG, 1);
    WRITE_IO(DEBUG_REG, 2);
    WRITE_IO(LEDS_REG, 3);
    WRITE_IO(DEBUG_REG, 4);
    WRITE_IO(LEDS_REG, 5);
    WRITE_IO(DEBUG_REG, 6);
    WRITE_IO(LEDS_REG, 7);
    WRITE_IO(DEBUG_REG, 8);
    WRITE_IO(LEDS_REG, 9);
    WRITE_IO(DEBUG_REG, 0);
  };
  return 0;
}


image

Arty-S7 VexRiscv LED toggle (3)

 

Point right As seen on the waves, it takes four (4) clock cycles to set up an IO register.

Arty-S7

The right PWM frequency

Finding the right Geared Motor DC PMW frequency and duty cycle was challenging. The geared dc motor added an extra complexity as the required starting torque was high. To speed up the test, firmware that used the dip switch and buttons to switch between different speeds and RTL with different PWM frequencies was created. After some trial and error, the best frequency found was 500Hz, with a duty cycle range between 30% and 100%. For the final version of the project, the max duty cycle was set to 80% as the difference in speed was not required.

#include<cstdint>
#include "memory_map.h"

const uint32_t CLK_FREQ     = 100000000;
const uint32_t RGB_PWM_FREQ =     20000;
const uint32_t RGB_DCYLE  = uint32_t(0.01 * CLK_FREQ/RGB_PWM_FREQ);

const uint32_t MOTOR_PWM_FREQ   = 500;
const uint32_t MOTOR_FULL_STOP  = 0;
const uint32_t MOTOR_SLOW_SPEED = uint32_t(0.1 * CLK_FREQ/MOTOR_PWM_FREQ);
const uint32_t MOTOR_HIGH_SPEED = uint32_t(0.5 * CLK_FREQ/MOTOR_PWM_FREQ);
const uint32_t MOTOR_SPEED_STEP = uint32_t(0.4/16 * CLK_FREQ/MOTOR_PWM_FREQ);

const uint32_t UART_MASK    = 0x80000000;

int main(void) {
  // LEDs
  uint32_t leds_st = 1;
  uint32_t rgb0 = 1;
  uint32_t rgb1 = 1;
  
  // IOs
  uint32_t btn = 0;
  uint32_t sw  = 0;
  
  // Setup Motors PWMs
  uint32_t dir_rpt = (uint32_t)('s');  // s:stop, f:forward, b:backward, l:left, r:right
  uint32_t motor_curr_speed = MOTOR_FULL_STOP;
  WRITE_IO(M0_BWD_PWM_REG, MOTOR_FULL_STOP);
  WRITE_IO(M0_FWD_PWM_REG, MOTOR_FULL_STOP);
  WRITE_IO(M1_BWD_PWM_REG, MOTOR_FULL_STOP);
  WRITE_IO(M1_FWD_PWM_REG, MOTOR_FULL_STOP);
  
  // Setup RGBs to low intensity
  WRITE_IO(RGB0_DCYCLE_REG, RGB_DCYLE);
  WRITE_IO(RGB1_DCYCLE_REG, RGB_DCYLE);
  
  // Turn on LEDs 1 to ACK PWR and RISCV boot OK.
  WRITE_IO(LEDS_REG, leds_st);
  
  // UART Hello World
  const char* hello_msg = "Arty-S7 ROVER (VexRiscv)\r\n";
  uint32_t inx = 0;
  
  bool pending_tx;
  uint32_t uart_rx;
  uint32_t uart_tx;
  
  while(hello_msg[inx]!=0) {
    uart_tx = READ_IO(UART0_TX_REG);
    if((uart_tx & UART_MASK)==0) {
      WRITE_IO(UART0_TX_REG, (uint32_t)hello_msg[inx] | UART_MASK);
      ++inx;
    }
  };
  
  // Loop forever
  pending_tx = false;
  uart_rx = 0;
  for(;;) {
    btn = READ_IO(BUTTONS_REG);
    sw  = READ_IO(SWITCHES_REG);
    
    // DC motors
    // Select speed from SW
    if(sw==0) {
      motor_curr_speed = MOTOR_FULL_STOP;
    }
    else if(sw==0xff) {
      motor_curr_speed = MOTOR_HIGH_SPEED;
    }
    else {
      motor_curr_speed = MOTOR_SPEED_STEP * sw + MOTOR_SLOW_SPEED;
    }
    
    // Select direction from button
    // Prioritize as only one setting is possible
    leds_st = btn;
    if(btn & 0x1) {
      // Move FWD
      dir_rpt = (uint32_t)('f');
      WRITE_IO(M0_BWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M0_FWD_PWM_REG, motor_curr_speed);
      WRITE_IO(M1_BWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M1_FWD_PWM_REG, motor_curr_speed);
    }
    else if(btn & 0x2) {
      // Move BKD
      dir_rpt = (uint32_t)('b');
      WRITE_IO(M0_BWD_PWM_REG, motor_curr_speed);
      WRITE_IO(M0_FWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M1_BWD_PWM_REG, motor_curr_speed);
      WRITE_IO(M1_FWD_PWM_REG, MOTOR_FULL_STOP);
    }
    else if(btn & 0x4) {
      // Move Right
      dir_rpt = (uint32_t)('r');
      WRITE_IO(M0_BWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M0_FWD_PWM_REG, motor_curr_speed);
      WRITE_IO(M1_BWD_PWM_REG, motor_curr_speed);
      WRITE_IO(M1_FWD_PWM_REG, MOTOR_FULL_STOP);
    }
    else if(btn & 0x8) {
      // Move Left
      dir_rpt = (uint32_t)('l');
      WRITE_IO(M0_BWD_PWM_REG, motor_curr_speed);
      WRITE_IO(M0_FWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M1_BWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M1_FWD_PWM_REG, motor_curr_speed);
    }
    else {
      // Stop
      dir_rpt = 0;
      WRITE_IO(M0_BWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M0_FWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M1_BWD_PWM_REG, MOTOR_FULL_STOP);
      WRITE_IO(M1_FWD_PWM_REG, MOTOR_FULL_STOP);
    }
    
    // Update LEDs
    WRITE_IO(LEDS_REG, leds_st);
    WRITE_IO(RGB0_REG, rgb0);
    WRITE_IO(RGB1_REG, rgb1);
    
    // UART
    if(!pending_tx) {
      uart_rx = READ_IO(UART0_RX_REG);
    }
    
    // Echo
    if(uart_rx & UART_MASK) {
      uart_tx = READ_IO(UART0_TX_REG);
      if((uart_tx & UART_MASK)==0) {
        WRITE_IO(UART0_TX_REG, uart_rx);
        pending_tx = false;
        uart_rx = 0;
      }
      else {
        pending_tx = true;
      }
    }
    else {
      // Report
      if(!pending_tx) {
        if(dir_rpt) {
          WRITE_IO(UART0_TX_REG, dir_rpt | UART_MASK);
          dir_rpt = 0;
        }
      }
    }
  };
  
  return 0;
}

A variable frequency variable duty cycle PWM

Given the issues with the PWM frequency and duty cycle, I decided to try a variable frequency / variable duty cycle PWM. When doing DC motor speed control with PWM. Usually, the PWM frequency is kept fixed while varying the duty cycle. A brushed DC motor's PWM frequency is characterized by the motor time constant which is set by the motor's internal impedance, and it can be modelled as an inductor with a resistor in series. Googling around you will find different recommendations, from ranges between 200Hz~500Hz or 5KHz~20KHz. As each motor model is different, a practical approach could be from trial and error to find a good frequency.

After finding different possible PWM frequencies/duty cycle pairs, I experimented by implementing a variable frequency / variable duty cycle PWM IP block controlled by the RISC-V FW. The results were kind of interesting, but more work is required.