FPGA
  • Technologies
  • More
FPGA
Blog VIDOR 4000: Clock Jitter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 12 Jul 2021 10:15 PM Date Created
  • Views 4251 views
  • Likes 8 likes
  • Comments 19 comments
  • intel
  • cyclone 10
  • vidor 4000
  • fpga
  • clock jitter
  • arduino
Related
Recommended

VIDOR 4000: Clock Jitter

jc2048
jc2048
12 Jul 2021

Without connecting anything else to the VIDOR, the only clock we're given to work with is one

that comes from the SAM microcontroller. Here it is on the VIDOR schematic, output from the SAM

part and going into one of the dedicated clock inputs.

 

image

 

image

 

 

I haven't tried to look at it directly with the 'scope. The processor is in quite a confined

space between the headers, so it would need doing very carefully.

 

If I take that clock and simply push it back out of an IO pin, I see this on the oscilloscope.

 

image

 

Here we're looking at the rising edge after the one being triggered on, i.e. the end of the

first full cycle. About 1ns of jitter. More than I was expecting.

 

For comparison, this is the equivalent experiment with my MAX CPLD board with its 50MHz crystal

oscillator, pushing the clock back out of an IO pin.

 

image

 

I wondered if we could use the PLL in the FPGA clock block to clean up the jitter. The Cyclone

10 datasheet has this to say

 

image

 

so whilst not necessarily a particularly good idea, it does look like the PLL could just about manage with

that input as it jitters around.

 

Way to find out is to try it. This is the output from a PLL set to take the 48MHz clock coming

in and produce a 100MHz clock. (I can literally see the change to 100MHz, because I left the

Johnson counter in there and the LEDs are still sequencing round, only about twice as fast.)

 

image

 

Leaving aside that my 200MHz oscilloscope can only display it as a sinewave, it is much

steadier.

 

For a lot of simple purposes the jitter on the 48MHz clock wouldn't matter anyway, but there is

the option of cleaning it up with a PLL and, for anything really critical, there's nothing to

stop you adding a xtal oscillator to your own external circuitry for a project. As you can see

from that snippet of the schematic, there's access to several of the dedicated clock lines from

the Mini PCIe connector (the signals that start PEX_).

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 5 years ago +3
    I'm not that suprised that the SAM output clock is jittery - where does it get its clock input from ? People often use differential clock inputs on modern fast FPGAs. Not sure that the Cyclone 10 quite…
  • jc2048
    jc2048 over 5 years ago in reply to michaelkellett +3
    Thanks for the comment. There's a 32.768kHz xtal. I'm trying to resist the temptation to look at the clock stuff on the SAM and how their firmware sets it up. There seems to be a Digital Frequency Locked…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048 +2
    R28 seems to be the gateway the designers provisioned for an alternative clock.
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Jan Cumps

    Repeating the exercise on Zynq:

     

    There are 4 fabric clocks. For this exercise I've kept them to the values that the Pynq team uses in their base bitstream:

    image

    I'll link each of them to an output pin and try to capture the outputs.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to shabaz

    That's very stingy of Arduino

     

    It saves a few pennies. I'm out of touch with where things are with processors [and I'm not well-versed with ARM parts], but reading that datasheet, it looks intentional to perch everything on the 32.768kHz xtal. Of course, it was Arduino's decision to then balance an FPGA on top.

     

    Think removing it and a oscillator hacked on

     

    You probably could. I don't think I'd want to even try.

     

    The processor is the Atmel part next to the blue switch. It sits between the headers on the top. On the bottom, the headers have long pins, though the access is easier: at least you wouldn't be melting the plastic connector housings.

     

    image

     

    image

     

    I could probably manage to solder a header to the 6-pin footprint on the bottom for the processor programming/debug cable, but I'm not going to mess about with 0201 resistors unless I have to.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    In the Zync 7 that I'm working with the last month, the clocks for the fpga fabric are generated by PLL modules (I would not call them peripherals because they are not external facing) in the ARM part of the silicon.

    I haven't checked the specs yet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to jc2048

    Hi Jon,

     

    That's very stingy of Arduino to use such a clock source : ) So-called Frequency Locked Loops are awful. I tried to use a similar clock generator in a TI MSP chip (they gave it a different name) and it had so much jitter I couldn't even do timing in milliseconds without large amounts of error : ( It was basically only close to the desired frequency on average, and that average still resulted into noticeably large error for millisecond-level measurements.

    The 10R might also be serving double duty just to protect against the situation that the FPGA accidentally got programmed as an output on that pin. Think removing it and a oscillator hacked on (e.g. maybe a SMD oscillator glued closely on the board dead-bug, supply decoupled closely and then a small wire running to the resistor pad perhaps through a resistor) could be a nice upgrade : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048

    Yes you are likely correct. They would have used a 0R (and bigger physical size) one if it was intended as a hacking vector.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>