FPGA
  • Technologies
  • More
FPGA
Blog Who is Interested in Experimenting with a Spartan-6 FPGA? If You Are, I have 2 Boards to Giveaway for Projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 5 Aug 2019 9:03 PM Date Created
  • Views 5260 views
  • Likes 16 likes
  • Comments 25 comments
  • scasny
  • xilinx
  • xilinx spartan 6
  • fpga
  • digilent
  • spartan-6
Related
Recommended

Who is Interested in Experimenting with a Spartan-6 FPGA? If You Are, I have 2 Boards to Giveaway for Projects

rscasny
rscasny
5 Aug 2019

I had a lot of interest in my giveaway for the Digilent CMOD S7 board, so I am offering another giveaway for 2 members who are interested in experimenting with a Spartan-6 FPGA. Let me tell you about the board first. image

 

It's called the Cmod S6 -- a Breadboardable Spartan-6 FPGA Module.

 

It's small, featuring a 48-pin DIP form factor board built around a Xilinx Spartan 6 LX4 FPGA.

 

The board also includes a programming ROM, clock source, USB programming and data transfer circuit, power supplies, and basic I/O devices. There are 46 FPGA I/O signals that are routed to 100-mil-spaced through-hole pins, making the Cmod S6 well suited for use with solderless breadboards. At just .7” by 2.6” inches, it can also be loaded in a standard socket and used in embedded systems.

 

Key features include:

 

Spartan 6 XC6SLX4-2CPG196 FPGA Features include:

  • 600 slices (each with 4 LUTs and eight flip-flops);
  • 8 DSP slices;
  • 216Kbits of block RAM;
  • 2 CMTs (4 DCMs and 2 PLLs).

 

Board features include:

 

16Mbyte Spansion Quad SPI Flash for storing FPGA configurations and/or user data;

  • 46 FPGA GPIO signals brought to DIP pins;
  • Two on-board clock sources;
  • 4 user LEDs and 2 user buttons;
  • On-board Adept USB2 port for configuration, test and communications interfaces.

 

Here's the datasheet:

 

https://www.farnell.com/datasheets/1841742.pdf?_ga=2.84073758.603595138.1565037142-1061579168.1558457094

 

 

What Do You Need to Do To Get These Boards?

 

I'm running these as board project giveaways instead of RoadTests to give members interested in experimenting with the Spartan-6 but may not feel they have the background to compete in a full roadtest. So like the last giveaway if you are would-be roadtester who would like to build up his/her portfolio of things you have done on the community or you want to do something to learn about the Spartan-6 FPGA and get some time to improve your skills with the associated design tool, this could very well be for you. (A side note: I may very well decide to roadtest this in the future. But for now, I want to do a giveaway project.)

 

So, tell me what you want to achieve with this little board? What's your goal in learning? What would you like to experiment with? Or what kind of project do you think you would build. I'll choose the 2 most interesting ideas and send you the board.

 

Randall Scasny

RaodTest Program Manager

  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 7 years ago in reply to Fred27 +5
    Yes, this board uses a different tool. Here's some places to start: ISE Design Suite https://www.xilinx.com/products/design-tools/ise-design-suite.html ISE WebPACK Design Software https://www.xilinx.com…
  • rachaelp
    rachaelp over 7 years ago +5
    Hi Randall I'm not going to put my hat in the ring to get a freebie here as I think it's intended for newbies getting into FPGA design (and I do this in my job) and I don't have the time to take on another…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to rscasny +4
    The ISE toolset is best run on a windows version lower than 10. For windows 10 users, Xilinx provides a virtual machine image with Xilinx toolset installed. You start that VM to work with ISE then.
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Hey Randy, why everything in the same short time window?

     

    I am very interested but I can't write anything on this device before the end of September when I can start testing on a project. I'll submit to your decision. Anyway if no one want this, I am ok to receive it image

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago

    Hey Randy, why everything in the same short time window?

     

    I am very interested but I can't write anything on this device before the end of September when I can start testing on a project. I'll submit to your decision. Anyway if no one want this, I am ok to receive it image

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • clem57
    clem57 over 7 years ago in reply to balearicdynamics

    Same here. I am too busy to meet this when Azure Sphere is Sept 30 deadline. But that is the way things go. Hope this finds someone with more time.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to clem57

    I have read that the deadline with Azure has been extended one month ahead. At least this gives us some more breath. Anyway, today I got board 1 blinking and board 2 registered. Soon I will start blogging some first impressions, in the meantimem the challenge project is designing in my mind.

     

    Enrico