FPGA
  • Technologies
  • More
FPGA
Forum Improve Your Skills with a "Free" Minized Dev Board Project Contest
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 592 subscribers
  • Views 3728 views
  • Users 0 members are here
  • avnet
  • xilinx
Related

Improve Your Skills with a "Free" Minized Dev Board Project Contest

rscasny
rscasny over 7 years ago

There's something to be said for making something just for the sake of it. You can say that for learning as well. At some point in time, we all learn something for the pure enjoyment of learning. But let's flip the coin. On the other side is making or learning with an end goal in mind. Entrepreneurs are in this group; they make something to sell for profit. Other people learn something so they can do something; often times this boils down to winning a job, a contract, or be a member of the gig economy!image

 

Learn as if you were to live forever.

A famous man once said, "Learn as if you were to live forever." I was reminded of this old saying when I was given a Minized development board to giveaway for "free" to someone on the element14 community.image

 

A lightbulb illuminated above my head when it happened. I thought, "geez, this is a great opportunity to give a member the gift of learning."

 

Yes, I said...FREE.

 

So, what do you have to do to get a "free" Minized development board?

Enter in the comments section below how the Minized will help you learn and improve your skills. Tell me how receiving a Minized will challenge you and help you do something that you have been wanting to do for a long time. Tell me a little about your background and any experience you have with the technology that's packed into a Minized.

 

Are you new to the Minized? Well, here are the facts in a few sentences:image

The MiniZedTm is a single-core Zynq 7Z007S development board. This compact design features on-board connectivity through USB, Wi-Fi and Bluetooth. Peripherals can be plugged into dual Pmod-compatible connectors, the Arduino-compatible shield interface or the USB 2.0 host interface. JTAG circuitry is incorporated onto the MiniZed base board, so with a single micro- USB cable to your laptop you are already up and running. User LED’s, a button and a switch allow for a physical board interface.

 

Here's a few specs

  • Xilinx Zynq XC7Z007S SoC
  • Micron 512 MB DDR3L,128 Mb QSPI flash, 8GB eMMC
  • Murata Wi-Fi 802.11b/g/n
  • User button, switch, 2 x OSRAM bi-element LEDs
  • On-board USB to JTAG and debug UART circuit
  • Murata Bluetooth 4.1 plus EDR
  • USB 2.0 host (Microchip PHY), 2 x Pmod, Arduino interface
  • Dialog Semiconductor PMIC
  • ST Micro Accelerometer & Temperature sensor
  • ST Micro Digital MEMS microphone

 

Here's What You Get

  • Micro USB cable
  • MiniZed development board
  • Voucher for SDSoC license from Xilinx
  • TDM114 Camera Module, 1.26 Megapixel, Pmod, For ZED Development Kits
  • Sign in to reply
  • Cancel

Top Replies

  • mfetting
    mfetting over 7 years ago +4
    Create a wind chime that transmits the XY position of its sail as a value to a receiving station. The receiving station (development board) converts the XY position to a midi value which in turn can be…
  • neuromodulator
    neuromodulator over 7 years ago +4
    Roughly 2 months ago I was given the chance to play for the first time with an FPGA board with the condition that I would have to blog about it. I gladly accepted and blogged about how to program the FPGA…
  • colporteur
    colporteur over 7 years ago +3
    I know, I don’t know, what I don’t know about the Minized is everything. I can accept the shortcoming or I can do something about it. I am far from the age of young and short of the years needed to be…
Parents
  • neuromodulator
    neuromodulator over 7 years ago

    Roughly 2 months ago I was given the chance to play for the first time with an FPGA board with the condition that I would have to blog about it. I gladly accepted and blogged about how to program the FPGA with Verilog (Learning Verilog with the Digilent Cmod S7). Even though FPGAs are quite flexible, there are many high level tasks that are better suited to microprocessors than FPGAs (the opposite is also true). So what solutions are there when one needs both technologies? One would be, to connect a microprocessor to an FPGA and have them work together, but the drawback is that communication may be slow, and PCB  space and power requirements high. A different alternative would be to use "softcores", which are softprocessors, or FPGA processor designs; this could eventually solve previously mentioned issues, but also introduce new ones: softcores consume FPGA fabric (which is expensive), and their computational performance is not on par to hardprocessors. A different approach would be to use a microprocessor and an FPGA integrated into a single package, like the Xilinx Zynq, which integrates a Cortex-A microprocessor and an FPGA. Zynqs more or less solves all previously mentioned issues, but again introduce news too, like the high price tag, and high programming complexity. As always in the end the best solution depends on the problem that needs to be solved.

     

    In my Cmod S7 blog, I showed a sneak-peek of what I'm currently working on, its a computer graphics project, which I plan to use to participate in the latest project14 (Vision Thing). My plan is to design a simple FPGA GPU that would be used/controlled by a microprocessor who would do all the high level operations. Although I haven't got to this point in the development, its very likely that the slow communication between the microprocessor and the FPGA could severely limit what can be done with this approach. I believe that a better approach would be to use a Zynq, as it would allow me to communicate much faster to the FPGA GPU (there is a reason CPUs have always required a very fat communication pipe to the GPUs).

     

    I would love to have the chance to experiment with a Zynq board and learn how make the microprocessor and programmable logic work together.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neuromodulator
    neuromodulator over 7 years ago

    Roughly 2 months ago I was given the chance to play for the first time with an FPGA board with the condition that I would have to blog about it. I gladly accepted and blogged about how to program the FPGA with Verilog (Learning Verilog with the Digilent Cmod S7). Even though FPGAs are quite flexible, there are many high level tasks that are better suited to microprocessors than FPGAs (the opposite is also true). So what solutions are there when one needs both technologies? One would be, to connect a microprocessor to an FPGA and have them work together, but the drawback is that communication may be slow, and PCB  space and power requirements high. A different alternative would be to use "softcores", which are softprocessors, or FPGA processor designs; this could eventually solve previously mentioned issues, but also introduce new ones: softcores consume FPGA fabric (which is expensive), and their computational performance is not on par to hardprocessors. A different approach would be to use a microprocessor and an FPGA integrated into a single package, like the Xilinx Zynq, which integrates a Cortex-A microprocessor and an FPGA. Zynqs more or less solves all previously mentioned issues, but again introduce news too, like the high price tag, and high programming complexity. As always in the end the best solution depends on the problem that needs to be solved.

     

    In my Cmod S7 blog, I showed a sneak-peek of what I'm currently working on, its a computer graphics project, which I plan to use to participate in the latest project14 (Vision Thing). My plan is to design a simple FPGA GPU that would be used/controlled by a microprocessor who would do all the high level operations. Although I haven't got to this point in the development, its very likely that the slow communication between the microprocessor and the FPGA could severely limit what can be done with this approach. I believe that a better approach would be to use a Zynq, as it would allow me to communicate much faster to the FPGA GPU (there is a reason CPUs have always required a very fat communication pipe to the GPUs).

     

    I would love to have the chance to experiment with a Zynq board and learn how make the microprocessor and programmable logic work together.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 7 years ago in reply to neuromodulator

    I like your idea here. May I can suggest a few general things. Here goes

    • When I design a project, I employ a divide and conquer plan. Your computer graphics idea can benefit too. First deal with getting raw data efficiently enough.
    • Next reduce the data as soon as possible. Most of what you handle is noise with little value for the end goals. Eliminate that. Be sure to craft the goal(s) within this framework.
    • Speaking of goals, be specific and not too broad. The goals need sharpness of vision( no pun intended). What I mean is try not solve every problem. This creates drift in focus making the project harder to achieve.
    • And most important have fun. Remember the journey can be the driver not the goal post.

    I hope this helps you. If you get stuck, there are many talented individuals on this community. Sorry if I pontificate too much.

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neuromodulator
    neuromodulator over 7 years ago in reply to clem57

    Thank you for your suggestions, I didn't want to get into too much details of the inplementation because it would make the project blog much less interesting. The project is far more specific than what it appeared in the previous post. Its not going to be a full blown general purpose GPU, but one with very tight functionalitt, t's going to be more or less a proof of concept. I have in the past programmed a few graphic engines using different techniques so that side of the project shouldn't give me any difficulty. The aspect I know the least and that I'm more interested in learning is how to have the PS communicate with he PL. The reason I want to do CG is because I've always enjoyed it,  the CG engine I'm thinking about would use a different technology (vector graphics for a vector display), than what I've done before. Since its a simple but non-trivial project it will allow me to experiment with PS-PL communication in a more realistic setting. About the divide and conquer, yeah that's always a good plan for any kind of development. And about data communication, you are right, and I'm aware it could be a bottleneck, but maybe not, so I'll have to test that. Complex optimizations too soon are usually not a good idea, so I'll first see how it works without any. And yeah, I definetely plan to have fun with the project, I've so far had a great time playing with my Spartan 7 and a Zynq would be a great upgrade that would allow to increase my knowledge and learn how to use PS and PL on a single package.

    • Cancel
    • Vote Up +3 Vote Down