FPGA
  • Technologies
  • More
FPGA
Forum Is there an FPGA that you don't need a computer engineering degree just to get a light to blink?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 584 subscribers
  • Views 3850 views
  • Users 0 members are here
Related

Is there an FPGA that you don't need a computer engineering degree just to get a light to blink?

e14 Contributor
e14 Contributor over 10 years ago

I have an Altera CPLD, Altera DE0-Nano-SoC, and a xilinx mojo v3.

the CPLD is the only I could get working with a lot of stupid usb drive hoops to jump through.

 

Does anyone make a board with good documentation on installation and troubleshooting.

I feel like Altera and Xilinx don't care about the maker community but want our money without putting any effort out on there part.

 

David

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +2
    Hi David, Which area are you specifically concerned about, the development software (toolchain), or the software that will push the final synthesized design into the board? Regardless of the board, you…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Jan Cumps +2
    I am trying to build a computer from first principals, a hardware version of NAND2Tetris The Elements of Computing Systems / Nisan & Schocken
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps +2
    I've filmed my first endeavours - warning: I had no knowledge at all when filming this, so it's really from a starters point of view. Only the last video is an own design (with most code blatantly stolen…
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    I haven't used the Mojo V3 board myself.  Its maker Embedded Micro has tutorials and a forum.  I'd recommend trying the tutorials and checking the forum if you get stuck.

     

    Unfortunately, there's a steep learning curve with all the FPGAs if you're using vendor tools.  With each release the curve gets worse.  If you've been designing with a vendor's parts for a long time, you don't really notice it that much since each release only makes incremental changes.  However, if you're just starting out you're trying to drink from a firehose and it's pretty brutal.  See the discussion: Barriers to designing with FPGAs?

     

    Altera and Xilinx are interesting in selling you huge quantities of reasonably-priced chips or medium quantities of very expensive chips.  If you're just a maker they're not going to give you individual help, though you can get useful information from the Xilinx community forum.  So your best bet is the tutorials and forum of whoever makes your board.

     

    I like Gadget Factory and their Papilio boards.  They have a very helpful forum.  However, you're still going to have to install and learn to use Xilinx ISE.  Plus the Xilinx Spartan-6 on the Mojo and Papilio DUO is a very complex beast.  So you're liable to get strange error messages and warnings.

     

    I really like the Lattice iCE40 as a simple chip for new users.  This is the only FPGA I know of that has open-source design tools (IceStorm).  They are quite simple to use, but a bit of a pain to install.  I use them on Ubuntu GNU/Linux.  I don't know whether they've been installed successfully on Windows.  People who care about open-source software usually have a GNU/Linux machine handy.

     

    I've backed a nice iCE40 board called Nandland Go Board which is designed for new users.  Its creator's site has some nice tutorials.  I expect to get my board by the end of March 2016.

     

    If you stick with it, FPGAs can do amazing things that you simply cannot do with a CPU.  Here's my "elevator speech" on why someone would want to learn FPGAs:

    Have you ever wanted a custom digital chip for a project, but didn't have $1 million lying around to pay for fabricating it?   Well, an FPGA lets you do it for tens of dollars.

    Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem

    It is The "They are quite simple to use, but a bit of a pain to install." I have an issue and where I call out both Altera and Xilinx for not supporting the community because It is left to the community to make videos like :https://www.youtube.com/watch?v=wF9vlO-ah-A

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to e14 Contributor

    I didn't have issues getting the toolchain for Xilinx and Papilio running. And hamsternz has a getting started guide that I like very much.

     

    I have a harder time stepping up from where that tutorial ends though image .
    I'm not that used anymore to think in digital hardware terms. The brain turned a little bit lazy now that I use a microcontroller as the hammer to hit any digital nail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Jan Cumps

    I am trying to build a computer from first principals, a hardware version of NAND2Tetris The Elements of Computing Systems / Nisan & Schocken

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to e14 Contributor

    That's definitely more advanced than blinking the proverbial led.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    I like the idea, but you may come up short because it it much simpler to simulate hardware than to build the real thing.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    I have a copy of that book, and found it only slightly useful, and would definitely not be a book for building a computer with an FPGA. I think it would be difficult to use such a book for your aim (despite the extended title of the book being "Building a Modern Computer System from First Principles") . HDL is relegated to a tiny appendix in the book, and the book is intended for computer science (and for a really tiny fraction of a CS course at best), not for hardware designers (an FPGA needs hardware design knowledge). It simply isn't possible to use a computer science or a software program approach (as detailed in the book) to design a computer in an FPGA.

    I can't suggest a specific book on building a computer in an FPGA. Usually there are books on computer architecture, and there are books on HDL, and there are books on digital design. You might find online fpga computer projects to do what you approximately want, but they may not be documented well either unfortunately.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • peterjcs23
    peterjcs23 over 10 years ago in reply to e14 Contributor

    If you want the challenge of a low level design based on registers and an ALU, you could do a lot worse than to base your design on a simple early device like the AMD AM2900 bit-slice. It has a straightforward microprogramming structure that would be easy to emulate in an FPGA. Take a look at this:

    http://bitsavers.informatik.uni-stuttgart.de/pdf/amd/ED2900A_vol1_Jan85.pdf

     

    Also I know that the Intel 8051 has a simple structure for a microcontroller and has been implemented in FPGAs. You can buy it as a core for example:

    8051 IP Core » Oregano Systems

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to e14 Contributor

    David shorey wrote:

     

    It is The "They are quite simple to use, but a bit of a pain to install." I have an issue and where I call out both Altera and Xilinx for not supporting the community because It is left to the community to make videos like :https://www.youtube.com/watch?v=wF9vlO-ah-A

    When I said "They are quite simple to use, but a bit of a pain to install" I was referring to the IceStorm tools (yosys, arachne-pnr, iceprog).  They're all command line tools, so you don't have to grok a big complex IDE that's "like flying a jet airliner with 100,000 switches".  The Xilinx suite is a pain to install and complex to use.  I haven't used Altera this century and I haven't used Lattice's tools, but I read user reports that both are PITAs.  I have used MicroSemi (previously Actel) and find it worse that Xilinx.

     

    I haven't used Altera since the 20th Century, but it actually went pretty well.  Altera had their own HDL called AHDL which was a lot easier to grok than VHDL or Verilog because AHDL was closer to the hardware.  That is, it was a hardware description language rather than a behavior description language, and designed specifically for synthesis rather than for simulation.

     

    Regarding LEDs and switches and pins: do look at the schematics and other documentation for your FPGA development boards.  Make sure you can tell whether switches and LEDs are active-high or active-low.  When I started in this business it was all variants of TTL so all switches and LEDs were active-low.  Modern CMOS outputs usually have the same drive for pull-up and pull-down, so the board may be either.

     

    You board may or may not have external pull-up or pull-down resistors for switches.  If it doesn't, you probably need to enable internal FPGA pull-up or pull-down circuits.  Be sure your FPGA inputs don't have pull-up/down circuits that conflict with external pull-up/down resistors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to johnbeetem

    John Beetem wrote:

    ...

    The Xilinx suite is a pain to install and complex to use.

    ...

    Different opinion warning image

    They installed smooth for me (I'm using ISE because I have a Spartan 6). And the IDE isn't that complex I think. At least, I don't have too much trouble doing work with it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to Jan Cumps

    Jan Cumps wrote:


    They installed smooth for me (I'm using ISE because I have a Spartan 6). And the IDE isn't that complex I think. At least, I don't have too much trouble doing work with it.

    Glad to hear it went well for you.  Did you have previous experience with FPGA design and FPGA tools?  I've read lots of comments over the years from new FPGA users who are terribly frustrated.  A big problem with FPGAs is that there are dozens of small details you have to get right and if you don't the FPGA doesn't load and you have no idea which of the details are right or wrong, and in some case don't know that a crucial detail even exists (like the Xilinx start-up clock).

     

    Advice to new users:  IMO your best bet is to follow a detailed tutorial for your FPGA board step by step.  Always start with a ludicrously simple example like controlling an LED with a push button.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to johnbeetem

    John Beetem wrote:

     

    ...

     

    Glad to hear it went well for you.  Did you have previous experience with FPGA design and FPGA tools?  I've read lots of comments over the years from new FPGA users who are terribly frustrated.  A big problem with FPGAs is that there are dozens of small details you have to get right and if you don't the FPGA doesn't load and you have no idea which of the details are right or wrong, and in some case don't know that a crucial detail even exists (like the Xilinx start-up clock).

     

    ...

     

    It was (and is) my first experience. Because it was all so new, I kept with the guide of hamster_nz until I got the concept of FPGAs and VHDL.

    If you follow that, you get the concepts of writing and synthetising a design. He also teaches you how to create the simulation part, and how to execute and interprete it. How to interprete the timing reports and how to set timing constraints.

    The tutorial got me up to a level good enough to look around for examples, understand them and integrate them in a design.

    I'm still a bit weak to write a more-than-basic design myself, but I'm working on that.

     

    John Beetem wrote:

     

    ...

     

    Advice to new users:  IMO your best bet is to follow a detailed tutorial for your FPGA board step by step.  Always start with a ludicrously simple example like controlling an LED with a push button.

     

    ...

     

    Yes! My first lesson was a LED. Then a button, Then doing AND/OR/... logic with multiple buttons,

    Then a running light with multiple LEDs and a clock, etc...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to johnbeetem

    John Beetem wrote:

     

    ...

     

    Glad to hear it went well for you.  Did you have previous experience with FPGA design and FPGA tools?  I've read lots of comments over the years from new FPGA users who are terribly frustrated.  A big problem with FPGAs is that there are dozens of small details you have to get right and if you don't the FPGA doesn't load and you have no idea which of the details are right or wrong, and in some case don't know that a crucial detail even exists (like the Xilinx start-up clock).

     

    ...

     

    It was (and is) my first experience. Because it was all so new, I kept with the guide of hamster_nz until I got the concept of FPGAs and VHDL.

    If you follow that, you get the concepts of writing and synthetising a design. He also teaches you how to create the simulation part, and how to execute and interprete it. How to interprete the timing reports and how to set timing constraints.

    The tutorial got me up to a level good enough to look around for examples, understand them and integrate them in a design.

    I'm still a bit weak to write a more-than-basic design myself, but I'm working on that.

     

    John Beetem wrote:

     

    ...

     

    Advice to new users:  IMO your best bet is to follow a detailed tutorial for your FPGA board step by step.  Always start with a ludicrously simple example like controlling an LED with a push button.

     

    ...

     

    Yes! My first lesson was a LED. Then a button, Then doing AND/OR/... logic with multiple buttons,

    Then a running light with multiple LEDs and a clock, etc...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    I've filmed my first endeavours - warning: I had no knowledge at all when filming this, so it's really from a starters point of view.

    Only the last video is an own design (with most code blatantly stolen from the web anyway image )

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.