FPGA
  • Technologies
  • More
FPGA
Forum Trigger pulse generation inside FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 583 subscribers
  • Views 2726 views
  • Users 0 members are here
  • trigger
  • cyclone
  • fpga
  • altera
  • 4
Related

Trigger pulse generation inside FPGA

Kilohercas
Kilohercas over 12 years ago

Hello, i am facing small problem with FPGA programming.

 

Problem is simple, i have unknown length trigger pulse (1ns-5us) that should start CCD readout. What i need is to be able to make that signal as short as possible, so i don't waste clock cycles to start readout. Ideally i should be able to control how long this signal are, new pulse must start at rising edge of trigger pulse, falling edge is ignored, and new falling edge is generated automatically, when x ns had passed from rising edge ( i could do that with 555 timer, but it's is too slow, and it would be nice to use Altera Cyclone 4 EP4CE6E17C6 for that.

 

image

 

This circuit is working very well, only problem is that if trigger is very long, i will miss clock cycles to start readout, and it will be delayed as long TRIGGER is high level. That's why i need to generate falling edge as fast as i can, but at the same time that fpga could catch it.If some one could help me with verliog code for trigger generator i would be very grateful, or any idea would be nice. Note that external trigger is not running on same oscillator, so it is fully asynchronous to fpga

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    Linas, if I understand correctly, you have an asynchronous pulse which you are feeding directly into 'aclr' which I guess is a synchronous block of logic. The trigger pulse amy be as short as 1ns. The first issue is that this pulse is almost certainly too short to reliably clear anyhting in the FPGA and if it is asynchronous to the ELIS_SK clock it will not reliably meet timing even if it is long enough - sometimes bad things will happen when the trigger arrives at just the wrong time relative to the clock.

    I think you need to stretch your trigger pulse in hardware to be at least 1 clock cycle long. Thn you need to synchronise it to the internal FPGA clock by passing though at least 2 flip flops, then you can detect the rising or falling edges reliably and do the clearing. You will get  a delay of three clock cycles but this can't be avoided with an FPGA. It may be possible to condition the trigger pulse in some other way or to use a PLL on the FPGA to generate a faster internal clock to synch the trigger pulse .

     

    Sorry, can't offer you any Verilog code because I use VHDL and my Verilog is too primitive to expsoe to the world.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 12 years ago

    Linas, if I understand correctly, you have an asynchronous pulse which you are feeding directly into 'aclr' which I guess is a synchronous block of logic. The trigger pulse amy be as short as 1ns. The first issue is that this pulse is almost certainly too short to reliably clear anyhting in the FPGA and if it is asynchronous to the ELIS_SK clock it will not reliably meet timing even if it is long enough - sometimes bad things will happen when the trigger arrives at just the wrong time relative to the clock.

    I think you need to stretch your trigger pulse in hardware to be at least 1 clock cycle long. Thn you need to synchronise it to the internal FPGA clock by passing though at least 2 flip flops, then you can detect the rising or falling edges reliably and do the clearing. You will get  a delay of three clock cycles but this can't be avoided with an FPGA. It may be possible to condition the trigger pulse in some other way or to use a PLL on the FPGA to generate a faster internal clock to synch the trigger pulse .

     

    Sorry, can't offer you any Verilog code because I use VHDL and my Verilog is too primitive to expsoe to the world.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Kilohercas
    Kilohercas over 12 years ago in reply to michaelkellett

    Clear is asynchronous to Counter, right now i am using 10ns pulse from DSP to clear it, and it works very well. This will work if clear pulse is picked by logic, that would clear counter, all other circuit will work without a problem, even if i have massive jitter compared to FPGA clock, which i will have.

     

    i was using compare if ELIS_SK counted to 129, that would mean that i have all data clocked out, and i had other counter to count triggers, if it counts to 1, i will let ELIS_SK to count, when it finishes, i will count finishing edge, and if it's not 1, i will not let it count. in theory it should work , but it had glitches upon glitches. Idea was the same like shoot yourself, you should be able to do that, problem is that FPGA is so fast, when it tries to reset counter it see that counter is reseted, and stop reseting, generating 1ns pulse, and logic is not capable to latch on it image