FPGA
  • Technologies
  • More
FPGA
Forum Trigger pulse generation inside FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 583 subscribers
  • Views 2724 views
  • Users 0 members are here
  • trigger
  • cyclone
  • fpga
  • altera
  • 4
Related

Trigger pulse generation inside FPGA

Kilohercas
Kilohercas over 12 years ago

Hello, i am facing small problem with FPGA programming.

 

Problem is simple, i have unknown length trigger pulse (1ns-5us) that should start CCD readout. What i need is to be able to make that signal as short as possible, so i don't waste clock cycles to start readout. Ideally i should be able to control how long this signal are, new pulse must start at rising edge of trigger pulse, falling edge is ignored, and new falling edge is generated automatically, when x ns had passed from rising edge ( i could do that with 555 timer, but it's is too slow, and it would be nice to use Altera Cyclone 4 EP4CE6E17C6 for that.

 

image

 

This circuit is working very well, only problem is that if trigger is very long, i will miss clock cycles to start readout, and it will be delayed as long TRIGGER is high level. That's why i need to generate falling edge as fast as i can, but at the same time that fpga could catch it.If some one could help me with verliog code for trigger generator i would be very grateful, or any idea would be nice. Note that external trigger is not running on same oscillator, so it is fully asynchronous to fpga

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    I think this might work:

     

    wire clk;    // Master clock.
    wire pulse;  // Pulse sets FF.
    reg  PFF;    // Pulse storage FF: async set when "pulse" occurs,
                 // sync reset when pulse goes away.
    reg  pulse1, pulse2;    // Resynchronized versions of "pulse".
    reg  PFF1, PFF2, PFF3;  // Resynchronized versions of PFF.
    // Detect rising edge of PFF.  This clears your counter.
    wire edge = PFF2 && !PFF3;

     

    always @(posedge clk or posedge pulse)
    if (pulse) PFF <= 1; else begin
        pulse1 <= pulse; pulse2 <= pulse1;        // Resynchronize pulse to clk.
        PFF1 <= PFF; PFF2 <= PFF1; PFF3 <= PFF2;  // Resynchronize PFF to clk.
        // "pulse" sets PFF asynchronously.  Hold PFF high until PFF3 is set,
        // and keep holding it until pulse goes away.
        // A short pulse sets PFF and PFF3 clears it.
        // A long pulse sets PFF but doesn't clear it until pulse2 goes away.
        PFF <= PFF && !(PFF3 && !pulse2);
    end

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to johnbeetem

    Here's a better version.  I've changed PFF's clocked update so it only occurs when PFF3 is high, i.e., PFF was set several cycles ago.  "PFF <= PFF && !(PFF3 && !pulse2);" has a hazard if a short pulse occurs when clk rises.

     

    wire clk;    // Master clock.
    wire pulse;  // Pulse sets FF.
    reg  PFF;    // Pulse storage FF: async set when "pulse" occurs,
                 // sync reset when pulse goes away.
    reg  pulse1, pulse2;    // Resynchronized versions of "pulse".
    reg  PFF1, PFF2, PFF3;  // Resynchronized versions of PFF.
    // Detect rising edge of PFF.  This clears your counter.
    wire edge = PFF2 && !PFF3;

     

    always @(posedge clk or posedge pulse)
    if (pulse) PFF <= 1; else begin
        pulse1 <= pulse; pulse2 <= pulse1;        // Resynchronize pulse to clk.
        PFF1 <= PFF; PFF2 <= PFF1; PFF3 <= PFF2;  // Resynchronize PFF to clk.
        // "pulse" sets PFF asynchronously.  Hold PFF high until PFF3 is set,
        // and keep holding it until pulse goes away.
        // A short pulse sets PFF and PFF3 clears it.
        // A long pulse sets PFF but doesn't clear it until pulse2 goes away.
       // This version disables the PFF clock until PFF3, which is sync'd to clk.
        // PFF clears when pulse2 (also sync'd to clk) goes away.
        if (PFF3) PFF <= PFF && pulse2;
    end

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to johnbeetem

    thank you, will try that soon and see how it goes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Kilohercas
    Kilohercas over 12 years ago in reply to johnbeetem

    thank you, will try that soon and see how it goes.