FPGA
  • Technologies
  • More
FPGA
Forum Project IceStorm: fully open-source FPGA tools for Lattice iCE40
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 583 subscribers
  • Views 26258 views
  • Users 0 members are here
  • floss
  • icestorm
  • fpga
  • ice40
  • yosys
Related

Project IceStorm: fully open-source FPGA tools for Lattice iCE40

johnbeetem
johnbeetem over 11 years ago

As some of you may have noticed, I've been obsessed for many decades with having open FPGA bitstream documentation so that people can write their own FPGA designs tools, especially FLOSS (Free-as-in-Liberty Open Source Software).

 

I recently found out about IceStorm, a project that has somehow reverse-engineered and documented the Lattice iCE40 FPGA.  They've actually put together a fully-open-source tool chain with Yosys for Verilog synthesis and Arachne_pnr for placement and routing.  I don't know how usable or robust the tools are.  I'm planning on taking a close look starting next month.

 

If you're interested, here's the IceStorm link, which has links to the other tools: Project IceStorm

Discussion of Yosys and the tools is at reddit: Yosys Open SYnthesis Suite

 

Update: Here are a couple of nice Hackaday items about IceStorm:

 

From 29 March 2015: Reverse Engineering Lattice’s iCE40 FPGA Bitstream | Hackaday

From 29 May 2015: An Open Source Toolchain For iCE40 FPGAs | Hackaday

 

Update 2: Here are some good IceStorm installation instructions: Projet IceStorm : le FPGA libéré ! | Front de Libération des FPGA.  They're in a combination of French and GNU/Linux.

 

Here's the Lattice IceStick directly supported by IceStorm: Lattice Semiconductor: ICE40HX1K-STICK-EVN iCEstick Evaluation Kit.  It's US$20.89 in the USA.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago +2
    I found out from a friend about another iCE40 board: Olimex iCE40HX1K-EVB It's a tiny board (5x5 cm or 2"x2") with an iCE40HX1K-VQ100, 256K x 16 SRAM, 16 Mb serial flash, 2 buttons, 2 LEDs, oscillator…
  • diablero
    diablero over 10 years ago in reply to johnbeetem +2
    A new board. Does the World Need an FPGA Arduino? | Hackaday
  • michaelkellett
    michaelkellett over 10 years ago in reply to johnbeetem +2
    My thinking was that if you are going to buy a board you could expect it to be made on a production line and almost any would be able to place BGAs. You can use one of Lattice's sparsely pinned BGAs on…
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    I'm amazed and impressed at the amount of effort going into this but for so little gain !

     

    Targeting the 1k part and no support for block ram or plls isn't really getting to the point where you could do any real design with the tools so the project has a very long way to go.

     

    From a personal point of view it's such a shame they are using Verilog 2005  - which is a pretty low base for an HDL.

     

    If it ever gets to the point of supporting the bigger iCE40 parts the packages will be a problem - some of the newer ones come in 0.5mm pitch BGA (or smaller if you like image).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    I'm amazed and impressed at the amount of effort going into this but for so little gain!

    I see IceStorm as a huge step in the right direction.  IMO the best way to get vendors to document their bitstreams is to have projects like IceStorm and my Flavia show that it's possible to use FLOSS tools and that there are advantages to doing so, both for users and vendors.  For example, Flavia is much faster than Xilinx tools for small designs, making it a better platform for teaching programmable logic concepts.  I'm hoping these projects will embarrass Xilinx and Altera into opening their bitstreams.

     

    I'm looking forward to playing with IceStorm.  While the iCE40 HX1K is indeed a small part, it's big enough for teaching about FPGAs and has a lot more capacity than any of my Flavia implementations.  So it looks like a good answer to morgaine's FPGA/CPLD education question: http://www.element14.com/community/thread/17692?start=56

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 11 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    I'm amazed and impressed at the amount of effort going into this but for so little gain!

    I see IceStorm as a huge step in the right direction.  IMO the best way to get vendors to document their bitstreams is to have projects like IceStorm and my Flavia show that it's possible to use FLOSS tools and that there are advantages to doing so, both for users and vendors.  For example, Flavia is much faster than Xilinx tools for small designs, making it a better platform for teaching programmable logic concepts.  I'm hoping these projects will embarrass Xilinx and Altera into opening their bitstreams.

     

    I'm looking forward to playing with IceStorm.  While the iCE40 HX1K is indeed a small part, it's big enough for teaching about FPGAs and has a lot more capacity than any of my Flavia implementations.  So it looks like a good answer to morgaine's FPGA/CPLD education question: http://www.element14.com/community/thread/17692?start=56