FPGA
  • Technologies
  • More
FPGA
Forum Neo Geo Pocket Color Video Out (DAC/FPGA)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 11 answers
  • Subscribers 583 subscribers
  • Views 5970 views
  • Users 0 members are here
  • retro gaming
  • dac
  • fpga
  • digital-to analog converter
  • video games
Related

Neo Geo Pocket Color Video Out (DAC/FPGA)

kragit
kragit over 9 years ago

Hi everyone!

 

Looking to achieve RGB analog video out on a Neo Geo Pocket Color. No known mods currently exist for this. There are single digit K2_VIDEOs out in the wild that achieve this, but I believe these were made by SNK themselves for internal use only. Other people have apparently gotten video out with FPGAs, but no one has publicly documented it.

 

Here are the LCD signals as printed on the board & additional information from someone who's apparently achieved this:

 

I've done it with a small FPGA. The LCD signals can't be simpler: R0~3 is 4bit red, G0~3 is 4bit green, B0~3 is 4bit blue, DOTCLK is the pixel clock, SPL is horizontal sync, SPS is frame sync.
[...]
It can't be done by just wiring a scart cable to the board, you have to buffer and convert the color data from the NGPC, then do digital to analog conversion if you want analog RGB output.

 

I'm venturing into the FPGA scene for this with no past experience with FPGAs and a rudimentary understanding of digital electronics (I can follow guides, solder, etc. I built a CMVS this way).

 

Any help would be appreciated. Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 9 years ago in reply to kragit +4 suggested
    Adam Kragt wrote: Appreciate the info! The biggest thing is just trying to figure out where to start as a total beginner. With FPGAs, start by copying a tutorial design exactly. FPGA tools have a steep…
  • jc2048
    jc2048 over 9 years ago +3 suggested
    You might consider applying for this roadtest https://www.element14.com/community/roadTests/1796/l/Terasic-P0082-DE0-Nano-FPGA-Development-Kit That would get you some kit to use and an opportunity to learn…
  • johnbeetem
    johnbeetem over 9 years ago +3 suggested
    These are general comments about FPGAs and VGA output and probably not all that helpful for the NPGC, but here goes anyway. There are a number of FPGA boards out there that support VGA graphics, and some…
Parents
  • johnbeetem
    0 johnbeetem over 9 years ago

    These are general comments about FPGAs and VGA output and probably not all that helpful for the NPGC, but here goes anyway.

     

    There are a number of FPGA boards out there that support VGA graphics, and some have tutorials available.  Gadget Factory's Papilio boards are very nice and have a VGA "wing".  It's not clear whether it's 8 or 64 colors.  The older through-hole version has 8 colors, but the photo of the SMT version at the link has enough resistors to do 64.  They both use resistors to make a "poor man's" DAC, which can probably get you up to 4 bits per color.  There's sample code around to generate VGA output -- I think it's VHDL.  (I like Verilog better.)

     

    The LOGI-PI and LOGI-Bone boards have a pretty powerful FPGA and you can get a LOGI-Edu adapter with VGA output (512 colors, I think).  The boards can be used stand-alone but you need an external programmer.

     

    Another nifty board is the Nandland Go Board, which has built-in VGA.  The FPGA on that board is pretty small, but it has the advantage that you can use open-source tools instead of the far more complex vendor tools.  The Go Board doesn't have much RAM -- just the small amount in the FPGA itself -- so it's probably no good for your NPGC project.

     

    I don't know what availability is these days for these boards.  I haven't done VGA output myself.  I plan to one of these days, since I have all those boards.  Just need more time!

     

    Hope this helps and/or inspires.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 9 years ago in reply to johnbeetem

    I'm a dunderhead! Thanks for pointing that out - I should have realised that there would be boards out there that could already do this; FPGAs and VGA are a very natural fit.

     

    The Papilo board has an 'Arcade Megawing' available that has 4-bit per colour.

     

    http://papilio.cc/index.php?n=Papilio.ArcadeMegaWing

     

    The method is the same as on the Nandland Go board - a cheap and cheerful (pseudo) current-mode DAC, with the currents summed by the termination resistor at the other end of the cable. Presumably, the output pins are set permanently high and then turned on and off with the tristate. Given that the VGA interface can be so simple - just a bunch of resistors and a connector (which you could do by just 'bird's nesting' the resistors between the connector and the header for the IO pins) - it would make for a possible proposal for the roadtest coming up. Generating some colour bars as a test card on the screen would then just be a matter of implementing some counters and a bit of decoding in the FPGA and it would show off the board's potential as a development platform quite nicely.

     

    With your experience, you'd be able to throw together something basic in a hour or two. Perhaps you could find the time - it would be a nice FPGA project to have here on e14.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    The Xess XuLA2 has an example (for VGA for its a plug-in board with the resistors DAC and vga connector)

    image

    The VHDL code is published on github.

     

    I have that VGA plug-in. I haven't tested it yet.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Jan Cumps

    If anyone in the road test decides to build a VGA implementation, I'll try to play along.

    Not in the roadtest area itself - I'm using a Xilinx FPGA and the roadtest is an Altera initiative.

    Maybe in the FPGA group here on e14...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Jan Cumps

    I've been playing with the VGA project.

    I don't have a video cable handy at the moment. As a test I've probed the HSYNC and VSYNC.

    image

     

    image

     

    HSYNC and Green 4:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 9 years ago in reply to Jan Cumps

    Very good. The HSYNCs look overly wide to me and there's no blanking at the end of the line, but you can fiddle around with all that once you see it on the screen. What next? Asteroids in VHDL would be impressive!

     

    And it's a chance to show off your new scope. Which model is it? Should I be envious?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048
    The HSYNCs look overly wide to me and there's no blanking at the end of the line

    I'll have to read-up on the VGA signal, but I believe there should be blanking.

    From the Xess doco:

    image

     

    And it's a chance to show off your new scope. Which model is it? Should I be envious?

    Yay Tektronix  TBS2102TBS2102 100 MHz 2 channel Yes please

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    Jon Clift wrote:

     

    ... there's no blanking at the end of the line ...

    Yes, I'll have to recheck the design:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    Jon Clift wrote:

     

    ... there's no blanking at the end of the line ...

    Yes, I'll have to recheck the design:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Jan Cumps

    I have now loaded a real image to RAM, and it looks ok now (edit: no I see the blackout for vsync but not yet for hsync end)

     

    Yellow: horizontal sync

    Blue: vertical sync

    Magenta: one of the video signals

     

    The capture below is triggered on the vertical sync, and shows blanking before and after.

    image

     

    This one shows the same signals, zoomed out to show multiple vsyncs:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 9 years ago in reply to Jan Cumps

    From the scope timing it looks like 600 displayed lines and a framerate of 70Hz. (Presumably, there are going to be 800 pixels across the line.)

     

    That doesn't tie up with the documentation you showed above which was a 480 line 60Hz mode.

     

    Have you found a VGA cable yet? I won't believe it until I see it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    I'm going to buy a cable on the second hand market in Brussels Marollen this Sunday.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    ... Yes, all samples are 800 x 600

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    ahead of plan image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Jan Cumps

    ... and then it turns out that my brand new flashy tv doesn't have VGA image

    I have a HDVD HDMI  -> VGA converter but it doesn't work the other way. Darn...