FPGA
  • Technologies
  • More
FPGA
Forum Looking for the right FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 582 subscribers
  • Views 755 views
  • Users 0 members are here
  • mos
  • commodore
  • fpga
  • 6526
  • vhdl
  • commodore_64
  • fpga developement
Related

Looking for the right FPGA

ajkatz83
ajkatz83 over 8 years ago

 

Hey all!

 

Been working a bit in the 8-bit world, especially with the Commodore machines, the 64 and SX-64 and I have noticed there have been some folks out there who have replaced some of the chips with FGPAs. I know I am crazy for thinking this, however, I am curious to see if that can be done. I have never used an FPGA nor VHDL, which seems to be the machine language necessary to make this all work. I was using my one machine the other day and the CIA (complex Interface Adapter) basically blew up and stripped me of the two I had for "just in case." I saw one fellow trying to do such a project more than a year ago, and I feel rather inspired.

 

For the specs below (off the datasheet) What kind of FPGA would be necessary?

 

FEATURES · 16 Individually programmable I/O lines · 8 or 16-Bit handshaking on read or write · 2 independent, linkable 16-bit interval timers · 24-hour (AM/PM) time of day clock with programmable alarm · 8-Bit shift register for serial I/O · 2TTL Load capability · CMOS compatible I/O lines · 1 MHz operation

 

ANd if there is a specific FPGA that meets all this, is there a VHDL development software that's free or do you buy it with said FPGA?

 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago +4 suggested
    You could fairly easily use an FPGA to make a plug compatible 6526 part except for the 5V working. Modern FPGAs don't support 5V IO and the CMOS type parts in small packages don't. There are a few 5V working…
  • johnbeetem
    johnbeetem over 8 years ago +3 suggested
    You might look into the original Xilinx Spartan II (not the IIE). The Spartan II is a 2.5 V internal device with 5V tolerant I/Os if you use 3.3V LVTTL standard. It's an old family but some parts are still…
Parents
  • ajkatz83
    0 ajkatz83 over 8 years ago

    Thanks guys this really does help a lot! I have never undertaken a project like this before but have been curious about FPGAs for a while.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ajkatz83
    0 ajkatz83 over 8 years ago

    Thanks guys this really does help a lot! I have never undertaken a project like this before but have been curious about FPGAs for a while.