FPGA
  • Technologies
  • More
FPGA
Forum Where to start for an easy intro to FPGAs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 18 answers
  • Subscribers 590 subscribers
  • Views 8054 views
  • Users 0 members are here
Related

Where to start for an easy intro to FPGAs?

Fred27
Fred27 over 8 years ago

I'm sure this is one of those questions that is going to have more opinion that definitive answer, but I'm going to ask it anyway. I've not done anything with FPGAs. I know what they are and what they can do. I know that they're a bit of a shift in mindset for someone who's used to coding for a microcontroller. I'm at the same stage that I'm sure many people are. I want to find out if FPGAs are the sort of thing that I want to get into or not. To dip my toe in the water so to speak.

 

The trouble is there are a lot of manufacturers who seem to have their own tool chains and programming approaches. It's tricky picking one to start with. There are road tests of a few on here but to be honest they all sound hard and are difficult to compare. Has anyone got advice on where to start? I suppose my priorities are:

 

  • Once I pick a manufacturer I want to stick with it. Jumping from one to another will just make it harder.
  • It would be hopefully easy to get the basics. I don't need raw power right now. Being able to create a microcontroller core is great, but will only confuse me at this stage.
  • The option of a SoC alongside a microcontroller would be a nice option for later, but once again I don't need it right now.
  • Reasonably cheap. It doesn't have to be the cheapest, but this may be a dead end experience so I'd prefer 10s rather than 100s of £/$.

 

Right now I was thinking of waiting see how the pans out for those selected, and to learn from their experience. However, any opinions are welcome

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +8 suggested
    David, You might want to look at CPLD's first. They are very much the same as FPGA, but smaller (#gates and #pins). They are typically programmed with the same tools and languages as FPGAs. I started with…
  • michaelkellett
    michaelkellett over 8 years ago +8 suggested
    If you want to learn about FPGAs then don't mess with CPLDs. The CoolRunners are ancient (15 year old designs). There are 4 major players in the FPGA business, Xilinx, Intel (was Altera), Lattice and Microsemi…
  • michaelkellett
    michaelkellett over 8 years ago in reply to neuromodulator +8 suggested
    Lots of interesting points - I'm off on a long weekend hol so not enough time to cover them all but I'll have a go. There are two primary HDL (Hardware Definition Languages), Verilog and VHDL. They both…
Parents
  • neuromodulator
    0 neuromodulator over 8 years ago

    I've also wanted to learn FPGA programming but I've found it to be kinda hard as there doesn't seem to be an agreed on good way to learn how to program them. I've found many tutorials in the net that teach VHDL/Verilog, but I feel like they give examples, show results, but don't explain any further. In the end I feel like they teach HDL recipes more than teaching how the HDL actually gets synthesized into the logic design. There have been a lot of FPGA roadtests, but I've felt a bit intimidated to apply to a roadtest as I'm not sure I would be able to deliver it in-time. On the other side I've seen that most FPGA roadtesters appear to dodge the HDL completly, and stick to the visual programming languages or soft/hard CPU programming in their reviews.

     

    I have also many questions about FPGAs, so I'll add a few myself in case any of the experts wants to answer them:

     

    - There appear to be many different languages that can be used on FPGA, besides the HDL, what is each of the languages good for? When should I use one language in opposition to another one?

    - When it comes to HDL, I've read that code could synthesise for one FPGA and not synthesise for another one, how hard is it to make HDL portable? Would programming in portable HDL make it inefficient to the point that its not worth the hassle?

    - I keep reading that tools are very complex and all that, I don't really understand how a tool could make such a great difference when the HDL is not tool dependent (or is it?). Could someone elaborate on that? (as an analogy, learning a computer language is what is hard, switching between IDEs is quite straightforward as much as you keep the same language. Why is it so different with FPGAs?)

    - What are FPGAs actually good at? What kind of tasks are FPGA the only good alternative? It appears to me that they are mostly good at I/O stuff (multiple or fast DACs, ADCs). I've seen some claims on FPGAs being good at some computational tasks, but I've also seen some others claiming that they are not that great anymore.

    - How hard is it to debug them? I've read some claims about debugging timing issues being super hard and requiring an excessive amount of time and patience. Considering that time is money, one would leave the FPGAs as a last resort alternative, as it could increase the product development time considerably if it is that slow to program and debug them.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to neuromodulator

    Lots of interesting points - I'm off on a long weekend hol so not enough time to cover them all but I'll have a go.

     

    There are two primary HDL (Hardware Definition Languages), Verilog and VHDL. They both come in different versions, there are fewer versions of VHDL than of Verilog. The latest versions of Verilog and VHDL both contain many features that synthesizers are unable to deal with. This is one reason why HDL "code" may be non-portable.

    Once you start using an HDL to target an FPGA you may want to use the special features of the FPGA like on chip RAM blocks, PLLs, DDRAM interface hardware etc etc. These are all different for different FPGAs and once your project uses them it becomes specific to that FPGA type.

    Many people use the FPGA vendors toolset including HDL editor, compiler, simulator,  synthesizer, timing checking, fitter, programmer and debugger.

    As you move up the food chain you'll find more use of separate tools, I use Aldec HDL for design and simulation, this makes it a bit easier to port designs from one part to another but you still gut stuck with targeting features which are specific to different chips.

    The tools have to do a great many things - the Aldec tool gives me a bunch of files in HDL that I know work OK in simulation, the vendor tool still has synthesize that into FPGA blocks, fit it into the FPGA, route it, check timing, and maybe re-route/fit many times.  The vendor tools also include stuff for helping you use the on chip features and joining together loads of different bits of IP (other peoples' HDL)  and managing the whole thing. A serious FPGA project will include hundreds of files.

     

    In terms of what FPGAs can do:

    AN FPGA is probably at least 10x less efficient in use of silicon than an ASIC. If you want an ASIC that can out compute a $2000 Xilinx FPGA expect to spend at least $100M getting it to production - if you only want less than 50,000 of them this doesn't work out fo you - even though the ASIC might only cost $100 each.  (These are very rough figures but you get the idea).

    For big projects big FPGAs can massively out compute pretty much anything, they have thousands of DSP blocks that can all work at once.

    For smaller projects - I'll give you some real  examples:

     

    Glue together 4 different audio chips to talk to a piece of pro audio gear with a rather odd digital interface. A Lattice ICE40 chip costing £5, using a few mA of current was used to do this. It was also able to replace the tiny processor previously used for configuring the chips and can easily be tweaked if any of the audio chips is upgraded. No processor could handle 4 different protocols and talk to 5 chips using two different voltages.

     

    Pre-process data from an 8 channel ADC generating 24 bit samples at an aggregate data rate of 1.92Ms/s. There are some DSPs that can just about talk to the ADC but none of them could handle the 128 bit wide data paths involved in the pre-processing. The DSP was a Cyclone 10.

     

    Control 32 channels of 10 bit resolution PWM - this was a 1000 LUT ICE40 in a 100 pin TQFP package - very low power and cheap.

     

    Debugging:

    Simulation is the key - make sure everything works before it hits the hardware. Of course some things get missed and still don't work.

     

    There are tools that try to embed some logic analysis in the FPGA but I've found them to be pretty much useless - the last project I tried to use them (Xilinx Vivado, Artix FPGA) whenever the debugging stuff was added the design wouldn't meet timing any more. I try to make sure that on a big project the FPGA has at least 16 pins on connectors exclusively for debugging. Then you can connect signals of interest to them and look with a logic analyzer. It's also a really good idea to add test connectors, series resistors or test pads (in descending order of preference) to on chip buses, so you can get access. On really fast stuff you can't do this - else it will stop working.

     

    MK

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to neuromodulator

    Lots of interesting points - I'm off on a long weekend hol so not enough time to cover them all but I'll have a go.

     

    There are two primary HDL (Hardware Definition Languages), Verilog and VHDL. They both come in different versions, there are fewer versions of VHDL than of Verilog. The latest versions of Verilog and VHDL both contain many features that synthesizers are unable to deal with. This is one reason why HDL "code" may be non-portable.

    Once you start using an HDL to target an FPGA you may want to use the special features of the FPGA like on chip RAM blocks, PLLs, DDRAM interface hardware etc etc. These are all different for different FPGAs and once your project uses them it becomes specific to that FPGA type.

    Many people use the FPGA vendors toolset including HDL editor, compiler, simulator,  synthesizer, timing checking, fitter, programmer and debugger.

    As you move up the food chain you'll find more use of separate tools, I use Aldec HDL for design and simulation, this makes it a bit easier to port designs from one part to another but you still gut stuck with targeting features which are specific to different chips.

    The tools have to do a great many things - the Aldec tool gives me a bunch of files in HDL that I know work OK in simulation, the vendor tool still has synthesize that into FPGA blocks, fit it into the FPGA, route it, check timing, and maybe re-route/fit many times.  The vendor tools also include stuff for helping you use the on chip features and joining together loads of different bits of IP (other peoples' HDL)  and managing the whole thing. A serious FPGA project will include hundreds of files.

     

    In terms of what FPGAs can do:

    AN FPGA is probably at least 10x less efficient in use of silicon than an ASIC. If you want an ASIC that can out compute a $2000 Xilinx FPGA expect to spend at least $100M getting it to production - if you only want less than 50,000 of them this doesn't work out fo you - even though the ASIC might only cost $100 each.  (These are very rough figures but you get the idea).

    For big projects big FPGAs can massively out compute pretty much anything, they have thousands of DSP blocks that can all work at once.

    For smaller projects - I'll give you some real  examples:

     

    Glue together 4 different audio chips to talk to a piece of pro audio gear with a rather odd digital interface. A Lattice ICE40 chip costing £5, using a few mA of current was used to do this. It was also able to replace the tiny processor previously used for configuring the chips and can easily be tweaked if any of the audio chips is upgraded. No processor could handle 4 different protocols and talk to 5 chips using two different voltages.

     

    Pre-process data from an 8 channel ADC generating 24 bit samples at an aggregate data rate of 1.92Ms/s. There are some DSPs that can just about talk to the ADC but none of them could handle the 128 bit wide data paths involved in the pre-processing. The DSP was a Cyclone 10.

     

    Control 32 channels of 10 bit resolution PWM - this was a 1000 LUT ICE40 in a 100 pin TQFP package - very low power and cheap.

     

    Debugging:

    Simulation is the key - make sure everything works before it hits the hardware. Of course some things get missed and still don't work.

     

    There are tools that try to embed some logic analysis in the FPGA but I've found them to be pretty much useless - the last project I tried to use them (Xilinx Vivado, Artix FPGA) whenever the debugging stuff was added the design wouldn't meet timing any more. I try to make sure that on a big project the FPGA has at least 16 pins on connectors exclusively for debugging. Then you can connect signals of interest to them and look with a logic analyzer. It's also a really good idea to add test connectors, series resistors or test pads (in descending order of preference) to on chip buses, so you can get access. On really fast stuff you can't do this - else it will stop working.

     

    MK

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer