FPGA
  • Technologies
  • More
FPGA
Forum Difficulties with interfacing external devices using Altera FPGAs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 583 subscribers
  • Views 940 views
  • Users 0 members are here
  • terasic
  • intel fpga
  • fpga
  • fpgas
  • cyclone v
  • traditional fpga development
  • altera
  • intel cyclone 10
  • altera_cyclone
  • quartus
  • fpga vhdl
Related

Difficulties with interfacing external devices using Altera FPGAs

ghinwa
ghinwa over 7 years ago

How can I interface external analog signals (from a potentiometer for example) and display the bits on the user LEDs? Is it also possible to apply fourier transform on these analog signals? I have both Cyclone 10 LP evaluation kit and the DE 10 Nano standard, yet I couldn't successfully implement this experiment in either of them. for the DE 10 Nano standard, i read the ADC controller IP manual but its directions weren't that clear for me.

 

Generally speaking, I still don't understand how configuring the pin planner works so that might be one of the issues. Also the problem doesn't lie just in this experiment, I am having difficulties with interfacing anything external whether it was a motor or an LCD screen.

 

I've only started teaching myself VHDL and FPGAs a few months ago so I'm still a beginner. I've implemented some basic logic design concepts such as full adders and multiplexers and they worked just fine.

 

If someone can guide me through the problems I'm facing now I'd truly appreciate it. Any advice, resources etc. would be helpful.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago +5 verified
    The DE 10 Nano board has an SPI interfaced ADC on board. Terrasic will supply example code that will operate it. If you are a beginner I suggest that the Cyclone 10 and Cyclone V SE are not good places…
  • ghinwa
    ghinwa over 7 years ago in reply to michaelkellett +1
    What you're saying makes sense. It just happens my university bought the two boards I mentioned although it doesn't use them much. I'll try to make the best out of them since these are the only available…
Parents
  • michaelkellett
    0 michaelkellett over 7 years ago

    The DE 10 Nano board has an SPI interfaced ADC on board. Terrasic will supply example code that will operate it.

     

    If you are a beginner I suggest that the Cyclone 10 and Cyclone V SE are not good places to start.

     

    These are complex chips with loads of stuff you really don't need yet.

     

    The boards (especially the DE 10 Nano) have lots of complicated additional features you don't want to get into yet.

     

    Consider going for a much simpler solution based on an easier FPGA.

     

    If you want to stick with Altera (and if you are struggling with the tools you may well not) then look at a nice simple board like this:

     

    https://kamami.com/boards/561438-maximator-promo-with-expander-shield-and-kamami-usb-blaster.html

     

    or even a cheap Chinese one like this:

     

    https://www.aliexpress.com/item/32859698607.html?spm=a2g0o.productlist.0.0.4b4e16c5hGMFWf&algo_pvid=7d4eef2d-0f93-4e9c-b…

     

    Alternatively consider trying the Lattice XP2 range - nice simple FPGA and nice simple dev board and nice simple tools (notice the pattern there ?)

     

    Lattice do a simple dev board, in stock at Farnell - part number 2253073, no ADC on the board.

     

    In my opinion you will find it much easier to learn the basics with older designs of chips and tools.

     

     

    Cheap Entry into FPGA

    Kamami MAXimator FPGA Board

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ghinwa
    0 ghinwa over 7 years ago in reply to michaelkellett

    What you're saying makes sense. It just happens my university bought the two boards I mentioned although it doesn't use them much. I'll try to make the best out of them since these are the only available resources I currently have.

     

    Also, thank you for taking some time to write your suggestions. I will surely buy one of the boards you mentioned someday and improve myself with the basics.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ghinwa
    0 ghinwa over 7 years ago in reply to michaelkellett

    What you're saying makes sense. It just happens my university bought the two boards I mentioned although it doesn't use them much. I'll try to make the best out of them since these are the only available resources I currently have.

     

    Also, thank you for taking some time to write your suggestions. I will surely buy one of the boards you mentioned someday and improve myself with the basics.