FPGA
  • Technologies
  • More
FPGA
Forum What are you using FPGAs for?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 586 subscribers
  • Views 3506 views
  • Users 0 members are here
  • fpga
Related

What are you using FPGAs for?

Catwell
Catwell over 16 years ago

I rarely use FPGAs. I mostly have stuck in other embedded development environments during my career. But, how are you using FPGAs these days?

 

Cabe

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    I am working on a design implementing a computationally-intensive image processing algorithm, which has to run real-time at up to 60 frames per second.  Such computation requires a large array of CPU cores, which is more costly and power-intensive than a custom FPGA solution.  They tend to excel at tasks where there is a fixed set of computations to be performed, and are able to achieve a high throughput because the operations can be performed in parallel across the logic fabric in the chip.  Image processing, telecommunications, and aerospace are areas which are using the larger FPGA devices these days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    I am working on a design implementing a computationally-intensive image processing algorithm, which has to run real-time at up to 60 frames per second.  Such computation requires a large array of CPU cores, which is more costly and power-intensive than a custom FPGA solution.  They tend to excel at tasks where there is a fixed set of computations to be performed, and are able to achieve a high throughput because the operations can be performed in parallel across the logic fabric in the chip.  Image processing, telecommunications, and aerospace are areas which are using the larger FPGA devices these days.