FPGA
  • Technologies
  • More
FPGA
Forum Recommend a beginners FPGA development kit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 587 subscribers
  • Views 5212 views
  • Users 0 members are here
  • fpga
  • learning
  • dev_kit
Related

Recommend a beginners FPGA development kit

Catwell
Catwell over 15 years ago

An engineering friend of mine could really benefit from learning more about FPGAs. I suggested getting a simple devkit to get some hands on experience programming and designing with them. When he asked what to get, I will admit, I was at a loss.

 

So, if anyone can recommend something that would be great.

 

Thanks ahead of time.

 

Cabe

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago +1 suggested
    There are virtually tons of inexpensive development boards out there. Xilinx has a $49 Spartan 3 board, for example. Development software is free, and the boards come with demo programs. If you just go…
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Catwell +1
    Personally, I'd go for an FPGA vs. a CPLD. The CPLD just doesn't have a lot of resources-256 macrocells(registers) as compared to the XC3S250 in the Butterfly which has THOUSANDS of registers, multipliers…
  • gbulmeruk
    gbulmeruk over 15 years ago in reply to Catwell +1
    Cabe - as I wrote, CPLD and FPGA are rather different animals. If your friend sees increasing numbers of FPGA-based products, and not CPLD, get FPGA. FPGA provides for MUCH more complex projects than a…
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    There are virtually tons of inexpensive development boards out there. Xilinx has a $49 Spartan 3 board, for example.  Development software is free, and the boards come with demo programs. If you just go to the FPGA manufacturer sites(Xilinx, Altera, Lattice) you'll find them.  The distributors (Avnet, Arrow, etc.) also have some of their own development boards.  You probably want to get a kit that comes with a download cable, or you're going to have to go buy one.

     

    Barry

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to e14 Contributor

    Barry,

     

    Thank you for the reply.

    The Spartan 3   boards are a little more thant $50 dollars from what I found. XILINX   - HW-SPAR3AN-SK-UNI-G

     

    This one looks like a good   starter kit, what do you think? XILINX   - SK-CRII-L-G - CoolRunner-II CPLD Starter Kit

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 15 years ago in reply to gbulmeruk

    I use Lattice tools on a daily basis - I don't consider them to be ruined.

    For projects that will only use a ready made development board it probably does not matter much where you start between A, L and X. (The A stands for Altera not Actel)

    If there is any prospect of production on a custom board then it matters a lot. Flash based parts are easier to use.

    I've found Lattice much easier to deal with for small (< 10,000) projects.(They may be better with bigger numbers too but I don't have experience in that area.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gbulmeruk
    0 gbulmeruk over 15 years ago in reply to michaelkellett

    michaelkellett - my friend uses Lattice for his work.

     

    He was using "ispLEVER" which he liked a lot, but now the IDE has changed and become "Diamond".

    He was particularly unhappy about the changes to the simulation workflow.

     

    I am learning about FPGA's (and so in the same market as Cabe's friend), and the toolchain matters to me a lot. I am primarily a 'software person'.

    I don't use Windows so that makes it harder too; though it is encouraging to see more manufacturer's (of MCU's and FPGA's) making their tools available on Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to gbulmeruk

    My two cents: I also use ispLEVER, haven't made the switch to Diamond yet.  I also use Xilinx and Altera tools.  They ALL have problems.  Xilinx Webpack(free) is available for Linux, I don't know about the rest.  If I might editorialize: I have migrated away from Altera because their support SUUUUUUCKS. If you're just starting out vendor support is particularly important. (I hope somebody from Altera is reading this.)  Altera's tools and devices are fine, but that's only part of the equation.

     

    Barry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to gbulmeruk

    Gbulmeruk,

    An FPGA capable of emulating an entire processor is under $20

    Point me in the right direction.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to e14 Contributor

    Barry,

    Your claims on Altera have me thinking twice about their boards. Can you post some links with info pertaining to ispLEVER?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ezekiel
    0 ezekiel over 15 years ago in reply to Catwell

    The Altera Cyclone III can use the NIOS2 softcore which is an ARM core that can run Linux.

     

    Again, check out the BeMicro $49 USB dev stick.

     

    As far as support goes, you have to remember that those who spend the most $$'s will get the most attention from the chip vendor.  It's the Golden Goose analogy. The company I worked for used a lot of Altera parts and they got good support because they bought tens of thousands of $$'s worth of parts a year from Altera.

     

    Us little guys have to stick together and help each other out. OpenCores.org is a perfect example of this mentality. Check them out for support too.

     

    In the end, you have to choose yourself which FPGA vendor to go with. They are all competitive. It's just like Ford vs. Chrysler vs. Chevrolet. Or, for others, it's just like Soda vs. Beer vs. Whiskey. Pick your own poison.

     

    No matter what choice is made, you *will* have to invest time and effort to learn how to program VHDL. That should be your bigger concern at this time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 15 years ago in reply to ezekiel

    @ezekiel,

    The NIOS2 is not an ARM - it is Altera's own processor architcture.

    If you want to use ARM + FPGA on one chip then look to Xilinx (big chips, big ARMs, very expensive) or Actel (much lower down the price range, Cortex M3 ARM - but now under new and uncertain ownership).

     

    IMO beginners with FPGA should steer well clear of embedded processors (soft or hard) .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gbulmeruk
    0 gbulmeruk over 15 years ago in reply to Catwell

    Cabe - Lattice have a soft 8-bit and 32-bit processor

    The 8-bit is at http://www.latticesemi.com/products/intellectualproperty/referencedesigns/8bitmicrocontrollermico8.cfm

     

    They say "The core consumes minimal device resources, less than 200 Look Up Tables  (LUTs) in the smallest configuration, while maintaining a broad feature  set."

     

    I checked their 32-bit soft core recently, and it would easily fit on something like a low-end, 5,000 LUT, XP2, e.g.

    http://uk.farnell.com/lattice-semiconductor/lfxp2-5e-5tn144c/fpga-5k-luts-100-i-o-dsp-144tqfp/dp/1571999

    which is in a DIY-able QFP (not BGA) package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gbulmeruk
    0 gbulmeruk over 15 years ago in reply to ezekiel

    I think a key point is the toolchain.

     

    Fortunately, you can download the tools for free and try them.

    They should all come with a simulator. If it doesn't don't bother with it (my chums recommend beginners to debug designs using simulators, especially when on a low budget, i.e. few pieces of gtest equipment)

     

    So your friend could futz around with the toolchain, without any hadware, and see what they like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to ezekiel

    At the risk of diverting this thread from it's original focus (which is usually the nature of discussions) my comment about Altera's support is relative to Xilinx and Lattice support.  We are a small customer of all three, but Xilinx and Lattice are far superior in support.  If I post a support request on the Xilinx site I normally get a response within 24 hours.  For Altera I have waited days for any kind of response.  Lattice, being the little guy, seems to be the most responsive.  Also, Avnet, the Xilinx distributor, has an FAE who is very helpful.

     

    Barry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to ezekiel

    At the risk of diverting this thread from it's original focus (which is usually the nature of discussions) my comment about Altera's support is relative to Xilinx and Lattice support.  We are a small customer of all three, but Xilinx and Lattice are far superior in support.  If I post a support request on the Xilinx site I normally get a response within 24 hours.  For Altera I have waited days for any kind of response.  Lattice, being the little guy, seems to be the most responsive.  Also, Avnet, the Xilinx distributor, has an FAE who is very helpful.

     

    Barry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ezekiel
    0 ezekiel over 15 years ago in reply to e14 Contributor

    I think that you point is probably the central motivator for the selection of a chip vendor.

     

    I think you hit the nail on the head with your last comment about the FAE. If you have an excellent *local* FAE then you will get excellent support. This is my experience too. Our local Arrow office hired (stole) the local Altera FAE and so they can give same day customer support to some key clients in our city. This is why I'm cheering on Altera.

     

    As an update to my BeMicro dev stick, I found the following webpages from its manufacturer:

     

    BeMicro FPGA-stick:  http://www.hitex.com/index.php?id=1489&L=2//controllers/My

    BeMicro SDK:  http://www.hitex.com/index.php?id=3180&L=2//controllers/My

     

    You will find info about the prototyping expansion board, its connector and the software development kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to e14 Contributor

    Barry,

     

    Diverting from the topic probably will not get the attention of Altera. Perhaps starting a separate post about Altera tech support is a good idea. For example "Altera tech support, your experiences?"

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to ezekiel

    Ezekiel,

     

    Thanks for the suggestion of the Bemicro. I will definitely suggest that to my friend.

     

    I, personally, wouldn't mind trying out everyone's suggestions in this thread. FPGA programming is a very useful skill to have.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ezekiel
    0 ezekiel over 15 years ago in reply to Catwell

    FYI, here is the Altera online forums:

     

    http://www.alteraforum.com/forum/index.php

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago in reply to Catwell

    For beginners I recommend Altera DE1 Board Cyclone II FPGA Starter Board. It is cheap and includes an Altera Cyclone II 2C20 FPGA. This development Kit provides the user with a USB command controller, a multi-port SRAM/SDRAM/flash memory controller. It provides a software controller in C++. Some examples written in Verilog code.

     

    Welcome to the Altera Cyclone II FPGA Starter Development Kit, which
    includes a full-featured field-programmable gate array (FPGA)
    development board, hardware and software development tools,
    documentation, and accessories needed to begin FPGA development.
    The development board includes an Altera Cyclone II 2C20 FPGA and
    comes preconfigured with a hardware reference design stored in flash
    memory. Hardware designers can use the development board as a
    platform to prototype complex embedded systems.
    The Development Kit provides the user with an integrated control
    environment that includes a software controller in C++, a USB command
    controller, a multi-port SRAM/SDRAM/flash memory controller, and
    demonstration circuitry specified in Verilog code. These features enable
    users to implement and test designs without the need to implement
    complex application programming interfaces (APIs), host control
    software, or SRAM/SDRAM/flash memory controllers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to maiatec

    just to add to this, there are even cheaper Altera university program boards such as the DE0. I would definitely recommend this over the BEMICRO due to more I/Os (switches, LEDs, etc.) disclaimer: i work for Terasic, but its my honest opinion image