FPGA
  • Technologies
  • More
FPGA
Forum TCAM implementations in FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 4 answers
  • Subscribers 584 subscribers
  • Views 4286 views
  • Users 0 members are here
  • tcam
  • fpga
Related

TCAM implementations in FPGA

e14 Contributor
e14 Contributor over 14 years ago

There is a need to implement TCAM memory in a FPGA. The size of TCAM memory is 128K entries. It supports both 72 bit and 144 bit addresses. Can anyone provide any info regarding this???

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 9 years ago +2 suggested
    Just for fun, I thought I might mention that you could do a 16x32 CAM quite nicely in Xilinx Spartan-3 or Spartan-6 using distributed dual-port RAMs as look-up tables. Basically, to identify a 32-bit number…
  • michaelkellett
    michaelkellett over 9 years ago in reply to bugzz2 +1 suggested
    I see now - that you aren't the same person - woops ! 16 x 32 is much more reasonable. www.xilinx.com/support/documentation/application.../xapp1151_Param_ CAM .pdf https://www.altera.com/en_US/pdfs/literature…
  • michaelkellett
    michaelkellett over 9 years ago in reply to bugzz2 +1 suggested
    Cyclone II is old and slow - I assume this isn't a commercial project. I'm going to make some big guesses here and tell you that you are doing it all wrong I bet the Ethernet frame doesn't get into the…
Parents
  • johnbeetem
    0 johnbeetem over 9 years ago

    Just for fun, I thought I might mention that you could do a 16x32 CAM quite nicely in Xilinx Spartan-3 or Spartan-6 using distributed dual-port RAMs as look-up tables.  Basically, to identify a 32-bit number you encode eight 4-input LUTs (or six 6-input LUTs) with the 32-bit pattern you want to match and then AND their outputs.  You can load the bit pattern you want to match using the second port.  Spartan-6 has reconfigurable LUTs you can load serially.

     

    On Spartan-6 you can use a 6-input LUT as two 5-input LUTs if they have the same inputs.  This could save some LUTs when doing a pair of CAM lines.

     

    This scheme works for a small number of entries since you need a bunch of LUTs for each entry.  If you have a large number of IP subnet addresses to match, use the CAM as a cache and a PATRICIA tree for other entries.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 9 years ago

    Just for fun, I thought I might mention that you could do a 16x32 CAM quite nicely in Xilinx Spartan-3 or Spartan-6 using distributed dual-port RAMs as look-up tables.  Basically, to identify a 32-bit number you encode eight 4-input LUTs (or six 6-input LUTs) with the 32-bit pattern you want to match and then AND their outputs.  You can load the bit pattern you want to match using the second port.  Spartan-6 has reconfigurable LUTs you can load serially.

     

    On Spartan-6 you can use a 6-input LUT as two 5-input LUTs if they have the same inputs.  This could save some LUTs when doing a pair of CAM lines.

     

    This scheme works for a small number of entries since you need a bunch of LUTs for each entry.  If you have a large number of IP subnet addresses to match, use the CAM as a cache and a PATRICIA tree for other entries.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • bugzz2
    0 bugzz2 over 9 years ago in reply to johnbeetem

    Thank you, insructions were helpful. I will upload my code as soon as I get sure that is near the solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • doomsday
    0 doomsday over 8 years ago in reply to bugzz2

    So did you complete the code, bruh! image