FPGA
  • Technologies
  • More
FPGA
Forum A 3.3v (or less!) issue.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 582 subscribers
  • Views 480 views
  • Users 0 members are here
Related

A 3.3v (or less!) issue.

YT2095
YT2095 over 14 years ago

How does one get around this problem in Design?

all My MCUs are 5v I/O, as are the CPUs and other peripheral ICs that I`d be interested in using with CPLDs, so any Gain in board real-estate and lower power consumption, would be taken away by having to use Level Translator ICs.

 

is this just the harsh reality, or there a workaround at all?

  • Sign in to reply
  • Cancel
  • johnbeetem
    0 johnbeetem over 14 years ago

    1.  If you're using CPLDs rather than FPGAs, you could go with a CPLD family that has 5V-tolerant I/Os such as the Xilinx XC9500XL series.

     

    2.  Usually you can drive 5V inputs with 3.3V outputs, so it's usually not a problem for inputs of 5V devices.

     

    3.  Some 3.3V FPGAs such as the Xilinx Spartan-IIE do not have 5V-tolerant inputs per se, but as long as you keep the input current low enough you can connect 5V outputs through (say) 1K Ohm resistors, assuming the resistors don't slow things down too much.  This may take care of some 5V outputs.

     

    4.  Otherwise you do need level shifters or use N-FET bus switches as voltage limiters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer