FPGA
  • Technologies
  • More
FPGA
Forum Some FPGA Beginner Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 78 replies
  • Answers 19 answers
  • Subscribers 584 subscribers
  • Views 13930 views
  • Users 0 members are here
Related

Some FPGA Beginner Questions

e14 Contributor
e14 Contributor over 13 years ago

Hi element14!

 

Some time ago I've watched a talk of the nand2tetris course/project. If you've never heard of it you can check it out here: http://www.nand2tetris.org/ Basically it is a course designed to build a computer from the very ground up. It starts with logic gates and goes all the way up to programming a small game project (hence the name nand2tetris). There is also a video available from someone who has been doing the course on FPGA hardware ( http://www.youtube.com/watch?v=UHty1KKjaZw ).

[At one point in the above linked youtube video you can see the designation "ep2c8q208", which should mean the project is running on Altera Cyclone II hardware.]

 

I've always been curious about doing something with FPGA hardware, but never had any idea of a feasible, yet interesting-result-yielding project. Well, as you can probably guess, up until now that is image

 

During my university days I attended an FPGA workshop and I've read some stuff about the hardware components and the available course material, so I think I kind of have an idea about the difficulty of the project. But since everything I've been reading just made me more excited, I decided I absolutely want to give this a shot. Now there's a lot of FPGA information out there, so I'm surely still missing a lot of important information, but I would like to get started and think the best way to learn is to actually experiment with a real FPGA instead of wasting too much time with HDL simulations only to become used to functions that aren't going to synthesize on the board anyway.

 

So I now would like to ask you about some things I'm still unsure about and would like to have clarified before buying an expensive development kit. I've read several articles about Altera and Xilinx and right now my choice would be a Spartan 3E Starter Board - this one to be exact: http://shop.embedded-projects.net/index.php?module=artikel&action=artikel&id=549

 

The main questions I'm having right now:

- Is there a general reason that would argue against getting the Spartan E3 board?

- I actually have no idea how powerful an FPGA really is.. but assuming it's running on Cyclone II hardware, it probably should run on a Spartan 3 as well? Or is that in itself already a stupid question, as FPGA comparison doesn't work so easily?

- As you can see, the price for the above board is about 150 Euro, which translates to something just short of $200. Yet I continue to find offers (on ebay or other websites) where boards are being sold for under $150 but even include small screens(!)*  What am I missing here? Did I pick an especially expensive outlet, or is there something shady about these cheap deals..?

- In general, who is more newbie-friendly, Altera or Xilinx? (I've worked with VHDL before, which I think is Xilinx, right? Altera's Quartus is probably very similar?)

- From how I understand the FPGA toolchain, in the above linked offer there should be everything included to get me going.. right? o_O

 

I also have this second candidate: http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,836&Prod=ATLYS

- Maybe I'm an idiot, but as I read the offer, *only* the board is sold? I.e., in contrast to the first offer, I would need additional stuff to get something running on the board?

- It also strikes me as a mayor drawback that there is not really an output option besides a few LEDs.. which for me would be very annoying; I'm already unhappy about the board linked before *only* having a small display (which in itself, however, is awesome to have of course).

- This might also be a stupid question: I remember from back in the FPGA workshop I mentioned that getting a number-display to run is not that hard at all. How much more effort is it to get something displayed on a screen (either an attached one or a PC screen accessed via one of the available ports)?

 

And as a final question: I've also seen some very much smaller boards than the ones linked here, that are also much cheaper.. are the boards I'm looking it overkill for what I'd like to do with them? Or does actually the contrary hold, and such a project wouldn't even run on one of the smaller boards available?

 

Thanks for your help!

 

Cheers,

pan

 

________________________

* Here for example:

http://www.sainsmart.com/evaluation-board/fpga-cpld-board/new-ep2c8q208c8n-development-board-kit-fpga-altera-cyclone-nios-ii-with-2-4-lcd.html

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 13 years ago +2 suggested
    Hi Christian, I just saw your discussion today. I don't check the element14 FPGA page much since activity is rare. There's some good FPGA discussion in this thread at the Raspberry Pi group, including…
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +2 suggested
    I'm going to offer some advice which has worked well for me over the last 10 years. Forget Xilinx and Altera and download the Lattice toolset - not as capable as the full Xilinx kit but good enough to…
  • michaelkellett
    michaelkellett over 11 years ago in reply to michaelkellett +2 suggested
    A simple counter example for LED twinkles ! There must be a way to add a text file - someone please tell how ! MK
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Old post, I know, but I ended up here so others might as well. Digilent has since put out a nexys 4 which is quite powerful, but priced like the previous nexii. I'd call it a good choice.

    ZYNQ is a little more available now, the cheapest options being a parallella board (not shipping as of this post) or the zed mini. I've had the nexys 2 and the ATLYS (and two parallellas that haven't come yet), and have been happy with both, though a friend has borrowed the ATLYS and has had it longer than I have at this point. He runs ubuntu and cray on it. The power of atlys is basically matched by the new nexys 4 though, so I'd start there.

     

    Sainsmart is… best avoided. I bought a cell phone board from them and it looks like they hand soldered it, SMA parts and all. A very important point to make is that it works exactly as advertised, but they also bridged a bunch of pins with a solder blob (apparently on purpose), so it makes me nervous. Like buying a car for $50; yes it drove me across town, and has not had a breakdown yet, there is a lot of ductape holding on the bumper though, and the ignition is two wires you twist, and it makes a noise, and a smell. Buyer beware I guess, sometimes cheap and works is all that matters to you. I WILL point out it came without documentation. I mean any. There are jumpers and buttons on this board and no doc anywhere that says what they do or where they connect. There are forum posts aplenty from others trying to puzzle it out. I've been able to use it because it came ready to connect via serial terminal straight to the 3rd party chip, which did have documentation. I just… buttons, unlabeled buttons. I feel bad since it works alright but, man is it just sketchy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Old post, I know, but I ended up here so others might as well. Digilent has since put out a nexys 4 which is quite powerful, but priced like the previous nexii. I'd call it a good choice.

    ZYNQ is a little more available now, the cheapest options being a parallella board (not shipping as of this post) or the zed mini. I've had the nexys 2 and the ATLYS (and two parallellas that haven't come yet), and have been happy with both, though a friend has borrowed the ATLYS and has had it longer than I have at this point. He runs ubuntu and cray on it. The power of atlys is basically matched by the new nexys 4 though, so I'd start there.

     

    Sainsmart is… best avoided. I bought a cell phone board from them and it looks like they hand soldered it, SMA parts and all. A very important point to make is that it works exactly as advertised, but they also bridged a bunch of pins with a solder blob (apparently on purpose), so it makes me nervous. Like buying a car for $50; yes it drove me across town, and has not had a breakdown yet, there is a lot of ductape holding on the bumper though, and the ignition is two wires you twist, and it makes a noise, and a smell. Buyer beware I guess, sometimes cheap and works is all that matters to you. I WILL point out it came without documentation. I mean any. There are jumpers and buttons on this board and no doc anywhere that says what they do or where they connect. There are forum posts aplenty from others trying to puzzle it out. I've been able to use it because it came ready to connect via serial terminal straight to the 3rd party chip, which did have documentation. I just… buttons, unlabeled buttons. I feel bad since it works alright but, man is it just sketchy.