FPGA
  • Technologies
  • More
FPGA
Forum Can someone advise me on an FPGA? Needs 4 LVDS Receive channels @ 900Mbit/s....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 585 subscribers
  • Views 1313 views
  • Users 0 members are here
Related

Can someone advise me on an FPGA? Needs 4 LVDS Receive channels @ 900Mbit/s....

vsluiter
vsluiter over 12 years ago

Hello all,

 

I've had my share of microcontrollers I worked with, but now I need to interface a high speed ADC, which outputs its 12-bit data at 900Mbit/s (450MHz). I can't ignore (or circumvent) FPGA's here, but I'm a bit daunted by the devices which are capapble of this. So far, I found the Lattice ECP3 family, Xilinx Spartan 6 and Altera Cyclone V devices to be able to do this.

However, these devices are very, very complicated, and I don't need much functionality apart from receiving and storing data for a couple of microseconds, and then slowly (could be UART!) transferring the data to a PC. Does anyone know a smaller (in pin count / real estate) device that can do this? I know I still have to figure out how to store my data, probably that's also going to be some LVDS storage(?).

 

I'd also be happy if anyone can tell me why smaller packages do not have the high-data-rate transceivers. Is that just market-driven, or am I overlooking something ?

 

 

Thanks for your help!

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    I think it's  a market thing - Lattice have  ECP5 and MachX03 families in the pipeline which might be simpler but you can't easily get parts yet. Lattice ECP3  is viable and even the smallest device has 4 serdes channels. It's still 256 ball BGA for the lowest pin count part.

    There is no difference between working with the ECP3 or the simpler Lattice ice40 parts except that the tools for the ECP3 work better.

     

    I've done a lot with ECP3 (but not serdes) so might be able to help out if you go that way.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to michaelkellett

    Thanks! As I understood, the ice40 does not have LVDS transceivers, and does not support (internal) clocks this fast. Can you confirm that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to vsluiter

    You need more than just LVDS, you need SERDES in hardware to get that 900MHz data down to FPGA fabric speed. Your 12 bit convertor is only supplying 75Msamples per second, on an ECP3 a 150MHz clock is feasible but it will be  a LOT easier to meet timing if you can get down to 75Mhz. The ice40 has no SERDES hardware and is not designed for speed.

     

    Which ADC are you using ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to michaelkellett

    Hello Michael,

    When and if I'll be making this design, it'll be something like Texas Instruments' AFE5803 or Analog's AD9670/AD9671 . I'd be happiest to have 14 bit data at 75MHz, but as far as I can see now, I could live with 12 bit at ~50MHz. The last option would require some more post processing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago in reply to michaelkellett

    Hello Michael,

    When and if I'll be making this design, it'll be something like Texas Instruments' AFE5803 or Analog's AD9670/AD9671 . I'd be happiest to have 14 bit data at 75MHz, but as far as I can see now, I could live with 12 bit at ~50MHz. The last option would require some more post processing.