FPGA
  • Technologies
  • More
FPGA
Forum Can someone advise me on an FPGA? Needs 4 LVDS Receive channels @ 900Mbit/s....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 585 subscribers
  • Views 1319 views
  • Users 0 members are here
Related

Can someone advise me on an FPGA? Needs 4 LVDS Receive channels @ 900Mbit/s....

vsluiter
vsluiter over 12 years ago

Hello all,

 

I've had my share of microcontrollers I worked with, but now I need to interface a high speed ADC, which outputs its 12-bit data at 900Mbit/s (450MHz). I can't ignore (or circumvent) FPGA's here, but I'm a bit daunted by the devices which are capapble of this. So far, I found the Lattice ECP3 family, Xilinx Spartan 6 and Altera Cyclone V devices to be able to do this.

However, these devices are very, very complicated, and I don't need much functionality apart from receiving and storing data for a couple of microseconds, and then slowly (could be UART!) transferring the data to a PC. Does anyone know a smaller (in pin count / real estate) device that can do this? I know I still have to figure out how to store my data, probably that's also going to be some LVDS storage(?).

 

I'd also be happy if anyone can tell me why smaller packages do not have the high-data-rate transceivers. Is that just market-driven, or am I overlooking something ?

 

 

Thanks for your help!

  • Sign in to reply
  • Cancel
Parents
  • michaelwylie
    0 michaelwylie over 12 years ago

    I've had this exact problem. I was gathering data at 400 MHz from a TI ADC. I ended up using an Altera FPGA, but I used a 4 to 1 deserializer to split the stream into chunks that could be clocked at 100 MHz. The Altera deserializers can run up in the GHZ for sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelwylie
    0 michaelwylie over 12 years ago

    I've had this exact problem. I was gathering data at 400 MHz from a TI ADC. I ended up using an Altera FPGA, but I used a 4 to 1 deserializer to split the stream into chunks that could be clocked at 100 MHz. The Altera deserializers can run up in the GHZ for sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer