FPGA
  • Technologies
  • More
FPGA
Forum 7 Ways to Leave Your Spartan-6 Challenge - What Toolchain version are you using?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 581 subscribers
  • Views 2188 views
  • Users 0 members are here
  • digilent ip
  • 7 Ways to Leave Your Spartan-6
  • vivado
  • spartan-7
  • vitis
  • Spartan_Migration
Related

7 Ways to Leave Your Spartan-6 Challenge - What Toolchain version are you using?

ralphjy
ralphjy over 4 years ago

It appears that some challengers have received their Arty S7 boards (lots of recent blogs).

Since I'm currently ruminating about an issue that I think most of us will face - I thought it would be a good topic for discussion.

These boards are 2017 vintage and the OOB example also dates to 2017.  So, I think that a lot of examples that we encounter will be using earlier versions of the toolchain.  If I'm not mistaken, Vitis showed up in 2019.2.

I'm thinking about which toolchain version to use.  Switching toolchain versions can be a nontrivial task (especially if an OS version change is needed - I use VMs, but I don't have every flavor).

I want to use Digilent IP for setting up various MicroBlaze implementations for running PMODs.

I noticed that the latest update to the github repo appears to be for 2019.2.  https://github.com/Digilent/vivado-library

image

Maybe I'm looking in the wrong place?  Anyone find more recent IP?

I found this link to a guide for 2020.1, but the link to the .zip file doesn't exist.  https://digilent.com/reference/programmable-logic/guides/getting-started-with-pmod-ips

Maybe I'm overthinking it and upconverting the IP won't be that difficult.  Thoughts?

I wasn't going to tackle this until I get some PMODs that I ordered, but I'd be interested if anyone has already worked this out.

Ralph

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 4 years ago +2
    I recommend using latest release (2022.1). Latest release can import projects from older version and contains bug fixes to known issues from all previous versions. I faced isseu on 1.1.2022. Some tools…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to misaz +2
    There is a patch for the older releases, as a separate download and activity after installation. Xilinx didn't release new installers with the fix for those older versions, though.
  • saadtiwana_int
    saadtiwana_int over 4 years ago +2
    I've been using 2019.1 and 2022.1 on two different PCs. Have had success with both, when using the Arty-S7. But moving forward, I will be doing most of my work using the latests version. I keep the 2019…
Parents
  • javagoza
    javagoza over 4 years ago

    Thanks for opening this discussion.

    I am still at the same research point as you and I have the same doubts. Until I have time to make my first bare metal application on a soft MicroBlaze I will continue with the doubts.

    I'm going to order some PMOD modules without even looking if I'm going to be able to use them but I'm sure I'll find them useful in the future. There is HDL code for many PMODs in that repository, I think at least for now trying them out as hardware only will be a good experience. I don't know if it will be very difficult either, I have no experience. I studied VHDL in the early 90's and haven't used it since.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 4 years ago

    Thanks for opening this discussion.

    I am still at the same research point as you and I have the same doubts. Until I have time to make my first bare metal application on a soft MicroBlaze I will continue with the doubts.

    I'm going to order some PMOD modules without even looking if I'm going to be able to use them but I'm sure I'll find them useful in the future. There is HDL code for many PMODs in that repository, I think at least for now trying them out as hardware only will be a good experience. I don't know if it will be very difficult either, I have no experience. I studied VHDL in the early 90's and haven't used it since.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Metaforest
    Metaforest over 4 years ago in reply to javagoza

    Getting oriented with the Xilinx tools and the quirks of the Digilent board defs will have you cussing... but once you get oriented it is not to bad.  there is a flow...  and it does work...  but I warn you...  the teeth are curved in....   once you start down the correct path you don't have much flexibility to change it.  Adding unsanctioned IP is a pain in the ass but it is doable.

    Xilinx like many other IP managment companies has particular ways they want their IP used.   And outside their preferred development path there be dragons, brambles and razor sharp sheet metal!