FPGA
  • Technologies
  • More
FPGA
Forum Vivado installing on Windows without admin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 583 subscribers
  • Views 10315 views
  • Users 0 members are here
  • 7 Ways to Leave Your Spartan-6
  • vivado
  • Spartan_Migration
Related

Vivado installing on Windows without admin

computerton
computerton over 4 years ago

Hello guys,

While I'm anxiously waiting for my Arty S7 board, I wonder if anyone knows of a portable install of Vivado.

I'm going to use it on my work PC, because it's much faster than mine, and I don't have admin rights on it...

  • Sign in to reply
  • Cancel

Top Replies

  • dramoz
    dramoz over 4 years ago +2 verified
    Xilinx Tools (2021.2) (Ubuntu) (Main OS, as VM guest, or as WSL2/Windows) NOTE : DON’T forget to replace .x or <#> for the proper version of the tools when running the commands <#> is used so an error…
  • dramoz
    dramoz over 4 years ago in reply to javagoza +2
    If you upgrade to Windows 11 (or on Windows 10 using MobaXterm ) you will only need one installation on WSL2 (Ubuntu 20.04) as both will give you GUI/X11 access - the only issue I had when running WSL2…
  • misaz
    misaz over 4 years ago +1
    I think you can download full offline installer: It is .tar.gz, but if I remember correctly, SFD (single file download) always contained both Linux and Windows installers). In fact, I recommend use…
Parents
  • javagoza
    0 javagoza over 4 years ago

    I'm using windows but have two instances of Vivado one under Windows and another one under Ubuntu with the WSL2 windows subsystem for linux. The reason to have both is to be able to work with the Petalinux tools which work only under Linux or so I think.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to javagoza

    I'm doing the same. I use the WSL2 Linux one only when an example or library comes with Linux-only make scripts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to javagoza

    I'm doing the same. I use the WSL2 Linux one only when an example or library comes with Linux-only make scripts.