FPGA
  • Technologies
  • More
FPGA
Forum Vivado installing on Windows without admin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 583 subscribers
  • Views 10309 views
  • Users 0 members are here
  • 7 Ways to Leave Your Spartan-6
  • vivado
  • Spartan_Migration
Related

Vivado installing on Windows without admin

computerton
computerton over 4 years ago

Hello guys,

While I'm anxiously waiting for my Arty S7 board, I wonder if anyone knows of a portable install of Vivado.

I'm going to use it on my work PC, because it's much faster than mine, and I don't have admin rights on it...

  • Sign in to reply
  • Cancel

Top Replies

  • dramoz
    dramoz over 4 years ago +2 verified
    Xilinx Tools (2021.2) (Ubuntu) (Main OS, as VM guest, or as WSL2/Windows) NOTE : DON’T forget to replace .x or <#> for the proper version of the tools when running the commands <#> is used so an error…
  • dramoz
    dramoz over 4 years ago in reply to javagoza +2
    If you upgrade to Windows 11 (or on Windows 10 using MobaXterm ) you will only need one installation on WSL2 (Ubuntu 20.04) as both will give you GUI/X11 access - the only issue I had when running WSL2…
  • misaz
    misaz over 4 years ago +1
    I think you can download full offline installer: It is .tar.gz, but if I remember correctly, SFD (single file download) always contained both Linux and Windows installers). In fact, I recommend use…
Parents
  • dramoz
    +1 dramoz over 4 years ago

    Xilinx Tools (2021.2) (Ubuntu) (Main OS, as VM guest, or as WSL2/Windows)

    NOTE: DON’T forget to replace .x or <#> for the proper version of the tools when running the commands <#> is used so an error will be generated when running the command. This is a general guide to download 202x.x versions.

    You need a Xilinx account to download the tools, they are free and the registration process is easy. The Spartan-7 are supported on the free license.

    You can download the full unified installer or the web installer. Try first the Web Installer as it will save you some download time, but if your internet connection does not like it, get the full unified installer (you can use a downloader manager)

    I have not tried 2022.1 yet, the 2021.2 is working fine for me on Ubuntu 20.4

    The windows version is easier to deal with, as the drivers for programming the boards are installed with the tools, on Linux you have to do an extra step (not documented here)

    You don't need a powerfull machine to do Spartan-7 designs, a decent computer would suffice. By decent I mean an Intel Core (i3, i5) or equivalent AMD, with ~4GB of RAM (8GB recommended) (https://www.xilinx.com/products/design-tools/vivado/vivado-ml.html#memory)

    All tools version MUST match:

    • Vitis/Vivado

    Vitis (+Vivado)

    • Vitis is the software platform
    • Vivado is the hardware platform

    NOTE: Download Vitis installer, it covers Vivado. You will need Vitis if you plan to use Microblaze.

    Prerequisites

    # Dependencies
    sudo apt install -y libcanberra-gtk-module libcanberra-gtk-module:i386
    

    Install (as user, local)

    # Download installer
    # -> I prefer to download the Unified Installer ~80GB
    firefox --new-window https://www.xilinx.com/support/download/index.html/content/xilinx/en/downloadNav/vitis.html
    
    # Untar file
    cd dir_download_location
    tar -xvzf Xilinx_Unified_2021.<#>_1021_0703.tar.gz
    cd Xilinx_Unified_2021.<#>_1021_0703/
    
    # Launch Installer
    # you can run xsetup as sudo if you want a global installation
    # if it is just you, do a user installation
    mkdir ~/tools # -> for local installations
    
    ./xsetup
    # Select your target devices (Spartan-7)
    # Select DocNav (not required)
    # Install under your home directory
    # -> /home/user_name/tools/Xilinx
    ...
    # After installation is complete, DO NOT FORGET:
    sudo ~/tools/Xilinx/Vitis/2021.<#>/scripts/installLibs.sh

    ! Don't forget at the end to run installLibs.sh

    To launch the applications from the command line:

    # Vivado
    source ~/tools/Xilinx/Vitis/2021.<#>/settings64.sh
    cd ~/dev/xilinx/2021.x/vivado
    vivado
    
    # Vitis
    cd ~/dev/xilinx/2021.x/vitis
    source ~/tools/Xilinx/Vitis/2021.<#>/settings64.sh
    vitis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • computerton
    0 computerton over 4 years ago in reply to dramoz

    This is great! I already use Ubuntu on WSL1 and love it. I guess it's time to upgrade to WSL2!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • computerton
    0 computerton over 4 years ago in reply to dramoz

    This is great! I already use Ubuntu on WSL1 and love it. I guess it's time to upgrade to WSL2!