FPGA
  • Technologies
  • More
FPGA
Forum Zedboard - Vitis project works randomly
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 583 subscribers
  • Views 2057 views
  • Users 0 members are here
Related

Zedboard - Vitis project works randomly

jmh127
jmh127 over 4 years ago

Hi,

I’m using a Zedboard and when I run a program in Vitis, weirdly it doesnt work everytime. Inded, for the same program, sometime everything works as expected (uart print are succesfull, gpio: sw and led too) but sometime it doesn’t work.

It’s occurs often when I already did a run and I try to do a second one, but sometimes afer using the board for long it occurs just after power up the board.

I try to always build my project before and let the card cool down but sometimes it doesn’t help.

When it doesn’t work, many possibilities :

  • The application does absolutly nothing
  • The uart stop in the middle of a printf
  • an error appears like :

« Error while launcing program : reset APU.APB AP transaction error, DAP status 0xF0000021 »

or

« Error while lauching program : no taargets found with « name=~"APU*" ,avalailable targets :

  • 1 DAP (APB AP transaction error, DAP status 0x30000021)
  • 2 xc7z020 »

It's the case for all project I have created ...

This behavior is very handicapping for my work. If you are any idea please share it ! 

Regards,

Julie

  • Sign in to reply
  • Cancel
Parents
  • saadtiwana_int
    0 saadtiwana_int over 4 years ago

    Hi,
    From the error messages you have shared, it seems related to the programming of the board over JTAG.

    To start with, perhaps you can try using a different USB cable. Try to use a good quaity cable. Also, perform a visual inspection of the  (JTAG) USB connector on the Zedboard to make sure it's ok. Also, try a different USB port on your PC.

    Try these first and see if it makes any difference, before troubleshooting further.

    Best Regards,
    Saad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • saadtiwana_int
    0 saadtiwana_int over 4 years ago

    Hi,
    From the error messages you have shared, it seems related to the programming of the board over JTAG.

    To start with, perhaps you can try using a different USB cable. Try to use a good quaity cable. Also, perform a visual inspection of the  (JTAG) USB connector on the Zedboard to make sure it's ok. Also, try a different USB port on your PC.

    Try these first and see if it makes any difference, before troubleshooting further.

    Best Regards,
    Saad