FPGA
  • Technologies
  • More
FPGA
Forum How to write the contents of a text file to DDR RAM on the Arty S7-50 board (or any fpga)?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 584 subscribers
  • Views 8891 views
  • Users 0 members are here
  • xilinx
  • fpga
  • vivado
  • spartan-7
  • Arty S7 50
  • vitis
  • Spartan_Migration
Related

How to write the contents of a text file to DDR RAM on the Arty S7-50 board (or any fpga)?

cbohra00627
cbohra00627 over 4 years ago

I am trying to load a image directly to the DDR SDRAM on the Art S7 board. I have converted the jpg image into a txt file containing the integer RGB values for each pixel in separate lines. The file is as shown below:

goku.txt

Then I created a block design in vivado for microcontroller preset with uartlite and the MIG as shown below and programmed my fpga board with this design.

Block Design

Now, I am trying to open a file in Vitis and load the contents of the file byte by byte into the SDRAM memory locations with the code given below:

#include <stdio.h>
#include <stdlib.h>
#include "platform.h"
#include "xparameters.h"
#include "xil_io.h"
#include "xil_printf.h"

int main() {

	char line[2];
	int num = 0;
	int num_rec = 0;
	int i = 0;

	FILE *source = fopen("C:/Users/Chinmay/Desktop/goku.txt", "r");
	FILE *target = fopen("C:/Users/Chinmay/Desktop/goku_vitis.txt", "w");

	if ((source == NULL) || (target == NULL)) {
		xil_printf("File Failure");
		exit(1);
	}

	init_platform();

	while (fscanf(source, "%s", line) == 1) {
		num = atoi(line);
		Xil_Out8(XPAR_MIG7SERIES_0_BASEADDR + i, num);
		i++;
	}

	for (long int j=0; j<4; j++) {
		num_rec = Xil_In8(XPAR_MIG7SERIES_0_BASEADDR + j);
		fprintf(target, "%d\n", num_rec);
	}

	cleanup_platform();

	fclose(source);
	fclose(target);

	return 0;
}

Now, I doubt that my approach is wrong. In fact, I am getting some error when I try to build this code in vitis. The console output is given below:

22:44:58 **** Incremental Build of configuration Debug for project MIG1 ****
make all 
'Building file: ../src/main.cpp'
'Invoking: MicroBlaze g++ compiler'
mb-g++ -Wall -O0 -g3 -c -fmessage-length=0 -MT"src/main.o" -IC:/Users/Chinmay/Desktop/Verilog_Vivado/MIG1_Vitis/MIG1_wrapper/export/MIG1_wrapper/sw/MIG1_wrapper/standalone_microblaze_0/bspinclude/include -mno-xl-reorder -mlittle-endian -mxl-barrel-shift -mxl-pattern-compare -mcpu=v11.0 -mno-xl-soft-mul -Wl,--no-relax -ffunction-sections -fdata-sections -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.cpp"
'Finished building: ../src/main.cpp'
' '
'Building target: MIG1.elf'
'Invoking: MicroBlaze g++ linker'
mb-g++ -Wl,-T -Wl,../src/lscript.ld -LC:/Users/Chinmay/Desktop/Verilog_Vivado/MIG1_Vitis/MIG1_wrapper/export/MIG1_wrapper/sw/MIG1_wrapper/standalone_microblaze_0/bsplib/lib -mlittle-endian -mxl-barrel-shift -mxl-pattern-compare -mcpu=v11.0 -mno-xl-soft-mul -Wl,--no-relax -Wl,--gc-sections -o "MIG1.elf"  ./src/main.o ./src/platform.o   -Wl,--start-group,-lxil,-lgcc,-lc,-lstdc++,--end-group
d:/xilinx/vitis/2021.2/gnu/microblaze/nt/x86_64-oesdk-mingw32/usr/bin/microblaze-xilinx-elf/../../libexec/microblaze-xilinx-elf/gcc/microblaze-xilinx-elf/10.2.0/real-ld.exe: MIG1.elf section `.text' will not fit in region `microblaze_0_local_memory_ilmb_bram_if_cntlr_Mem_microblaze_0_local_memory_dlmb_bram_if_cntlr_Mem'
d:/xilinx/vitis/2021.2/gnu/microblaze/nt/x86_64-oesdk-mingw32/usr/bin/microblaze-xilinx-elf/../../libexec/microblaze-xilinx-elf/gcc/microblaze-xilinx-elf/10.2.0/real-ld.exe: region `microblaze_0_local_memory_ilmb_bram_if_cntlr_Mem_microblaze_0_local_memory_dlmb_bram_if_cntlr_Mem' overflowed by 88968 bytes
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:50: MIG1.elf] Error 1

22:45:00 Build Finished (took 1s.910ms)

At the end of the 12th line, it says "region `microblaze_0_local_memory_ilmb_bram_if_cntlr_Mem_microblaze_0_local_memory_dlmb_bram_if_cntlr_Mem' overflowed by 88968 bytes". So, my guess is that when I try to open the file, it first gets loaded into the BRAM which has less capacity than the file itself. Well, I might be wrong because when I tried to load a small 1KB file, it showed the same error.

I am stuck here. Is there any way through which I can load my file directly into the SDRAM? The size of my file is around 8MBs.

Actually I am trying to implement image processing on FPGA. I need to load an image on the board, then I will make a image processing IP in vitis HLS and use it in my design.

  • Sign in to reply
  • Cancel

Top Replies

  • saadtiwana_int
    saadtiwana_int over 4 years ago in reply to cbohra00627 +2 verified
    On your linker script screenshot, as i remember, the "memory region" values are drop-down items. Right now everything is assigned to be saved to bram (as you can see in your screenshot). You can use the…
  • Metaforest
    Metaforest over 4 years ago +2
    Make sure you have built and run the memory and platform test projects. Make sure you understand how they work. Including the base address configuration in your Object diagram. Prove you can read and write…
  • saadtiwana_int
    saadtiwana_int over 4 years ago in reply to cbohra00627 +1
    Glad it worked for you. So one way that i can think of to know where your array is stored at, is by looking the address of the variable. In one of the screenshots you shared above, the bram has the address…
Parents
  • ehernand
    0 ehernand over 3 years ago

    How did you convert the jpg image into a txt file containing the integer RGB values for each pixel in separate lines?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ehernand
    0 ehernand over 3 years ago

    How did you convert the jpg image into a txt file containing the integer RGB values for each pixel in separate lines?