FPGA
  • Technologies
  • More
FPGA
Forum Crypto Mining on FPGA Board!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 583 subscribers
  • Views 4467 views
  • Users 0 members are here
  • fpga
  • spartan-7
  • Spartan_Migration
Related

Crypto Mining on FPGA Board!

cbohra00627
cbohra00627 over 4 years ago

I was wondering if I could somehow do some crypto mining on my Arty S7-50 board. I know that it might not be much profitable. ASICs are better for this job. But I want to try it just for education purposes.

What does the members think? Will it be profitable i.e. will it be able to mine enough amount of crypto to cover the electricity cost? Where do I start from?

  • Sign in to reply
  • Cancel

Top Replies

  • jure
    jure over 4 years ago +5
    I haven't looked deeply into it, but as far as I know, it isn't easy to implement. There is also the fact that you need to connect it to the internet, which could be done through an ethernet module or…
  • Jan Cumps
    Jan Cumps over 4 years ago +3
    If the design fits, it will not be profitable
  • jc2048
    jc2048 over 4 years ago +3
    That's impossible to answer because it depends on how clever you are. 'Hard problems' aren't impossible problems, they just take a long time to accomplish using the algorithms that everyone knows about…
Parents
  • jure
    jure over 4 years ago

    I haven't looked deeply into it, but as far as I know, it isn't easy to implement. There is also the fact that you need to connect it to the internet, which could be done through an ethernet module or by communicating with a host PC (you would be limited by the Baud rate probably). In any way, it would be challenging to implement on a single standalone FPGA without using any high-speed communication protocol (USB 2.0 or higher) or even PCIe. It would probably be much easier using an Arty A7 (due to integrated Ethernet). Still, it would probably be much easier to implement into an SoC. There are some boards on AliExpress that are less than 50€ and would suit the needs a lot better (EBAZ4205, colorlight i5/i9) along with the fact that new FPGA boards are getting more and more expensive.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • cbohra00627
    cbohra00627 over 4 years ago in reply to jure

    Yeah, you are right. The Arty S7 doesn't have any ethernet port.

    I guess I will do some research by myself and see if it is possible in any way or not.

    Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cbohra00627
    cbohra00627 over 4 years ago in reply to jure

    Yeah, you are right. The Arty S7 doesn't have any ethernet port.

    I guess I will do some research by myself and see if it is possible in any way or not.

    Thanks!