FPGA
  • Technologies
  • More
FPGA
Forum Trying to generate a modern kernel dts for avnet-uz7ev-cc board.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 580 subscribers
  • Views 2307 views
  • Users 0 members are here
Related

Trying to generate a modern kernel dts for avnet-uz7ev-cc board.

brianmckee
brianmckee over 3 years ago

I'm using kernel 6.4.2 and the Xilinx source code appears to work for Xilinx boards, based on the presence of the dts files.

I have created avnet-uz7ev-evcc.dts and have been slowly bringing features on line by studying documentation, schematics and other dts files.

I have USB, i2c, Ethernet, and SATA working.

I'm working on DisplayPort at the moment. DisplayPort works when I boot the 2022.1 example image provided by avnet.

With my kernel, these are the only two error messages I'm getting:

[    8.294252] zynqmp-dpsub fd4a0000.display: DP output port not connected
[    8.294281] zynqmp-dpsub: probe of fd4a0000.display failed with error -22

I checked the source code and this appears to be a device tree issue.

I'm not entirely sure what is going on, but I have a question about setting the phy for DP.

On the 7ev card carrier board, the display port has only one lane. This creates issues with my monitor, but I have found a work around.

According to the main line kernel: xlnx,zynqmp-dpsub.yaml:

phys:
description: PHYs for the DP data lanes
minItems: 1
maxItems: 2
phy-names:
minItems: 1
items:
- const: dp-phy0
- const: dp-phy1

The example is:

phys = <&psgtr 1 PHY_TYPE_DP 0 3>,
<&psgtr 0 PHY_TYPE_DP 1 3>;

According to psgtr documentation:
properties:
  "#phy-cells":
    const: 4
    description: |
      The cells contain the following arguments.

      - description: The GTR lane
        minimum: 0
        maximum: 3
      - description: The PHY type
        enum:
          - PHY_TYPE_DP
          - PHY_TYPE_PCIE
          - PHY_TYPE_SATA
          - PHY_TYPE_SGMII
          - PHY_TYPE_USB3
      - description: The PHY instance
        minimum: 0
        maximum: 1 # for DP, SATA or USB
        maximum: 3 # for PCIE or SGMII
      - description: The reference clock number
        minimum: 0
        maximum: 3

I think I need to set the phys to this:

       phy-names = "dp-phy0";
       phys = <&psgtr 3 PHY_TYPE_DP 1 3>;

But that, and many other combinations, doesn't work.

I'm not sure what the PHY instance is supposed to be.

I have tried 0, 1 and 3 but, I'm not sure I tried all combinations as I wasn't methodical.

I'm not seven sure this is the issue because SATA and USB work without having to set PHYS.

If anyone can offer help, I'd really appreciate it.

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +1
    yes, it is device tree issue. You might need to define &psgtr clock for DP at system-user.dsti. I might not be right for your case. However, I found that DP &psgtr need some device tree setup at system…
Parents
  • flyingbean
    0 flyingbean over 3 years ago

    yes, it is device tree issue. You might need to define &psgtr clock for DP at system-user.dsti. I might not be right for your case. However, I found that DP &psgtr  need some device tree setup at system-user.dsti after Petalinux 2021. If you cannot find solution until end of this month,  I might have time to help you with that. I might have time for the trouble-shooting after the coming week.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brianmckee
    0 brianmckee over 3 years ago in reply to flyingbean

    Are you using peta-linux? I'm using the mainline kernel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • flyingbean
    0 flyingbean over 3 years ago in reply to brianmckee

    Yes. I am using Petalinux. I don't know how to use mainline kernel under Yocto flow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • flyingbean
    0 flyingbean over 3 years ago in reply to brianmckee

    Yes. I am using Petalinux. I don't know how to use mainline kernel under Yocto flow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • brianmckee
    0 brianmckee over 3 years ago in reply to flyingbean

    If I can get the mainline kernel working, then getting a yocto flow working will be way easier. However, generating the device tree for the PL is probably way more complicated that way. But that's my plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • flyingbean
    0 flyingbean over 3 years ago in reply to brianmckee

    Since the platform is Xilinx, I would like to use Petalinux to generate device tree files for the targeted Xilinx FPGA, which can be used as a reference for your mainline kernel development.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brianmckee
    0 brianmckee over 3 years ago in reply to flyingbean

    The Xilinx kernel is very outdated and uses a very different set of device tree descriptors and, as I understand, there's even a difference in the drivers.

    I don't want to be stuck on kernel 5.15 as there are many changes since then.