FPGA
  • Technologies
  • More
FPGA
Forum Suggestions for designing with ZYNQ MPSoC UltraScale+ ZCU104: Using PS side DDR4 memory for storing trained weights and biases of Convolutional Neural Network(CNN) for implementation of CNN inference in real-time.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 578 subscribers
  • Views 1633 views
  • Users 0 members are here
  • ddr4
  • cnn
  • fpga
  • zynq mpsoc
  • verilog
  • xili
Related

Suggestions for designing with ZYNQ MPSoC UltraScale+ ZCU104: Using PS side DDR4 memory for storing trained weights and biases of Convolutional Neural Network(CNN) for implementation of CNN inference in real-time.

BinitKP
BinitKP over 2 years ago

I have trained weights and biases from a CNN network for different layers. I have converted those data into fixed point 16-bit binary format and saved them as .txt files for different convolutional layers. Since the data files are too large to accommodate them into BRAM (On-chip memory), I need to use external PS side DDR4 memory to store those.

However, I don't understand how I can store those data in DDR4 memory for simulation purposes as the Verilog function of $readmemb() says out of memory in the Vivado while loading a single file as I think it is taking the BRAM only; which is too small in capacity.

So, please guide me on how to approach the simulation and then real-time inference operation after making the equivalent CNN using Verilog HDL coding, whether my approach is correct or if I need to approach it another way.

Attached are the file organization and sample contents for reference.

imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • JB58
    0 JB58 over 2 years ago

    I believe you can mimic the behavior of the data transfer engine from DDR to your internal module inside your testbench! Am I right?

    You can read the .txt file in your testbench, and handle the hand shake required for your data transfer in your simulation bench. I am assuming you are using AXI_DMA, reading the data in AXI_MM world and your module wrapper is AXI_S compatible which makes it easier. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • JB58
    0 JB58 over 2 years ago

    I believe you can mimic the behavior of the data transfer engine from DDR to your internal module inside your testbench! Am I right?

    You can read the .txt file in your testbench, and handle the hand shake required for your data transfer in your simulation bench. I am assuming you are using AXI_DMA, reading the data in AXI_MM world and your module wrapper is AXI_S compatible which makes it easier.