FPGA
  • Technologies
  • More
FPGA
Forum Snickerdoodle board on FLOSS Weekly
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 584 subscribers
  • Views 7259 views
  • Users 0 members are here
  • floss
  • open_source
  • crowd_supply
  • fpga
  • snickerdoodle
  • podcast
Related

Snickerdoodle board on FLOSS Weekly

fustini
fustini over 10 years ago

The Snickerdoodle board (featuring the Xilinx Zynq) was featured on FLOSS Weekly yesterday:


FLOSS Weekly #360

https://twit.tv/shows/floss-weekly/episodes/360?autostart=false

An affordable platform for powering everything robots, drones, and computer vision.


Snickerdoodle is a $55 hybrid development board that has an ARM application processor with an onboard FPGA.  Ryan Cousins (rcousins) cousins of krtkl (the creators) and David Scheltema (interested1) of MAKE magazine join Randal and Aaron to discuss the board.


Here's the episode on YouTube:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

cheers,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 10 years ago in reply to fustini +2
    Drew: I hope that they will release schematics, PCB layout and BOM. Schematics and BOM definitely, never really understood the need for PCB layout unless there is a layout related problem. If there is…
  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor +2
    My, but you guys have a serious attitude issue !! I'm the original writer referred to here: My interpretation was that the original writer was *complaining* about having to boot a full blown multi-megabyte…
  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor +2
    No - don't go - this is one of the most interesting threads on E14 in while ! I just told myself to get on with some work until I saw that bit on your post. Re: Software/Hardware - it seems to me that…
  • johnbeetem
    johnbeetem over 10 years ago in reply to e14 Contributor

    Ryan Cousins wrote:

     

    John Beetem By that logic, no ARM or x86 project or platform could *ever* be considered "FLOSS." Is anyone expecting ARM or Intel to provide the masks for their chips? How do you change the arrangement of the gates on the STM32 sitting on my desk? I'm a bit confused as to why FPGAs are somehow held to a different standard of "openness" than any other (closed) silicon component simply because they give you more granular control over the function and configuration of the chip. Oh, and the tools are free.

    ARM and x86 silicon is not software.  It's hardware.  It's proprietary hardware and nobody expects ARM or x86 to become OSHW.

     

    However, ARM and x86 silicon are a hardware platform that can be used for FLOSS (Free-as-in-Liberty Open-Source Software).  The ARM and x86 intruction sets are published, including both assembly language and their binary codings.  So as a programmer, you can write FLOSS that runs on those platforms and when you distribute source code your users have the option of modifying your source code for their own needs and recompiling it for their hardware.

     

    In addition, you can write a compiler for any language you want and generate ARM or x86 machine language.  You are not dependent on the chip maker.  You are not required to use (for example) PL/M for the x86 machine or (as a silly example) APL for the ARM.  You buy the chip, the manufacturer tells you what the instruction bits do, and you can write whatever software you want.  You have freedom.

     

    You don't get that kind of freedom with FPGAs other than iCE40.  You can't write your own compiler because you don't know what the machine-language bits do.  You have to use the Free-as-in-Beer tools from the FPGA vendor.  If they don't do what you want there's nothing you can do about it.  Yes, that's adequate for the majority of FPGA users and you can produce useful chips -- I do this professionally as a free-lance FPGA designer.  But there are a bunch of things that are impractical.  My favorite example is reconfigurable computing: FPGA tool bottleneck stalls HPC.  Reconfigurable computing doesn't sell a lot of chips for an FPGA vendor, so there's no motivation for them to produce tools that support it.  If FPGAs supported FLOSS, that wouldn't be a problem: other people could create that software.  The fact that the bitstream formats are proprietary means that they can't, and an amazingly useful FPGA application is stalled.

     

    I'm not asking Xilinx or any other FPGA vendor to provide masks, just like I don't expect Intel or ARM to document how they implement their instruction sets.  I just want to know how to set the bits in FPGA bitstreams to perform the functions documented in their architecture documentation.  That's all I need for FLOSS.

     

    Hope this helps image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 10 years ago in reply to johnbeetem

    << but the GPU is a small part of BeagleBoard/Bone and many projects don't need it and can therefore be fully FLOSS.

     

    >> And others do need it which makes it not FLOSS. Is this some kind of quantum FLOSS ? You make this argument

    all the time and it still does not make sense. By the very definition there is no FLOSS when your SoC contains proprietary

    hardware no matter how fine you try (and try, and try) to split that hair.

     

     

    << As I understand it, the Broadcom documentation doesn't really give you enough information to write your own operating system and you must reverse-engineer from the Linux source code and use a "binary blob" to boot the GPU.

     

    >> BSD ? RISCOS ? There has also bee a port to an RTOS. I don't remember which RTOS but I was part of a

    discussion about porting it in these forums and the person trying to do it made the same argument as you. After

    pointing him to the Broadcom documentation he was able to complete the port. Your "understanding" needs updating.

     

    >> Since the GPU documentation has been released, an assembler and disassembler have been made available

    which allows anyone to disassemble the boot code. Since BSD, RISCOS, a couple of bare metal projects and

    the RTOS port I spoke of earlier use the existing boot loader, I'm not sure why using the binary blob is such a

    bad thing but it is nice to be able to produce an alternative.

     

     

    << OTOH, they do document the GPU but I haven't heard whether RasPi users have been successful writing their own GPU applications and integrating them into actual RasPis.

     

    >> I have seen a couple of projects that do. Google it with "using raspberry pi GPU" and learn.

     

     

    << If the proprietary tools don't give you the correct result, you can't go into the source code and figure out why.

     

    >> I probably couldn't figure it out even if I had the source code. High speed logic routing and optimization

    of large FPGA designs is beyond my skill set and I would venture a guess that it is beyond yours and most

    other peoples' in the business as well.

     

     

    << "Synthesizing an FPGA in an FPGA" can be useful, but as far as I can tell it makes terribly inefficient

    use of silicon resources and you cannot get good performance. 

     

    >> I'm not real big on this idea either for exactly the same reason.

     

     

    << I think my Flavia project Flavia: the Free Logic Array is a wonderful tool for teaching about programmable logic, since it's small and fast: you can recompile and download a small design in a second or two.  IMO that's awesome compared to the longueurs you face using proprietary tools -- assuming you have the patience to download them in the first place and get the license to work.  OTO FH,lavia is really only suitable for small projects.  You can do a much bigger project with a tiny Lattice iCE40-HX1K and IceStorm than you can do with Flavia and the much larger Xilinx Spartan-6 LX9.

     

    >> As you say, the Vivado Design Suite is not a tool for teaching about programmable logic. It is a fully

    professional tool for creating large, high speed logic designs. Comparing these two objectives and the

    complexity of the tools needed are like comparing building and an Estes model rocket to a Saturn V. It

    just doesn't work as a reasonable argument.

     

    >> It took about 20 minutes to download the 6.9 GB VDS and another few minutes to download some other files.

    Modern high speed Internet (mine is "only" 50 Mb/s although I have seen it hit, but not hold closer to 80 on

    one or two occasions) is a wonderful thing. YMMV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem

    ARM and x86 silicon is not software.  It's hardware.  It's proprietary hardware and nobody expects ARM or x86 to become OSHW.

     

    However, ARM and x86 silicon are a hardware platform that can be used for FLOSS (Free-as-in-Liberty Open-Source Software).  The ARM and x86 intruction sets are published, including both assembly language and their binary codings.  So as a programmer, you can write FLOSS that runs on those platforms and when you distribute source code your users have the option of modifying your source code for their own needs and recompiling it for their hardware.

     

    In addition, you can write a compiler for any language you want and generate ARM or x86 machine language.  You are not dependent on the chip maker.  You are not required to use (for example) PL/M for the x86 machine or (as a silly example) APL for the ARM.  You buy the chip, the manufacturer tells you what the instruction bits do, and you can write whatever software you want.  You have freedom.

     

    Again, this part has an ARM processor.

    << "Synthesizing an FPGA in an FPGA" can be useful, but as far as I can tell it makes terribly inefficient

    use of silicon resources and you cannot get good performance.

     

    >> I'm not real big on this idea either for exactly the same reason.

     

    Neither am I, but it *is* possible...and you can make it as proprietary or open as you'd like. I can almost taste the freedom.

     

    << If the proprietary tools don't give you the correct result, you can't go into the source code and figure out why.

     

    >> I probably couldn't figure it out even if I had the source code. High speed logic routing and optimization

    of large FPGA designs is beyond my skill set and I would venture a guess that it is beyond yours and most

    other peoples' in the business as well.

     

    Indeed. Unfortunately this is a slightly different situation than messing something up and just doing a 'core dump' and starting over. If you decide you're more qualified than the chip/tool designers (and their 100s of thousands/millions of hours of experience and their army of engineers) to figure out what they've been doing wrong all this time and you start fiddling with the timing/optimization of these parts at the gate level, you're about 1,000x more likely to do something that's going to result in screwing something up so badly that the parts gets so hot that they melt solder and fall off the PCB than you are to find a better solution - regardless of the warm fuzzies you might experience along the way.


    On the other hand, it would be kinda cool to see...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 10 years ago in reply to e14 Contributor

    Ryan,

     

    I know, I know. I checked it out first thing this morning !! Now the really hard part, waiting for March 2016.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    "you need a full blown OS which implies many megabytes of code"

     

    With regards to the Zynq specifically this is actually a completely false statement. The free Xilinx tools are designed to target Linux, FreeRTOS and *bare metal* and will include C driver files for any peripherals you use (like configuring the DDR at startup etc.).   You can go right ahead and write a 5 line program in main.c and load/execute it over JTAG just like a microcontroller and w/o any operating system.   This is totally supported by Xilinx and in fact is the way that most of the tutorials at http://zynqbook.com are done.    This is no suprise as you need to keep in mind that the very serious industries in which Zynq is used don't just care about slapping 10 million lines of buggy "off-the-shelf" code into a Linux powered multimedia appliance so they can make the next 8 week product cycle deadline.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem

    So if you have a closed-source binary bitstream for the FPGA that implements a GPU/DSP/accelerator and you openly provide the instruction set that that closed HDL source accelerator executes (Which is also synthesized with a closed source FPGA toolchain).

     

    Then all of a sudden that would be open-source?

     

    Because that's precisely how most semiconductor IP is deployed --- like the ARM or GPU on your RPi/Arduino/BeagleBone

    But magically they are more "open source" than Zynq?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    Hi Jamil,

     

    You may have a great product, but your last two comments are quite rude. You only quoted a portion of the sentence, it actually said

    "in order to get it to do anything much (ie to make serious use of the processor) you need a full blown OS" and that is the case.

    Who has the time to re-write the tens of thousands of lines of code that are present in rich Linux libraries to run bare-metal?

    To make intensive use of an application processor in a practical amount of time, you do need the support of a full-blown OS.

    With all the associated problems of having a team to manage the OS, packages and build.

     

    It seems a team-wide issue. Your colleague (Ryan) was also rude on hackaday to makers in general when he said (quote):

    ""I am coming to the realization (maybe a little too late) that “makers” really aren’t interested in building anything beyond a LED-enabled garage door opener or an automated cat feeder."

     

    If makers are your target market, then you and your team might want to be polite to potential customers.

     

    Someone else on hackaday said to Ryan "You should really have a friendlier person handling your social media presence. I know you probably didn’t intend it, but you kinda came off as a xyz".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz

    shabaz In reference to the partial conversation you quoted, I subsequently apologized to this person on Hackaday

     

    <<Hi xxx and everyone – I apologize. I haven’t slept much recently…or in a long time. I haven’t had a decent meal in weeks. I haven’t seen a lot of my closest friends in months. I literally wake up and do nothing but work on this project all day every day 7 days a week. It’s not a hobby or a past time. It’s my life. Needless to say, it means a lot to me.

    I don’t expect everyone to agree with what we’re doing or find it interesting or really care about us or our project for that matter. I do occasionally let my frustration get the better of me when I hear people badmouthing or second-guessing our intentions, our ability, our dedication, and, in some cases, our integrity. And for that, I am sorry.

    We have put more of our time, bodies, and souls into this than most would consider reasonable or even humanly possible. We’ve been told – and continue to be told – it’s a bad idea and that we should give up and do something different/easier for more reasons and by more people than I can count.

    Ultimately, if we can’t get anyone else to buy into the *vision* of what we’re proposing to provide, there’s really no one to blame but ourselves. And if that’s that case, it’s just something we’ll have to live with.

    So again, my apologies for coming off as a **. My emotions got the better of me.>>

     

    Not sure if you've ever been part of a crowdfunding campaign or a public product launch but to say it's a stressful time would be a severe understatement. I got caught up in the moment (after taking countless personal and professional bashings for a product we'd just released into the wild a few days prior). The moment passed and I have since had dozens of fruitful and civil conversations with the folks at Hackaday and the folks here at Element, like yourself. Only time will tell how the maker audience receives our product, but we certainly hope the initial dream when we started on this project - of making professional-caliber development tools more accessible and usable for makers, students, and hobbyists so that they may take their projects to the next level and directly contribute to the next generation of great technological advances - comes to fruition.

     

    And I'd have to politely disagree with your statement that this was being misrepresented:

    "in order to get it to do anything much (ie to make serious use of the processor) you need a full blown OS" and that is the case.

     

    in the sense that these two statements: "in order to get it to do anything much" and "to make serious use of the processor" contradict each other (or, at the very least, one does not imply the other). Maybe to "make serious use of the processor" typically does involve a full-blown OS. But it's just not true that you need a full blown OS to "get it to do anything much." Unless I am misunderstanding what you are saying or you see it differently?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    Hi Ryan,

     

    I'm not going to comment any more on the rest, but regarding the OS issue, everyone's opinion on what 'serious use' (which is how the text 'do anything much' was qualified in the original text) means could vary. Serious use means different things to different people, as does doing anything much. I interpret serious use as "using modern protocols, application frameworks and software services which by nature entail using many of the building blocks of the built-in SoC". These would in a lot of cases entail the use of an OS such as Linux in practice. And in other peoples opinion serious use may not mean the same thing at all.

    Basically, a body of engineers would agree, and a body of engineers may disagree, and

    there is no harm in that.

    Which is why it is odd for someone to say it is a "completely false statement" in bold

    and italics on this point.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz

    Fair enough, shabaz. Not trying to beat this into submission or anything but (formatting aside), I think you gotta admit that "do anything much" is a generalization - and, contextually or not, it is actually not true. I totally appreciate that this particular comment was being made from one individual's point of view. But there are thousands (or more) of application examples taking full advantage of  uPs yet are not running any sort of OS (i.e. bare metal).

     

    Naturally every system is different and different approaches to the same problem can be equally valid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>