FPGA
  • Technologies
  • More
FPGA
Forum What FPGA content would you like to see?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 586 subscribers
  • Views 5304 views
  • Users 0 members are here
  • fpgafeatured
  • fpga
Related

What FPGA content would you like to see?

e14phil
e14phil over 9 years ago

FPGA and element14

 

I am very happy to say we have lots of big, exciting things in the pipeline for FPGA and the extended element14 family, but I want to take this time to ask the community what FPGA content interests you?

 

Do you want some reviews of FPGA kit?

Do you want Tutorials, if so on what?

What would help you to work with FPGA?

 

We have some things in the works but we always want to add quality content to our community.

 

If you have something you want to share in the FPGA space but want help, kit or just to run it past us, we will always try help!

 

- Your Friendly Neighborhood e14phil

  • Sign in to reply
  • Cancel

Top Replies

  • pettitda
    pettitda over 9 years ago +7
    1) tutorials on VHDL and/or Verilog 2) tutorials on vendor tools (i.e. Xilinx, Altera, Modelsim?) 3) information on where FPGAs have advantage over microcontrollers/processors (i.e. parallel versus serial…
  • rscasny
    rscasny over 9 years ago in reply to pettitda +5
    David, Thanks for the feedback. You pretty much read my mind and my plan. I have been looking at tutorial content to see what's viable. I have been thinking about bringing in tutorials on the Vivado Design…
  • e14 Contributor
    e14 Contributor over 9 years ago +5
    Im enthusiastic to work more with fpga's, after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here. Also I want to…
Parents
  • e14 Contributor
    e14 Contributor over 9 years ago

    Im enthusiastic to work more with fpga's, after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here.

     

    Also I want to add a graphical interface of some sort (lcd) so I'll likely use a small board computer for that part as I feel that would be easier and an fpga for the bus reading and decoding and make a standalone piece of test equipment so expect some more content from me image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to e14 Contributor

    lucie tozer wrote:

     

    Im enthusiastic to work more with fpga's, after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here.

     

    Also I want to add a graphical interface of some sort (lcd) so I'll likely use a small board computer for that part as I feel that would be easier and an fpga for the bus reading and decoding and make a standalone piece of test equipment so expect some more content from me

    lucie tozer wrote:

    ... after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here.

     

    ...

    I blatantly stole someone's design image

     

    The Papilio boards and Dangerous Prototypes LogicSniffer are virtually the same hardware - except input protection and level shifting.

    So the only thing I did is to make input protection board and load the LogicSniffer bitstream (I just changed some pull-up settings in the constraint file - the standard ones loaded some circuits a bit too hard).

    I've got a blog on that here on e14. I'll search it ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to e14 Contributor

    lucie tozer wrote:

     

    Im enthusiastic to work more with fpga's, after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here.

     

    Also I want to add a graphical interface of some sort (lcd) so I'll likely use a small board computer for that part as I feel that would be easier and an fpga for the bus reading and decoding and make a standalone piece of test equipment so expect some more content from me

    lucie tozer wrote:

    ... after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here.

     

    ...

    I blatantly stole someone's design image

     

    The Papilio boards and Dangerous Prototypes LogicSniffer are virtually the same hardware - except input protection and level shifting.

    So the only thing I did is to make input protection board and load the LogicSniffer bitstream (I just changed some pull-up settings in the constraint file - the standard ones loaded some circuits a bit too hard).

    I've got a blog on that here on e14. I'll search it ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    Here is the explanation:

     

    Make a Logic Analyzer from your Dev Kit Part 2: Papilio FPGA