FPGA
  • Technologies
  • More
FPGA
Forum What FPGA content would you like to see?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 586 subscribers
  • Views 5306 views
  • Users 0 members are here
  • fpgafeatured
  • fpga
Related

What FPGA content would you like to see?

e14phil
e14phil over 9 years ago

FPGA and element14

 

I am very happy to say we have lots of big, exciting things in the pipeline for FPGA and the extended element14 family, but I want to take this time to ask the community what FPGA content interests you?

 

Do you want some reviews of FPGA kit?

Do you want Tutorials, if so on what?

What would help you to work with FPGA?

 

We have some things in the works but we always want to add quality content to our community.

 

If you have something you want to share in the FPGA space but want help, kit or just to run it past us, we will always try help!

 

- Your Friendly Neighborhood e14phil

  • Sign in to reply
  • Cancel

Top Replies

  • pettitda
    pettitda over 9 years ago +7
    1) tutorials on VHDL and/or Verilog 2) tutorials on vendor tools (i.e. Xilinx, Altera, Modelsim?) 3) information on where FPGAs have advantage over microcontrollers/processors (i.e. parallel versus serial…
  • rscasny
    rscasny over 9 years ago in reply to pettitda +5
    David, Thanks for the feedback. You pretty much read my mind and my plan. I have been looking at tutorial content to see what's viable. I have been thinking about bringing in tutorials on the Vivado Design…
  • e14 Contributor
    e14 Contributor over 9 years ago +5
    Im enthusiastic to work more with fpga's, after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here. Also I want to…
Parents
  • e14 Contributor
    e14 Contributor over 9 years ago

    Im enthusiastic to work more with fpga's, after my current project I intend to make a multi protocol analyzer, Jan Cumps mentioned he's made one using an fpga so I might follow suit here.

     

    Also I want to add a graphical interface of some sort (lcd) so I'll likely use a small board computer for that part as I feel that would be easier and an fpga for the bus reading and decoding and make a standalone piece of test equipment so expect some more content from me image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to e14 Contributor

    Once you had that going, it might be interesting to see if you could move the processor to the FPGA. A custom processor, designed to be good at the kind of tasks you'd want in such an embedded type application, might look quite different to the kind of thing we're all used to which has to be a 'Jack of all trades'.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to jc2048

    That would be awesome but thats probably out of my depth, and probably more than just 1 person can manage. My first thoughts are a custom processor needs a custom command set and then a custom compiler for a higher level language to make it functional for things like graphical work.

     

    Maybe its not as complicated as that though, I might look into it as a potential option. Right now Im not proficient enough with FPGA's to develop a processor inside one!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to e14 Contributor

    The vendors have code for soft processors.

     

    The Altera one is called NIOS. Downside is that I think you have to pay for licence if you ship it as part of a product.

     

    Xilinx have the PicoBlaze (8 bit) and MicroBlaze (32 bit) - they seem to be free for development but again may have licence restrictions (I haven't looked in detail).

     

    I don't have any experience of either, so can't say how easy they are to use or what the supporting toolchains are like.

     

    If you had a look at the code for the PicoBlaze it would give you an idea of what's involved with a very simple microcontroller - that will be about as simple as it gets, unless you did a calculator-style 4-bit processor. Copy Intel's 4004 maybe? https://en.wikipedia.org/wiki/Intel_4004

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to jc2048

    Alternatively there are SoC type FPGA's which have a whole bunch of stuff including Ethernet, Memory controllers, an ARM core etc all tightly coupled with the FPGA fabric. Something like the MicroSemi SmartFusion2 range: https://www.microsemi.com/products/fpga-soc/soc-fpga/smartfusion2#product-tables

     

    Then do what makes most sense in traditional software on the ARM core and build custom hardware in the FPGA part for where this can really help out.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago in reply to jc2048

    Alternatively there are SoC type FPGA's which have a whole bunch of stuff including Ethernet, Memory controllers, an ARM core etc all tightly coupled with the FPGA fabric. Something like the MicroSemi SmartFusion2 range: https://www.microsemi.com/products/fpga-soc/soc-fpga/smartfusion2#product-tables

     

    Then do what makes most sense in traditional software on the ARM core and build custom hardware in the FPGA part for where this can really help out.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gdstew
    gdstew over 9 years ago in reply to rachaelp

    There is also the Xilinx Zynq-7000 series which have single or dual core ARM processors and 25K -  85K logic cells (~400K to ~1.3M "ASIC gates")  FPGAs.

    There are a couple of companies that offer boards based on these chips (I bought a Snickerdoodle), they are fairly expensive starting at ~95 USD but they

    also have SDRAM, a large number of available I/O connections to the ARM core peripherals and the FPGA, and in the case of the Snickerdoodle, Wi-Fi.

    • Cancel
    • Vote Up +4 Vote Down