FPGA
  • Technologies
  • More
FPGA
Forum In Preparation for the AVNET MiniZed (Xilinx Zynq XC7Z007S SoC) RoadTest. What Do You Need?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 573 subscribers
  • Views 5576 views
  • Users 0 members are here
  • scasny
  • avnet
  • xilinx
  • avnet_rt
  • fpga
  • xilinx zynq soc
Related

In Preparation for the AVNET MiniZed (Xilinx Zynq XC7Z007S SoC) RoadTest. What Do You Need?

rscasny
rscasny over 8 years ago

We will be roadtesting the AVNET MiniZed FPGA SoC development board in September. I find this to be an exicting prospect and can't wait to let it loose on the element14 community.

 

In brief, the MiniZedTm is a single-core Zynq 7Z007S development board. This board targets entry-level Zynq developers with a low-cost prototyping platform.image

 

The Minized's compact design features on-board connectivity through USB, Wi-Fi and Bluetooth. Peripherals can be plugged into dual Pmod-compatible connectors, the Arduino-compatible shield interface or the USB 2.0 host interface. JTAG circuitry is incorporated onto the MiniZed base board, so with a single micro-USB cable to your laptop you are already up and running. User LED’s, a button and a switch allow for a physical board interface.

 

Micron memory solutions are presented for QSPI flash, DDR3L memory and on-board eMMC instead of an external SD card. The Murata Type 1DX wireless solution incorporates 802.11b/g /n Wi-Fi as well as Bluetooth 4.1, which provides both Bluetooth Classic and Low Energy (BLE). The integrated power supply from Dialog generates all on-board voltages, while an auxiliary supply input can be used to power designs that require additional current. From ST Micro there is an on-board motion and temperature sensor, as well as a digital microphone.

 

MiniZed provides for an efficient hardware reference design, while it is also an inexpensive board that can be used to run workshops and tutorials. The board aims to showcase the power of Zynq, where the Cortex A9 processor core integrates seamlessly with the programmable fabric to provide signal processing and control solutions. The on-board digital microphone serves as an input for a variety of illustrations of how to implement FIR filters, FFT’s and direct memory access.

 

Feel free to download the attached pdf to learn more about the Minized.

 

In preparation of roadtesting the Minized, what do you feel you need?

 

  • Technical Information?
  • Tutorials?
  • Example Projects?
  • Other?

 

Please leave your comments below. I will try to get any additional information and post it to both the RoadTest and the FPGA groups.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

Attachments:
image5239-PB-XC7Z007S-1CLG225C-V11a.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago in reply to johnbeetem +5
    I'd like to echo John's comment that this board is not really suitable for initial learning about FPGAs - the Zynq chips are very, very difficult to get to grips with. There is all the difficulty of the…
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to michaelkellett +5
    Michael, considering your opinion trustable - as I do - as it is also following logic and a minimal knowledge of the FPGA world, why do they assume that this is (one of) the best solution for projects…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to balearicdynamics +5
    Enrico Miglino wrote: ... why do they assume that this is (one of) the best solution for projects oriented to hobbyists and makers? ... Enrico, I don't see this claim being made. The description says it…
Parents
  • rscasny
    rscasny over 8 years ago

    Here's a link to the webinar :

     

    NEW!: Let's Get Started with the Zynq 7000 Using the AVNET MiniZed Dev Board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bm010
    bm010 over 8 years ago in reply to rscasny

    Is this link now out of date? Looks like there is a 3-4pm CST one now?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bm010
    bm010 over 8 years ago in reply to rscasny

    Is this link now out of date? Looks like there is a 3-4pm CST one now?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 8 years ago in reply to bm010

    Thanks for catching that!

     

    Sometimes the time zone flips. the 3-4pm was a european time zone.

     

    The time is 9-10 am CST (Chicago time on Nov 17th.

     

    Check back again:

     

    NEW!: Let's Get Started with the Zynq 7000 Using the AVNET MiniZed Dev Board