• Products and Partners
    Products and Partners
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
FPGA
  • Technologies
  • More
FPGA
Files Data files for FlaviaLB56 release 0.0p
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

Data files for FlaviaLB56 release 0.0p

FlaviaLB56-00p.zip contains data files for the FlaviaLB56 implementation of the Free Logic Array, described in Flavia: the Free Logic Array and Chapter 12 of The XXICC Anthology rev 0.0n.  FlaviaLB56 is for the ValentF(x) LOGI-Bone FPGA board, rev R1.0.  To reduce chances of confusion, I recommend that you only install this file if you want to synthesize Flavia logic for the LOGI-Bone.

 

FlaviaLB56 rev 0.0p adds pinout tables to map top-level ports and signal names to FPGA pins.  You can also specify pull-up, pull-down, and keeper circuits for FPGA I/Os.  These are described in my element14 'blog Raspberry Pi 2 meets Papilio DUO.  I'll be incorporating these changes in the next version of The XXICC Anthology.

 

I've only tested FlaviaLB56 rev 0.0p using an Adafruit FT232H Breakout Board as a JTAG controller and the "use JTAG" option.  I haven't tried programming 0.0p directly from a BeagleBone.  I didn't touch any of that code, so it should work.

 

Unless you're using JTAG, Flavia rev 0.0p probably won't work "out of the box" with the new LOGI-Bone-2, marked R1.5.1 on the PC board. LOGI-Bone-2 has a different I2C GPIO expander and changes its pin assignment, so programming LOGI-Bone-2 directly from BBone is slightly different.  Flavia 0.0p programs LOGI-Bone by writing a bitstream to "/dev/logibone".  This is equivalent to "dd" from the command line.  From looking at the documentation at ValentF(x) http://valentfx.com/wiki/index.php?title=Logi-Bone_User_Guide#Programming_the_FPGA_from_the_BeagleBone, it looks like you now need to write the bitstream to /dev/LOGIbone.  Since GNU/Linux is case-sensitive, this means Flavia probably won't work unless you go into Xbitscan.gal and change "/dev/logibone" to "/dev/LOGIbone".  However, first try downloading a test image using "dd".

 

If you've been able to get Flavia running on LOGI-Bone-2, please add comments below telling us what worked.  If you're having trouble getting LOGI-Bone-2 to work, add comments and/or e-mail me and we'll figure it out.

 

Note: LOGI-Bone-2 changed the default FPGA configuration mode from Slave Serial to Master Serial/SPI, i.e., self-config.  So when you power it on, LOGI-Bone-2 tries to read a valid bitstream from on-board serial Flash.  Flavia can override it, but if there's a valid bitstream it will affect whatever you have hooked up to LOGI-Bone-2 bins.

 

There may be other LOGI-Bone-2 changes that affect Flavia.  I don't have the new board to test things at this time.

 

Flavia is part of XXICC.  For more information on XXICC, see the 'blog post XXICC (21st Century Co-design) release 0.0p and XXICC's home page: xxicc.org.

 

This work is licensed under the Creative Commons Attribution-ShareAlike 3.0 Unported License.  To view a copy of this license, visit creativecommons.org/licenses/by-sa/3.0/.  No warranty is expressed or implied.

  • fpga
  • flavia
  • xxicc
  • logi-bone
johnbeetem
johnbeetem
  • 29 May 2015
  • 3 Downloads