Internet of Things
  • Technologies
  • More
Internet of Things
Blog Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 1: build and test
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 28 Dec 2023 9:20 PM Date Created
  • Views 8049 views
  • Likes 8 likes
  • Comments 37 comments
  • raspberry
  • the things network
  • lorawan
  • ttn
  • gateway
  • iot
Related
Recommended

Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 1: build and test

Jan Cumps
Jan Cumps
28 Dec 2023
Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 1: build and test

I installed the software for the Elecrow LoRaWAN gateway (see  Low-Cost LoRaWAN Gateways! ), and enabled the gateway on The Things Network (TTN). I used Raspberry OS bullseye 32-bit lite on a Raspberry Pi  A+. I tested this on a B+ with the same OS too.

epic

Instructions from Elecrow: https://www.elecrow.com/wiki/index.php?title=LR1302_LoRaWAN_Gateway_Module

Preparation

sudo apt-get update

sudo apt install -y git

cd ~

run sudo raspi-config to enable

  • i2c,
  • SPI and
  • Serial Port. For Serial Port, do not allow console (question 1: no), but allow enabling of the port (question 2: yes).

Build the software


The following section is different than the vendor's instructions:

clone https://github.com/Elecrow-RD/LR1302_loraWAN.git

cd LR1302_loraWAN

cd LR1302_HAL

cd sx1302_hal

back to the existing instruction

make

Create new TTN Gateway

If you don't have an account yet, create one. Select the suggested settings for your location. Once logged in, navigate to the console. Select Gateways

image

Register your new Gateway. Accept the suggested frequency and setup. I used https://descartes.co.uk/CreateEUIKey.html to generate an ID

image

Then download the json file that's created for you. It holds some of the settings you 'll need to update in the gateway's config file later.

Configure the packet_forwarder

The following section is different than the vendor's instructions:

cd packet_forwarder

nano global_conf.json.sx1250.EU868

I had to change this line extra, not in instructions:
"gps_tty_path": "/dev/ttyS0",

back to the existing instruction

change the EUI in the config file, and check the TTN server URL. Save

The following section is different than the vendor's instructions:

chmod +x reset_lgw.sh

Test

back to the existing instruction

./lora_pkt_fwd -c global_conf.json.sx1250.EU868

You will get a log of what's happening:

image

The TTN console confirms it found you:

image

And after some time, you will appear on the maps: https://ttnmapper.org/heatmap/

image

I've tested with an Arduino MKR 1310, and all worked fine:

Proper install of all software (covered fully in the next blog)

There's more than this. To install all software in a location of your choice, check the instructions on git: https://github.com/Elecrow-RD/LR1302_loraWAN/blob/master/LR1302_HAL/sx1302_hal/readme.md

first edit target.cfg, and set your user name and location where to install (must exist)

Then 

make install

make install_conf

Full install post:  Set up Elecrow TTN LoRaWAN gateway on Raspberry Pi - Pt. 2: full install and run as service 

Enjoy

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DaniLecx +1
    In the github issue you are referring to, there is a replacement reset script attached ( here ). If you overwrite sx1302_hal/bin/reset_lgw.sh with those contents, it should work with a sysfs-less linux…
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Jan Cumps +1
    the USE_LIBGPIOD setting in docker does the same : (see start file ) if [[ ${USE_LIBGPIOD} -eq 0 ]]; then cp /app/reset.sh.legacy ${RESET_FILE} else cp /app/reset.sh.gpiod ${RESET_FILE} fi /app…
Parents
  • kpin404
    kpin404 over 2 years ago

    Hello Jan Cumps , 

    I have received an Elecrow LR1302 (868) LoRaWAN gateway module included with Pi HAT from Elecrow. After hardware assembling with Raspberry- Pi board I have tried to setup as per the vendor's instructions, but afraid to say that I am unable to make a setup configuration for this. Could you please help me to assist further with its complete step-by-step setup configuration instructions to make it work for me. Thanks.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to kpin404

    This series of blog posts is my step by step document. I have nothing more detailed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kpin404
    kpin404 over 2 years ago in reply to shabaz

    Hello shabaz , Okay! got it. Thanks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to kpin404

    If you do that correctly, you should have a specific .json file in your service status: 

    in my case, the sevice shows this info: 

    615 /home/jancumps/sx1302_hal/bin/lora_pkt_fwd -c /home/jancumps/sx1302_hal/bin/global_conf.json.sx1250.EU868


    I see that you have  ....   ./global_config.json.

    This is the file where I had to configure gateway ID and lorawan network url . Did you do all steps from start to end?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kpin404
    kpin404 over 2 years ago in reply to Jan Cumps

    Yes! i done all the procedure step-by-step and configured everything including network server access url, gps tty path, but i didn't change the gateway id as its already showing in the configuration file. Do i must have to change it also?image 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to kpin404

    In my case, the gateway_ID is identical (without the blank spaces) to Gateway EUI on the gateway general information page on TTN

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to kpin404

    Same in my case as Jan. It's critical that the value entered on the LoRaWAN provider site config item Gateway EUI  matches the Gateway ID value (which is also known as Gateway EUI) that is in your LoRaWAN gateway. You don't need to change the value that is in your gateway. You simply copy it, and paste it into the Gateway EUI config box on the LoRaWAN provider site.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 2 years ago in reply to kpin404

    Same in my case as Jan. It's critical that the value entered on the LoRaWAN provider site config item Gateway EUI  matches the Gateway ID value (which is also known as Gateway EUI) that is in your LoRaWAN gateway. You don't need to change the value that is in your gateway. You simply copy it, and paste it into the Gateway EUI config box on the LoRaWAN provider site.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kpin404
    kpin404 over 2 years ago in reply to shabaz

    Hello there, thanks all for your support. I have configured and tested to setup with TTN server and it did connected successfully. Now this confirms that there is an issue with my local network server to be to check with. Thanks.image