I connected an Arduino MKR WAN 1310 to Amazon Web Services (AWS IoT). Then tested if the Arduino can publish uplinks to AWS, and can receive AWS topics as downlinks. This post is my log of the activity.
image source: me
Read this p...
I connected an Arduino MKR WAN 1310 to The Things Network. And enabled both send and receive. This post is my log of the activity.
A few weeks ago, I bought a LoRaWan gateway. In this post, it helps to get and end-to-end trace. I have ...
I installed the software for the Elecrow LoRaWAN gateway (see Low-Cost LoRaWAN Gateways! ), and enabled the gateway on The Things Network (TTN). I used Raspberry OS bullseye 32-bit lite on a Raspberry Pi A+. I tested this on a B...
I saw in an e-mail an advert for LoRaWAN gateway modules, so I took a quick peek, and was surprised at how low-cost they had become. These can be used with any computer, such as a Raspberry Pi, to wirelessly monitor or control sensors ...
Seeed MR60BHA1: Sense presence, breathing, and heartbeat with mmWave precision. Non-contact, low-power, and compact for smart homes, health
The MR60BHA1 60GHz mmWave Module is a versatile sensor that utilizes Frequency Modulation Continuou...
I bought a Useful Sensors Tiny Code Reader from Sparkfun https://www.sparkfun.com/products/23352 back in September, but as always have been too busy to try it out until now...
The Tiny Code Reader (TCR) is the second Useful Sensors product ...
Hello everyone, this blog post will delve into the topic of energy monitoring, featuring the utilization of the SONOFF POW Elite energy monitoring device in conjunction with OpenHAB. In the forthcoming pair of videos, I will demonstrate the process...
NASA's ILLUMA-T will send laser signals to the LCRD satellite, which transmits them to ground stations in Hawaii and California. (Image Credit: Dave Ryan/NASA)
The International Space Station is getting an upgrade with an Integrated LCRD Low Ear...
The term "Internet of Things" (IoT) refers to a network of physical objects that can interact with one another using the Internet. The IoT network connects existing sensors and devices to the Internet in real-time, creating its ecosystem. IoT seamles...
Hey, fellow home automation enthusiasts! Are you tired of manual backing up your TASMOTA device configurations? We've got some exciting news for you! Check out these two amazing videos that demonstrate a quick and straightforward way t...
I noticed that the Summer of Green Tech Design Challenge is being sponsored by Seeed Studio and uses a kit that includes the Xiao SamD21 microcontroller and a Grove sensor pack. I've been using Xiaos for over a couple of years (Sa...
Dispositivo BPLC 10Gbps, Power Line Communications (PLC) Red linea electrica + Banda ancha (Internet) High Velocity en red electrica, Broadband Power Line 2,4 Gbps. (BPL) + WIFI 7 Power Wireless 1200w + 1000 nodos y con 2 Gigabit ethernet puerto.
Ser...
Servicios que promueve la conectividad, la interconexión, el acceso a internet a muy alta velocidad o superior a la de Fibra Óptica, velocidades que van de 200 Mbps hasta2.4Gbps con esta tecnología llamada Power Line Communicatio...
Are you tired of relying on traditional motion detection systems that require complex wiring and bulky hardware? Then it's time to upgrade to an IoT-based motion detection system with ESP32! With this project, you can create a sleek and intellige...
Introduction
One similarity among different industries, is a need for energy. This essential resource unlocks possibilities for investments, innovations, and new businesses that then lead to job creation, sustainable growth, and shared prosperity for...
Introduction
The digital revolution has led to a significant increase in data use across industries worldwide. As a result, many organizations and individuals are struggling to maintain their essential information, systems, and programs on their in-h...
Introduction
In this tutorial today we would like to how to create an Environment Data Monitoring Dashboard using the Maker Feather AIOT S3. As we know environmental data are crucial be it for personal, company or the government. The environmen...
In LoRa based system we can transmit the information to Another LoRa, then we can use that information and display it on the Local LCD Display or somewhere. if we need the data to be transmitted far longer distances than the LoRa Coverage? What do w...
The Snapdragon Satellite will provide global messaging for next-gen Android phones using the weather-resilient L-band spectrum. (Image credit: Qualcomm)
Finally, consumers have access. Hope it doesn’t arrive with a hefty price.
Qualcomm recent...
I have home automation implemented at my house that allows me to control and monitor things remotely (lights, cameras, etc). We were on a trip last week when my wife got a call after dinner from a neighbor who asked if we sitting home in t...
You can measure the temperature without any external temperature sensor, for measuring the temperature all you need is only nrf52832.
When you want to measure the temperature of the surroundings while developing Bluetooth low-energy projec...
(Image Credit: Compare Fibre/Unsplash)
Engineers at the Technical University of Denmark set a new data transmission speed record at 1.84 petabits per second through a photonic chip and a fiber optic cable. The team accomplished such an amazing feat ...
About The Project
I currently reside in Ooty, a beautiful hill station in southern India. The main problem is that elephants frequently enter the village. We can be alerted by their sounds sometimes, but most of the time they are silent, so we cann...