Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building A Direct Digital Synthesis Dual-Channel Signal Generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Aug 2018 6:37 AM Date Created
  • Views 28981 views
  • Likes 17 likes
  • Comments 148 comments
  • mbed enabled
  • ad9834
  • signal generator
  • direct digital synthesis (dds)
  • arm mbed
  • freescale
  • mbed os 5
  • dds
  • kinetis
  • direct digital synthesizer
  • ad9954
  • frdm
  • frdm-kl25z
  • radiofrequencych
  • mbed
  • frdm-family
  • frequency synthesizer
  • mbed-os
  • nxp
Related
Recommended

Building A Direct Digital Synthesis Dual-Channel Signal Generator

shabaz
shabaz
11 Aug 2018

Introduction

This blog post discusses some practical implementations of super-low-cost ($30 upward) direct digital synthesis (DDS) based signal generator for home use. To save effort and time, they can all be built around an off-the-shelf microcontroller board, and an off-the-shelf direct digital synthesis (DDS) board.

image

There are several different ideas discussed in this blog post, and all are similar – the principles are exactly the same, just that frequency range and desired control/monitoring capabilities can be chosen to suit needs. They are all be lumped together since they are all so similar.

 

There is a three-minute demo of the user interface here:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What Does it Do?

This project allows for the creation of controlled sine waves, at a desired frequency. This has uses for testing radio receivers, measuring the frequency response of filters, creating a radio transmission, creating a stimulus for testing amplifiers, and so on.

 

Manipulations such as frequency sweeping, frequency modulation and frequency shift keying (FSK) is possible with this project.

 

This project relies on an external amplifier or attenuator to adjust the signal level, although some limited adjustment is possible without additional hardware.

 

How Does it Work?

For a more in-depth look at DDS, see the blog post here Building a Frequency Synthesiser but briefly, the DDS board constructs a sine wave digitally by sending a table of numbers to a digital to analog converter (DAC). DDS devices allow a desired frequency to be programmed using an internal register (e.g. programmed via an SPI or other I/O bus). The programmed value is fed into a summing device or counter, known as a phase accumulator. This is just responsible for repeatedly adding the programmed value to the existing sum, on each clock cycle. So, if the desired frequency is a low value then the phase accumulator will increment in low values too. If the desired frequency is higher, then the phase accumulator will increment in larger chunks The phase accumulator loops back to zero once it reaches its maximum. Each possible value that the output of the accumulator can take represents a different point on a sinewave. A look-up table is used to convert from the phase accumulator output to an amplitude on the curve of a sine wave. This then drives a DAC and and external filter.

 

Some of the benefits are:

  • Extremely low noise close to the oscillation frequency
  • High granularity (sub-Hz is possible)
  • On-board RAM and instruction set allow for very fast frequency hopping or ramping (it is possible to achieve FM and FSK modulation using this method)

 

A disadvantage of DDS is that there can be some spurious content (usually relatively far away from the selected output frequency) that may need filtering for very demanding applications. Since filters can be expensive, often just a fixed low-pass filter is used, as in the project described here.

 

DDS boards are available from ebay, with a digital input interface, and an RF connector ready for providing the signal output. All that is required is to configure the DDS board to output the desired frequency, using a microcontroller for example.

 

For the project described here, a FRDM-KL25Z microcontroller boardmicrocontroller board is used. It is very low cost (about $15) and easy to program using a USB cable. For more detail about the board and the programming process, see here: Working with FRDM Boards and ARM mbed 

 

The board has 128 kbyte Flash and 16 kbyte RAM, and lots of input/output pins, on a near-credit-card-sized board around 5mm thick - it's really great!

(image source: NXP website)image

 

 

The easiest implementation was to not have any buttons or display on the device, and just enable the USB connection on the FRDM board to become a USB Serial interface. Thus whenever the user wishes to modify the frequency output, all that needs to be done is to connect the board to a PC via USB, and run terminal software such as PuTTY on Windows or ‘screen’ on Mac or Linux. A text-based menu system becomes the user interface.

image

 

With this method, the project can be constructed for about $30 or a bit more, depending on which DDS board is used. I tried two boards; a 0-10 MHz one, and a 0.05-160 MHz board.

 

If a permanent display is desired, an LCD screen can be attached. It adds another $20 to the cost. If buttons are needed, they can be added too. A rotary encoder or even a keypad could also be attached. There are plenty of free pins available on the FRDM board. Although I didn’t do it for this project, for information on how to attach a keypad, see here: Building a USB Keypad: A Mini-Project

 

In summary there’s a lot of flexibility concerning implementation. The core functionality uses the USB Serial menu system however. Code can be added to make use of the display, and buttons/keypad/encoder. I'd also like to incorporate a USB based SCPI interface (based on Jan Cumps SCPI project on element14) at some stage. This blog post is just to give ideas, not all combinations are implemented today so if you modify the code to implement a new combination, please do share the code.

 

The current code implements the text menu system, and rotary encoder for frequency selection, and display update indication of the menu selections and frequency. The plan is to extend rotary encoder usage so that it works with the menu system. So, if the text menu has the options such as sine and ramp at a particular menu level for instance, then the rotary encoder should also allow for selection of these two options before going into the next menu level in the hierarchy.

 

For this project I decided to develop my own menu system called picocli (I originally planned to take a Linux shell’s source code and run it Linux-kernel-less since the FRDM board has just a microcontroller). I may still revert to that, but for now I’m using custom code). It is at proof-of-concept level but functions reliably enough for now to use in this project, and it implements things like help, tab completion and a last-command history. It will be explored more in Part 2.

 

I also had to write a custom rotary encoder library rather than use an existing one, because I wanted to integrate things like velocity based modification of behaviour. Anyway, this was a short exercise compared to writing the menu system.

 

Making the Basic Configuration

The basic implementation (using a DDS board and the FRDM-KL25Z board connected to the PC for control via a USB serial interfaced menu) takes about five minutes to assemble. One or two boards are purchased and wired together with jumper cables.

image

 

For the DC to 10 MHz range, AD9834 boards are purchased. I have only tested a single AD9834 board, but two could be connected in theory if desired, for dual output, but there is no way to synchronise the two board outputs with the AD9834 chip.

 

For approx. 50 kHz to 160 MHz, AD9954 boards are used.

 

Nearly all the wiring throughout the project relied on jumper wires. To make these to custom lengths, this crimp toolthis crimp tool is great. It works with the crimpscrimps and then the result is inserted into SIL and DIL header socket shells. Standard pre-assembled jumper wires could be used too.

image

 

Here is a table of the specific wiring shown in the diagram above:

 

AD9834 DDS board markingFRDM-KL25Z board marking (conn. J9)
FSY  (fsync)B11 (PTB11) J9 pin 7
PS (phase select)B9 (PTB9)   J9 pin 3
SCK (clk)E3 (PTE3)   J9 pin 11
FS (freq select)B10 (PTB10) J9 pin 5
SDA (data)E2 (PTE2)   J9 pin 9
RST (reset)B8 (PTB8)   J9 pin 1
GND (0V)GND           J9 pin 12
5V5V              J9 pin 10

 

 

For using the 160 MHz boards, the connection diagram is below. Please note that I believe this diagram is correct, but I don’t have these actual boards to verify. I used some custom boards (based on the same chip) that I created a while back. However I see no reason why the ebay boards wouldn’t work.

image

 

With a bit of effort, it will be possible to have phase locked and phase adjustable outputs with these 160 MHz boards, since the AD9954 chip supports this capability. I have not tried it yet, because I’m still considering the optimal way to do that (I didn’t originally design my custom boards with that capability in mind : (

 

Still, there is plenty of room in the enclosure to add this capability at a future date once I’ve figured it out.

image

 

Building the Software

Instructions on how to use the development environment and how to push the compiled code into the board are described at the location mentioned earlier: Working with FRDM Boards and ARM mbed 

 

The code can be compiled and then programmed into the board via the USB cable. The next blog post will cover the software, but if you wish to use it now (it won’t be pretty code, it still needs tidying) then please let me know.

 

Using It

Connect up the output of the DDS board to an oscilloscope or spectrum analyzer, plug in the USB connection into the PC and the project should power up! Open up a serial terminal and connect to the board. Hit the Enter key and a command prompt (‘$’) should appear. You can type help or ? for assistance. Generally the menu structure has been designed to accept a command, or a command followed by parameters. Some commands will drop you into a new level in the menu, and you can exit that level by typing exit.

 

So, to output a sinewave at 1.2 MHz, type the following to enter the sinewave mode and invoke the signal output at the desired frequency:

 

$ sine
sine$ frequency 1.2M 
sine$ on

 

Here is another example, to generate a frequency sweep from 2.1 MHz to 2.2 MHz. Here the sweep command will drop you into the sweep mode, so type exit afterwards if you want to go into a different mode. You can type help or ? at any time to get help for the mode that you’re in:

 

sweep
range 2.1M 2.3M
on

 

There are extra parameters that can be configured (press ‘?’ to see the commands to do so) for adjusting the sweep steps and so on. I'd like to add a trigger output on the rear panel, so that the project can be used for basic scalar analysis of things like filters.

image

 

Adding a Display and User Controls

I decided to use an enclosure and front panel similar to what I’ve used before for this project: Building a SMT Pick-and-Place Buddy and so both projects rely on a Hammond instrument case and LCD on the front, and FRDM board stuck at the back so that the USB connector is accessible. The two signal outputs will also be at the back (using SMA connectors) because the front panel ended up becoming too full. It's not very convenient, but I can live with it.

image

 

This time I used a parallel mode LCD which is more inconvenient to use than the I2C displays, but I wanted to use it for the high quality output. The display uses ‘VATN’ LCD technology, which looks very close to Organic LED (OLED) in terms of contrast, when viewed at the right angle. So, it has near-OLED looks, but with LCD display lifetime, which seemed ideal for a test instrument. For the user input, I used a rotary encoder. An optical encoder with no detents is quite good for setting frequency, because it can be rapidly spun for getting from one end of the spectrum to the other in a short time. I used a Marquardt switch too. These almost feel like a keyboard switch, so they are light to press.

 

The Hammond case comes with aluminium plates, but plastic is easier to machine so I replaced the front panel with a black ABS plastic sheet instead, and cut a few other bits of plastic to hold the switch and rotary encoder at a convenient depth. A 3D printer could be used to make these, although I did it manually with sheet plastic.

image

 

After lots of epoxying, the front panel was semi-complete.

image

 

Sanding parts makes them easier to epoxy together. Thread-lock glue was used to hold some of the screwed bits together.

image

 

The particular rotary encoder I had operated at 5V whereas the FRDM-KL25Z board has 3.3V logic inputs, so a couple of potential divider resistor pairs were used on the quadrature encoder output lines, to drop from 5V to 3.3V (I used 1.8k and 3.3k resistors); the resistors can be seen attached to the header socket that will be connected to the rotary encoder in the photo below.

image

 

The LCD screen was a couple of millimetres taller than the inside of the case! : ( so I had to cut a shallow groove in the top and bottom of the case, to accommodate it. A piece of wood was glued to hold the display in the correct position. Jumper cables were used everywhere in case things ever need disassembly.

image

 

Performance

The performance is quite good, but that’s to be expected from DDS technology.

 

Here is what it looks like on an oscilloscope, using the AD9834 board; the output extends down to DC incidentally, because there is no output capacitor on the board.

image

 

The AD9954 board provides for up to 160 MHz output although at the low end it is limited; much lower than 50 kHz results in reduced amplitude, because my board has a transformer on the output. The ebay versions do not have this according to the photos on ebay, so they should extend down to DC.

image

 

It is hard to tell how good or bad a signal is from the ‘scope trace, so the FPC1500 spectrum analyzer was used. A span of 2MHz was examined when the DDS was set to 9.55MHz, and also 134MHz in the case of the AD9954. The result was good. The close-in noise is almost entirely due to the crystal oscillator module. The module on the AD9954 board for example contains an internal phase locked loop (PLL) to generate a 100MHz clock. Another PLL inside the AD9954 multiplies this by 4 to generate a 400MHz internal clock. I have a 400MHz oscillator module (which still uses a PLL) that I may try at some point; it has worse jitter than the 100MHz module, but it means that I can then disable the PLL inside the AD9954. Or I could try to source a better module, but it could get expensive.

 

The AD9834 board uses a similar style of oscillator module, with a PLL inside it too I suspect.

image

 

To see how this compared with a commercial signal generator, I connected a Rigol DG1022Z to the FPC1500. The DG1022Z has a 14-bit DAC internally, as does the AD9954 DDS chip.

 

The result is fairly similar when set to approximately the same power level. At higher output level this situation can change! - see the second spectrum trace below.

image

 

The DG1022Z operates to 25MHz, and I only tested at 10MHz. The AD9954 can go to 160MHz. Of course the DG1022Z is more flexible since it has arbitrary waveform capability too, but if just a sine wave and a few frequency modulation based schemes are required, then the AD9834 or AD9954 are great options.

 

Summary

A simple design has been presented to create a fairly usable signal generator. It costs less than $30 and perhaps half an hour of time to build and program it all. The full enclosure version takes longer of course.

 

It could be extended with an amplifier circuit if desired. If you build this project as-is or extend or modify it, it would be great to hear about it to bounce off ideas.

 

image

  • Sign in to reply
Parents
  • derick007
    derick007 over 6 years ago

    Hi Shabaz,

     

    I have re-written the sketch entirely. My understanding now is alot simpler than when I started 6 months ago - hopefully it is correct ?

     

    It would appear all that is required is to get the ARDUINO to write data to the registers in the AD9954 ?

     

    I have worked all the values for all the registers, for the AD9954, on a spreadsheet so that I only need to use the sketch to send these values to the DDS.

     

    However there are a few things I still am not clear about.

     

    1. UPD - is this required ? If so when do I activate it > at the end of every transfer for each register ?

     

    2. Surely I only need to write the values to the AD9954 once ? This being the case, then the part of the sketch which writes the values should be included in the void setup, rather than the void loop ?

     

    One other thing, I have an old Tetronix 2465 scope which I am using for this project. I bought it some time ago and have rarely used it. Unfortunately it doesnt appear to trigger so well as I am getting a lot of jitter. This is really just a hobby so I have a very limited budget for test equipment - any suggestions apart from the obvious.

     

    Many thanks, Derek

     

     

    //************************************************ 

    //* SCLK test code for MKRZERO 

    //* rev 0.1 December 2019 

    //************************************************

     

     

    // DECLARING / DEFINING VARIABLES & THEIR TYPES

     

    char clockpin = A1;       // declaring or defining the variable named clockpin as a character type which has a value A1

    char datapin = A2;        // declaring or defining the variable named datapin as a character type which has a value A2

    char resetpin = A3;       // declaring or defining the variable named resetpin as a character type which has a value A3

    char ioupdatepin = A4;    // declaring or defining the variable named ioupdatepin as a character type which has a value A4

     

    // DECLARING / DEFINING DDS REGISTERS

    // INTEGERS ARE THE PRIMARY DATA TYPE FOR NUMBER STORAGE

    // THE DDS HAS 11 REGISTERS WHICH NEED TO BE PROGRAMMED

    // REGISTERS HAVE VARIOUS LENGTHS FROM 2 BYTES TO 5 BYTES

    // I HAVE DECLARED EACH REGISTER HAS AN ARRAY OF INTEGER TYPE

    // THE NUMBERS IN THE ARRAYS ARE DECIMAL NUMBERS

     

    int CFR1 [] = {128, 174, 0, 112, 8};      // declaring or defining the variable named CFR1[] (control function register 1) as a 5 byte array and integer data type

    int CFR2 [] = {129, 0, 0, 164};           // declaring or defining the variable named CFR2[] (control function register 2) as a 4 byte array and integer data type

    int ASF [] = {130, 0, 0};                 // declaring or defining the variable named ASF[] (amplitude scale factor) as a 3 byte array and integer data type

    int ARR [] = {131, 0};                    // declaring or defining the variable named ARR[] (amplitude ramp rate) as a 2 byte array and integer data type

    int FTW0 [] = {132, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 0) as a 5 byte array and integer data type

    int POW0 [] = {133, 0, 0};                // declaring or defining the variable named POW0[] (phase offset word) as a 3 byte array and integer data type

    int FTW1 [] = {134, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 1) as a 5 byte array and integer data type

    int RSCW0 [] = {135, 0, 0, 0, 0};         // declaring or defining the variable named RSCW0[] (ram segment control word 0) as a 5 byte array and integer data type

    int RSCW1 [] = {136, 0, 0, 0, 0};         // declaring or defining the variable named RSCW1[] (ram segment control word 1) as a 5 byte array and integer data type

    int RSCW2 [] = {137, 0, 0, 0, 0};         // declaring or defining the variable named RSCW2[] (ram segment control word 2) as a 5 byte array and integer data type

    int RSCW3 [] = {138, 0, 0, 0, 0};         // declaring or defining the variable named RSCW3[] (ram segment control word 3) as a 5 byte array and integer data type

     

    void setup() {

     

      pinMode(clockpin, OUTPUT);    // sets pin A1 as OUTPUT

      pinMode(datapin, OUTPUT);    // sets pin A2 as OUTPUT

      pinMode(resetpin, OUTPUT);    // sets pin A3 as OUTPUT

      pinMode(ioupdatepin, OUTPUT);    // sets pin A4 as OUTPUT

     

      //reset the AD9954

     

      digitalWrite(resetpin, LOW);

      delay(1);

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

    }

     

    void loop() {

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<3; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ASF[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<2; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ARR[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

    }

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, POW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<5; i=i+1) {

     

    shiftOut(datapin, clockpin, MSBFIRST, RSCW2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to derick007

    Hello Derek,

    Shabaz is correct (almost) re the /CS pin, actually it is essential that you control it - see the diagram on page 24 of the AD9954 data sheet - CS is used to frame the serial control messages.

     

    From page 21 you can see that the IO Update pin must be toggled after a write to registers since the data is transferred from buffers to working registers in the AD9954 only on the rising edge

    of UPDATE, synched with the SYNC_CLK (which is an AD5594 output). There is (probably)  no way that the Arduino can sync correctly with the SYNC_CLK so just toggle UPDATE after setting the

    registers and hope for the best.

     

    Your scope only has two channels so you will need to be creative about checking the signals:

    Use ch1 on SCLK and ch2 on SDIO and trigger from the falling edge of /CS - you should see bursts of clock cycles on SCLK and data patterns on SDIO.

     

    I haven't checked the code in the loop{}, and I've no idea exactly what shiftOut() does - but with your scope you should be able to see if its doing what page 24 requires, if not then let us know !

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 6 years ago in reply to michaelkellett

    Thanks Michael and Shabaz.

     

    I remember reading somewhere that as the CS pin is active low, it was ok to ground it - thats what I did.

     

    I now toggle the i/o update pin after writing to each register.

     

    I am now trying to read back one of the registers and display in the serial monitor to prove the reading/writing to the AD9954 is correct. Unfortunately I havent had much success and without any proper diagnostic equipment I think I may have bitten off more than I should have.

     

    //************************************************ 

    //* SCLK test code for MKRZERO 

    //* rev 0.1 December 2019 

    //************************************************

     

     

    // DECLARING / DEFINING VARIABLES & THEIR TYPES

     

    char clockpin = A1;       // declaring or defining the variable named clockpin as a character type which has a value A1

    char datapin = A2;        // declaring or defining the variable named datapin as a character type which has a value A2

    char resetpin = A3;       // declaring or defining the variable named resetpin as a character type which has a value A3

    char ioupdatepin = A4;    // declaring or defining the variable named ioupdatepin as a character type which has a value A4

     

    // DECLARING / DEFINING DDS REGISTERS

    // INTEGERS ARE THE PRIMARY DATA TYPE FOR NUMBER STORAGE

    // THE DDS HAS 11 REGISTERS WHICH NEED TO BE PROGRAMMED

    // REGISTERS HAVE VARIOUS LENGTHS FROM 2 BYTES TO 5 BYTES

    // I HAVE DECLARED EACH REGISTER HAS AN ARRAY OF INTEGER TYPE

    // THE NUMBERS IN THE ARRAYS ARE DECIMAL NUMBERS

     

    int CFR1 [] = {0, 174, 0, 112, 8};      // declaring or defining the variable named CFR1[] (control function register 1) as a 5 byte array and integer data type

    int CFR2 [] = {1, 0, 0, 164};           // declaring or defining the variable named CFR2[] (control function register 2) as a 4 byte array and integer data type

    int ASF [] = {2, 0, 0};                 // declaring or defining the variable named ASF[] (amplitude scale factor) as a 3 byte array and integer data type

    int ARR [] = {3, 0};                    // declaring or defining the variable named ARR[] (amplitude ramp rate) as a 2 byte array and integer data type

    int FTW0 [] = {4, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 0) as a 5 byte array and integer data type

    int POW0 [] = {5, 0, 0};                // declaring or defining the variable named POW0[] (phase offset word) as a 3 byte array and integer data type

    int FTW1 [] = {6, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 1) as a 5 byte array and integer data type

    int RSCW0 [] = {7, 0, 0, 0, 0};         // declaring or defining the variable named RSCW0[] (ram segment control word 0) as a 5 byte array and integer data type

    int RSCW1 [] = {8, 0, 0, 0, 0};         // declaring or defining the variable named RSCW1[] (ram segment control word 1) as a 5 byte array and integer data type

    int RSCW2 [] = {9, 0, 0, 0, 0};         // declaring or defining the variable named RSCW2[] (ram segment control word 2) as a 5 byte array and integer data type

    int RSCW3 [] = {10, 0, 0, 0, 0};         // declaring or defining the variable named RSCW3[] (ram segment control word 3) as a 5 byte array and integer data type

    int readin = 134;

    int FREQREG[4];

     

     

    void setup() {

     

      Serial.begin(57600);

     

      pinMode(clockpin, OUTPUT);    // sets pin A1 as OUTPUT

      pinMode(datapin, OUTPUT);    // sets pin A2 as OUTPUT

      pinMode(resetpin, OUTPUT);    // sets pin A3 as OUTPUT

      pinMode(ioupdatepin, OUTPUT);    // sets pin A4 as OUTPUT

     

      //reset the AD9954

     

      digitalWrite(resetpin, LOW);

      delay(1);                       // delay 1 ms

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

     

      // WRITE TO AD9954

     

      // CFR1

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to CFR1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // CFR2

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to CFR2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // ASF

     

      for (int i=0; i<3; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ASF[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ASF register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // ARR

     

      for (int i=0; i<2; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ARR[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ARR register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // FTW0

     

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

    }

     

     

    // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // POW0

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, POW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // FTW1

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW0

     

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW1

     

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  RSCW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW2

     

     

      for (int i=0; i<5; i=i+1) {

     

    shiftOut(datapin, clockpin, MSBFIRST, RSCW2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW3

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

      // READ FROM AD9954

     

      shiftOut(datapin, clockpin, MSBFIRST, readin);  // the instruction word to read register FTW1 from AD9954 is sent

     

      pinMode(datapin, INPUT);    // sets pin A2 as INPUT

     

      for (int i=0; i<4; i=i+1) {

     

      FREQREG[i] = shiftIn(datapin, clockpin, MSBFIRST); 

      }

     

      

       

       

    }

     

      void loop() {

     

          if (Serial.available() > 0) {

         // FREQREG[0] = Serial.read();

        

        Serial.print(FREQREG[0], DEC);

        delay(10000);

     

       

       

        // FREQREG[1] = Serial.read();

        Serial.print(FREQREG[1], DEC);

        delay(10000);

        Serial.print(FREQREG[2]);

        Serial.print(FREQREG[3]);

     

          }

       

       

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to derick007

    This won't work  - you need to crank the /CS (the / means it's active low) for every command.

     

    digitalWrite(ncs_pin, LOW);

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

    digitalWrite(ncs_pin,HIGH);

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Ah got it. I've just checked, my old source code mistakenly kept CS low (I had a line to set it high but I'd commented it out for some reason : ( I probably mistakenly ran the risk of the interface getting out-of-sync as a result. I need to revisit and correct the code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Hello Shabaz,

     

    That's the doc:

     

    Page 21, using IO_UPD, no mention of /CS

     

    image

     

     

    Basic stuff about the serial port:

     

    image

     

     

    Note the reference to IOSYNC function, this is a separate pin, nothing to do with update pin.

     

     

    and the key diagram showing how the framing by /CS works

    Page 24, clocking data:

     

     

    image

     

    And no mention of IO_UPD

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    Which document are you referring to? I'm looking at this one: https://www.analog.com/media/en/technical-documentation/data-sheets/AD9954.pdf

    maybe there is a different revision : ( (or it could be my misinterpretation since I'm suffering from a lack of caffeine this morning so far!). Trying to decipher my old code, I thought IO_UPD was manipulated with the CS line low.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to derick007

    You are still not cranking that chip select correctly.

    The chip select forms the frame for clocking data into the chip.

    The falling edge tells the chip to get ready for data, the rising edge tells it the transfer is done.

    Youv'e got:

     

    chip select low

    shift some data

    waggle the update signal

    chip select high

     

    that is not what the diagram on page 24 of the data sheet says - you need to go:

     

    chip select low

    shift some data

    chip select high

    waggle the update signal

     

    Why not connect that scope of yours as I described before and send some pictures of scope traces to us ?

     

    I'm forever getting SPI (or similar) interfaces going and I reckon that I get them working without using a scope or logic analyser a lot  less than half the time.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 6 years ago in reply to shabaz

    Hi Shabaz, Michael

     

    I am using the MKRZERO.

     

    I have changed the value in the ASF to 3FFF, I also changed bits 24 and 25 in CFR1 so that autoshaped on-off keying was selected because I believe the old values of zeros in 24 and 25 meant that the ASF register had no effect on the operation of the AD9954.

     

    There is a button on the AD9954 board which I pressed and each of the outputs (x2) increased from 0v to 1.5 and 1.3v dc. I think it possibly is just an ON/OFF button.

     

    Here is the latest sketch;

     

     

    //************************************************ 

    //* SCLK test code for MKRZERO 

    //* rev 0.1 December 2019 

    //************************************************

     

     

    // DECLARING / DEFINING VARIABLES & THEIR TYPES

     

    char clockpin = A1;       // declaring or defining the variable named clockpin as a character type which has a value A1

    char datapin = A2;        // declaring or defining the variable named datapin as a character type which has a value A2

    char resetpin = A3;       // declaring or defining the variable named resetpin as a character type which has a value A3

    char ioupdatepin = A4;    // declaring or defining the variable named ioupdatepin as a character type which has a value A4

    char chipselectpin = A5;     // declaring or defining the variable named chipselectpin as a character type which has a value A5    

     

    // DECLARING / DEFINING DDS REGISTERS

    // INTEGERS ARE THE PRIMARY DATA TYPE FOR NUMBER STORAGE

    // THE DDS HAS 11 REGISTERS WHICH NEED TO BE PROGRAMMED

    // REGISTERS HAVE VARIOUS LENGTHS FROM 2 BYTES TO 5 BYTES

    // I HAVE DECLARED EACH REGISTER HAS AN ARRAY OF INTEGER TYPE

    // THE NUMBERS IN THE ARRAYS ARE DECIMAL NUMBERS

     

    byte CFR1 [] = {0, 177, 0, 112, 8};      // declaring or defining the variable named CFR1[] (control function register 1) as a 5 byte array and byte data type

    byte CFR2 [] = {1, 0, 0, 164};           // declaring or defining the variable named CFR2[] (control function register 2) as a 4 byte array and byte data type

    byte ASF [] = {2, 63, 255};              // declaring or defining the variable named ASF[] (amplitude scale factor) as a 3 byte array and byte data type

    byte ARR [] = {3, 0};                    // declaring or defining the variable named ARR[] (amplitude ramp rate) as a 2 byte array and byte data type

    byte FTW0 [] = {4, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 0) as a 5 byte array and byte data type

    byte POW0 [] = {5, 0, 0};                // declaring or defining the variable named POW0[] (phase offset word) as a 3 byte array and byte data type

    byte FTW1 [] = {6, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 1) as a 5 byte array and byte data type

    byte RSCW0 [] = {7, 0, 0, 0, 0};         // declaring or defining the variable named RSCW0[] (ram segment control word 0) as a 5 byte array and byte data type

    byte RSCW1 [] = {8, 0, 0, 0, 0};         // declaring or defining the variable named RSCW1[] (ram segment control word 1) as a 5 byte array and byte data type

    byte RSCW2 [] = {9, 0, 0, 0, 0};         // declaring or defining the variable named RSCW2[] (ram segment control word 2) as a 5 byte array and byte data type

    byte RSCW3 [] = {10, 0, 0, 0, 0};         // declaring or defining the variable named RSCW3[] (ram segment control word 3) as a 5 byte array and byte data type

    int readin = 134;

    byte FREQREG[4];

     

     

    void setup() {

     

      Serial.begin(57600);

     

      pinMode(clockpin, OUTPUT);    // sets pin A1 as OUTPUT

      pinMode(datapin, OUTPUT);    // sets pin A2 as OUTPUT

      pinMode(resetpin, OUTPUT);    // sets pin A3 as OUTPUT

      pinMode(ioupdatepin, OUTPUT);    // sets pin A4 as OUTPUT

      pinMode(chipselectpin, OUTPUT);    // sets pin A4 as OUTPUT

     

      

      //reset the AD9954

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);                              // delay 1 ms

     

      digitalWrite(resetpin, LOW);

      delay(1);                       // delay 1 ms

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // WRITE TO AD9954

     

      // CFR1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

    // the next few lines transfer data from the i/o buffer latches to CFR1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

    digitalWrite(chipselectpin, HIGH);     // toggle CS

    delay(1);                              // delay 1 ms

     

      // CFR2

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to CFR2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // ASF

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<3; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ASF[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ASF register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

      // ARR

     

      digitalWrite(chipselectpin, LOW);      // toggle CS

      delay(1);

     

      for (int i=0; i<2; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ARR[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ARR register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

      // FTW0

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

    }

     

     

    // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // POW0

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, POW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // FTW1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // RSCW0

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

      // RSCW1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  RSCW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // RSCW2

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

    shiftOut(datapin, clockpin, MSBFIRST, RSCW2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // RSCW3

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW3 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // READ FROM AD9954

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      shiftOut(datapin, clockpin, MSBFIRST, readin);  // the instruction word to read register FTW1 from AD9954 is sent

     

      // the next few lines transfer data from FTW1 register memory to the i/o buffer latches 

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      pinMode(datapin, INPUT);    // sets pin A2 as INPUT

     

      for (int i=0; i<4; i=i+1) {

     

      FREQREG[i] = shiftIn(datapin, clockpin, MSBFIRST);

     

      

      }

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

       

       

    }

     

      void loop() {

     

        digitalWrite(chipselectpin, HIGH);     // toggle CS

        delay(1);                              // delay 1 ms

     

          if (Serial.available() > 0) {

         // FREQREG[0] = Serial.read();

        

        Serial.print(FREQREG[0], DEC);

        delay(10000);

     

       

       

        // FREQREG[1] = Serial.read();

        Serial.print(FREQREG[1], DEC);

        delay(10000);

        Serial.print(FREQREG[2]);

        Serial.print(FREQREG[3]);

     

        digitalWrite(chipselectpin, HIGH);     // toggle CS

        delay(1);                              // delay 1 ms

     

          }

       

       

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • derick007
    derick007 over 6 years ago in reply to shabaz

    Hi Shabaz, Michael

     

    I am using the MKRZERO.

     

    I have changed the value in the ASF to 3FFF, I also changed bits 24 and 25 in CFR1 so that autoshaped on-off keying was selected because I believe the old values of zeros in 24 and 25 meant that the ASF register had no effect on the operation of the AD9954.

     

    There is a button on the AD9954 board which I pressed and each of the outputs (x2) increased from 0v to 1.5 and 1.3v dc. I think it possibly is just an ON/OFF button.

     

    Here is the latest sketch;

     

     

    //************************************************ 

    //* SCLK test code for MKRZERO 

    //* rev 0.1 December 2019 

    //************************************************

     

     

    // DECLARING / DEFINING VARIABLES & THEIR TYPES

     

    char clockpin = A1;       // declaring or defining the variable named clockpin as a character type which has a value A1

    char datapin = A2;        // declaring or defining the variable named datapin as a character type which has a value A2

    char resetpin = A3;       // declaring or defining the variable named resetpin as a character type which has a value A3

    char ioupdatepin = A4;    // declaring or defining the variable named ioupdatepin as a character type which has a value A4

    char chipselectpin = A5;     // declaring or defining the variable named chipselectpin as a character type which has a value A5    

     

    // DECLARING / DEFINING DDS REGISTERS

    // INTEGERS ARE THE PRIMARY DATA TYPE FOR NUMBER STORAGE

    // THE DDS HAS 11 REGISTERS WHICH NEED TO BE PROGRAMMED

    // REGISTERS HAVE VARIOUS LENGTHS FROM 2 BYTES TO 5 BYTES

    // I HAVE DECLARED EACH REGISTER HAS AN ARRAY OF INTEGER TYPE

    // THE NUMBERS IN THE ARRAYS ARE DECIMAL NUMBERS

     

    byte CFR1 [] = {0, 177, 0, 112, 8};      // declaring or defining the variable named CFR1[] (control function register 1) as a 5 byte array and byte data type

    byte CFR2 [] = {1, 0, 0, 164};           // declaring or defining the variable named CFR2[] (control function register 2) as a 4 byte array and byte data type

    byte ASF [] = {2, 63, 255};              // declaring or defining the variable named ASF[] (amplitude scale factor) as a 3 byte array and byte data type

    byte ARR [] = {3, 0};                    // declaring or defining the variable named ARR[] (amplitude ramp rate) as a 2 byte array and byte data type

    byte FTW0 [] = {4, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 0) as a 5 byte array and byte data type

    byte POW0 [] = {5, 0, 0};                // declaring or defining the variable named POW0[] (phase offset word) as a 3 byte array and byte data type

    byte FTW1 [] = {6, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 1) as a 5 byte array and byte data type

    byte RSCW0 [] = {7, 0, 0, 0, 0};         // declaring or defining the variable named RSCW0[] (ram segment control word 0) as a 5 byte array and byte data type

    byte RSCW1 [] = {8, 0, 0, 0, 0};         // declaring or defining the variable named RSCW1[] (ram segment control word 1) as a 5 byte array and byte data type

    byte RSCW2 [] = {9, 0, 0, 0, 0};         // declaring or defining the variable named RSCW2[] (ram segment control word 2) as a 5 byte array and byte data type

    byte RSCW3 [] = {10, 0, 0, 0, 0};         // declaring or defining the variable named RSCW3[] (ram segment control word 3) as a 5 byte array and byte data type

    int readin = 134;

    byte FREQREG[4];

     

     

    void setup() {

     

      Serial.begin(57600);

     

      pinMode(clockpin, OUTPUT);    // sets pin A1 as OUTPUT

      pinMode(datapin, OUTPUT);    // sets pin A2 as OUTPUT

      pinMode(resetpin, OUTPUT);    // sets pin A3 as OUTPUT

      pinMode(ioupdatepin, OUTPUT);    // sets pin A4 as OUTPUT

      pinMode(chipselectpin, OUTPUT);    // sets pin A4 as OUTPUT

     

      

      //reset the AD9954

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);                              // delay 1 ms

     

      digitalWrite(resetpin, LOW);

      delay(1);                       // delay 1 ms

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // WRITE TO AD9954

     

      // CFR1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

    // the next few lines transfer data from the i/o buffer latches to CFR1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

    digitalWrite(chipselectpin, HIGH);     // toggle CS

    delay(1);                              // delay 1 ms

     

      // CFR2

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to CFR2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // ASF

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<3; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ASF[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ASF register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

      // ARR

     

      digitalWrite(chipselectpin, LOW);      // toggle CS

      delay(1);

     

      for (int i=0; i<2; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ARR[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ARR register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

      // FTW0

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

    }

     

     

    // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // POW0

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, POW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // FTW1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // RSCW0

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

      // RSCW1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  RSCW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // RSCW2

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

    shiftOut(datapin, clockpin, MSBFIRST, RSCW2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // RSCW3

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW3 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // READ FROM AD9954

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

      delay(1);

     

      shiftOut(datapin, clockpin, MSBFIRST, readin);  // the instruction word to read register FTW1 from AD9954 is sent

     

      // the next few lines transfer data from FTW1 register memory to the i/o buffer latches 

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

      pinMode(datapin, INPUT);    // sets pin A2 as INPUT

     

      for (int i=0; i<4; i=i+1) {

     

      FREQREG[i] = shiftIn(datapin, clockpin, MSBFIRST);

     

      

      }

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

       

       

    }

     

      void loop() {

     

        digitalWrite(chipselectpin, HIGH);     // toggle CS

        delay(1);                              // delay 1 ms

     

          if (Serial.available() > 0) {

         // FREQREG[0] = Serial.read();

        

        Serial.print(FREQREG[0], DEC);

        delay(10000);

     

       

       

        // FREQREG[1] = Serial.read();

        Serial.print(FREQREG[1], DEC);

        delay(10000);

        Serial.print(FREQREG[2]);

        Serial.print(FREQREG[3]);

     

        digitalWrite(chipselectpin, HIGH);     // toggle CS

        delay(1);                              // delay 1 ms

     

          }

       

       

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 6 years ago in reply to fmilburn

    Hi Frank,

     

    Thanks! It did feel weird connecting the PWR pin to GND : )

    I've summarized the connections below, from the AD9954 board to the MKR ZERO.

    image

    This works with the earlier code, with the code modification for the 20 MHz oscillator (my original board had a 100 MHz oscillator).

    So, this code works with the ebay/aliexpress board:

     

    //************************************************
    //* dds test code for MKRZERO
    //* rev 0.2 Nov 2019
    //************************************************
    
    
    // ************** definitions ******************** 
    // input/output (I/O)
    #define IO_UPD_LOW digitalWrite(A4, LOW)
    #define IO_UPD_HIGH digitalWrite(A4, HIGH)
    #define SCLK_LOW digitalWrite(A1, LOW)
    #define SCLK_HIGH digitalWrite(A1, HIGH)
    #define SDIO_LOW digitalWrite(A2, LOW)
    #define SDIO_HIGH digitalWrite(A2, HIGH)
    #define CS_BAR_LOW digitalWrite(A5, LOW)
    #define CS_BAR_HIGH digitalWrite(A5, HIGH)
    #define RESET_LOW digitalWrite(A3, LOW)
    #define RESET_HIGH digitalWrite(A3, HIGH)
    #define LED_ON digitalWrite(LED_BUILTIN, HIGH)
    #define LED_OFF digitalWrite(LED_BUILTIN, LOW)
    // DDS registers
    #define CFR1 0
    #define CFR2 1
    #define ASF 2
    #define ARR 3
    #define FTW0 4
    #define FTW1 6
    #define RSCW0 7
    #define RAM 0x0b
    // these are used for converting a frequency in Hz to the register format
    // needed for the AD9954. If the system frequency is not 400 MHz this will need changing
    #define SYSFREQ 400E6
    #define TWLEN 4294967296
    // other definitions
    #define FOREVER 1
    // This disables the comparator. Set this to zero if
    // square wave output is required!
    #define COMPDIS 1
    // max amplitude is (2^14)-1 i.e. 16383
    #define MAX_OUTPUT 16383
    
    
    // ***************** structures *********************
    typedef struct freq_info_s {
      double hz;
      unsigned char regdata[4];
    } freq_info_t;
    
    
    // ********** function prototypes *******************
    void set_sysfreq(void); // sets up PLL to multiply the hardware crystal oscillator output
    void set_ctrl_reg1(void); // sets up the CFR1 (control function register #1) to some defaults
    void set_output_level(unsigned int amp); // set amplitude register 0-0x3fff (0x3fff is highest)
    void freq2ftw(double freq, unsigned char* data); // convert freq (in Hz) into 4 bytes that represent it
    void write_bytes(unsigned char instr, unsigned char* data, int len); // write instruction and data to AD9954
    
    
    // ************** initialization code ***************
    void setup() {
      int i;
      pinMode(A1, OUTPUT);
      pinMode(A2, OUTPUT);
      pinMode(A3, OUTPUT);
      pinMode(A4, OUTPUT);
      pinMode(A5, OUTPUT);
      pinMode(LED_BUILTIN, OUTPUT);
    
    
      // wait a short while for power to stabilise in the system.
      // blink an LED rapidly while we wait
      for (i=0; i<5; i++) {
        LED_ON;
        delay(50); // 50 msec delay
        LED_OFF;
        delay(50);
      }
      
      // Reset the AD9954 and get the pins into a known state
      RESET_HIGH;
      CS_BAR_HIGH; // initialize *CS to be high
      IO_UPD_LOW; // initialise IO_UPD to be low
      SCLK_LOW; // initialise SCLK to be low (data is toggled in on the rising edge)
      RESET_LOW; // bring the DDS board out of reset
      delay(50); // probably not needed but anyway..
    }
    
    
    // *************** main code ************************
    // note: this function, despite being called loop, never
    // gets to loop around, because I'm misusing it, by not
    // allowing the execution of the function to ever complete,
    // so that it cannot ever loop.
    void loop() {
      unsigned int output_level; // 0-0x3fff, with 0x3fff being the highest
      
      freq_info_t freq; // this holds the desired frequency
      freq_info_t freq2; // alternate desired frequency, for test purposes
      output_level=MAX_OUTPUT;
      freq.hz=89000000; // 89 MHz signal
      freq2.hz=89100000; // this is 89.1 MHz, used as a test
    
    
      // set up the AD9954 suitable for generating single tones
      set_ctrl_reg1(); // sets up CFR1 register with some defaults
      set_sysfreq(); // sets up CFR2 register with PLL settings
      set_output_level(output_level);
    
    
      // perform the math manipulation from Hz to FTW0 register format
      freq2ftw(freq.hz, freq.regdata);
      freq2ftw(freq2.hz, freq2.regdata);
      
      // done! now loop just this following segment of code forever
      while(FOREVER) // play out two frequencies alternated
      {
        LED_ON;
        write_bytes(FTW0, freq.regdata, 4);
        delay(1); // 1 millisecond delay
        LED_OFF;
        write_bytes(FTW0, freq2.regdata, 4);
        delay(1);
      }
      
    }
    
    
    // ***** set control reg 1 (CFR1) to some defaults ****
    void
    set_ctrl_reg1(void)
    {
      unsigned char data[4];
      data[0]=0x06; // OSK Enable; we need this to have amplitude control
      data[1]=0; data[2]=0x02; data[3]=0x00; // We always stick to MSB first mode. 0x42
      if (COMPDIS) data[3]|=0x40; // disable comparator
      write_bytes(CFR1, data, 4);
    }
    
    
    // ************** set SYSFREQ *************************
    // Sets SYSFREQ to 400MHz
    void
    set_sysfreq(void)
    {
      unsigned char data[3];
      // 100MHz external oscillator, multiplied by 4 for 400MHz system freq:
      //data[0]=0x18; data[1]=0; data[2]=0x24; // my board
      data[0]=0x18; data[1]=0; data[2]=0xa4; // Derek's board
      write_bytes(CFR2, data, 3);
    }
    
    
    // *********Set the amplitude register *****************
    // Range is 0 (lowest) to 0x3fff (highest)
    void
    set_output_level(unsigned int amp)
    {
      unsigned char data[2];
      unsigned char* aptr;
      aptr=(unsigned char*)&
      if (amp>0x3fff)
      {
        // error
        exit(1);
      }
      data[1]=*aptr; // adjust these lines for endian'ness
      data[0]=*(aptr+1);
      write_bytes(ASF, data, 2);
    }
    
    
    // ******* convert freq into 4 data bytes that represent it *****
    void
    freq2ftw(double freq, unsigned char* data)
    {
      unsigned char* tptr;
      unsigned int tword; // 32-bit tuning word
      
      tptr=(unsigned char*)&tword;
      tword=(unsigned int)((freq)*TWLEN/(SYSFREQ));
      // endian'ness: MKR ZERO: *tptr+0 is the least significant byte
      data[3]=*tptr; // adjust these lines for endian'ness
      data[2]=*(tptr+1);
      data[1]=*(tptr+2);
      data[0]=*(tptr+3); 
    }
    
    
    // **** Write instruction and data to the AD9954 *****************
    void
    write_bytes(unsigned char instr, unsigned char* data, int len)
    {
      int i, j;
      unsigned char dbyte, ibyte;
      
      ibyte=instr;
      CS_BAR_LOW;
      // transmit instruction byte
      for (i=0; i<8; i++)
      {
        if (ibyte & 0x80)
        {
          SDIO_HIGH;
        }
        else
        {
          SDIO_LOW;
        }
        ibyte=ibyte<<1;
        SCLK_HIGH;    
        SCLK_LOW;
      }
      
      // transmit data byte(s)
      for (j=0; j<len; j++)
      {
        dbyte=data[j];
        for (i=0; i<8; i++)
        {
          if (dbyte & 0x80)
          {
            SDIO_HIGH;
          }
          else
          {
            SDIO_LOW;
          }
          dbyte=dbyte<<1;
          SCLK_HIGH;
          SCLK_LOW;
        }
      }
    
    
      IO_UPD_HIGH; // toggle IO_UPD to transfer the data into the registers
      delay(1); // delay 1 millisec
      IO_UPD_LOW;
      CS_BAR_HIGH;
    }

     

    This test code above generates an FM-ish signal (not really, but it's enough for the test) at 89 MHz, so tuning an FM receiver to that frequency will result in a tone being heard.

     

    I also tried generating just an unmodulated signal, to see the output from the SMA connector marked OUT1 on the board:

     

    Board programmed for 12.7MHz output - the marker M1 indicates that the output was -9.2 dBm. RBW is set to 1 kHz. Span is 1 MHz for all of these screenshots:

    image

     

    Board programmed for 89 MHz, RBW set to 100 Hz:

    image

     

    Board programmed for 140.7 MHz:

    image

     

    The signal quality from the ebay/aliexpress board is great. The main chip alone costs £28+tax, so for generating RF (unmodulated, or FM or FSK) at sub-150 MHz, I think the board at £45GBP/$60USD is good value (plus the cost to attach to a MKR ZERO or whatever).

    An SDR would be more versatile (and cover a wider range), but for a good reference signal for test purposes, then the AD9954 board is better.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to shabaz

    Great work Shabaz!  I don’t think I would have ever thought to check if a pin marked PWR should be connected to GND :-). I looked at the photos of the board and did not see the offending pins.  Where are they located?

    Frank

     

    Edit:  never mind, found them.  They are on the data port.  Makes sense now.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 6 years ago in reply to shabaz

    Hi Shabaz,

     

    Joy o joy, cant believe it. Thank you soo much.

     

    Cant wait to get it back and start experimenting.

     

    Regards, Derek

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to derick007

    Hi Derek,

     

    Good news, it finally works : )

    I had a look at the board, it was not anything you were doing wrong, but basically the board didn't have some connections with defaults. On my board, I'd defaulted some pins using pull-down resistors etc.on the PCB itself, but on the ebay/aliexpress PCB, they are not defaulted.

    There are a couple of pins, marked IOSY and PWR (the actual pin names are IOSYNC and PWRDWNCTL), and they both needed to be connected to GND. After that was done, it worked.

    I'll get the board posted back to you on Friday or Saturday.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to shabaz

    Hi Shabaz and Derek,

     

    I am glad you are going to have a look at this.  The board is reasonably priced and would be useful so I was considering ordering one to see if I could help and figure it out myself.

    • Cancel
    • Vote Up +3 Vote Down