Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building A Direct Digital Synthesis Dual-Channel Signal Generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Aug 2018 6:37 AM Date Created
  • Views 29032 views
  • Likes 17 likes
  • Comments 148 comments
  • mbed enabled
  • ad9834
  • signal generator
  • direct digital synthesis (dds)
  • arm mbed
  • freescale
  • mbed os 5
  • dds
  • kinetis
  • direct digital synthesizer
  • ad9954
  • frdm
  • frdm-kl25z
  • radiofrequencych
  • mbed
  • frdm-family
  • frequency synthesizer
  • mbed-os
  • nxp
Related
Recommended

Building A Direct Digital Synthesis Dual-Channel Signal Generator

shabaz
shabaz
11 Aug 2018

Introduction

This blog post discusses some practical implementations of super-low-cost ($30 upward) direct digital synthesis (DDS) based signal generator for home use. To save effort and time, they can all be built around an off-the-shelf microcontroller board, and an off-the-shelf direct digital synthesis (DDS) board.

image

There are several different ideas discussed in this blog post, and all are similar – the principles are exactly the same, just that frequency range and desired control/monitoring capabilities can be chosen to suit needs. They are all be lumped together since they are all so similar.

 

There is a three-minute demo of the user interface here:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What Does it Do?

This project allows for the creation of controlled sine waves, at a desired frequency. This has uses for testing radio receivers, measuring the frequency response of filters, creating a radio transmission, creating a stimulus for testing amplifiers, and so on.

 

Manipulations such as frequency sweeping, frequency modulation and frequency shift keying (FSK) is possible with this project.

 

This project relies on an external amplifier or attenuator to adjust the signal level, although some limited adjustment is possible without additional hardware.

 

How Does it Work?

For a more in-depth look at DDS, see the blog post here Building a Frequency Synthesiser but briefly, the DDS board constructs a sine wave digitally by sending a table of numbers to a digital to analog converter (DAC). DDS devices allow a desired frequency to be programmed using an internal register (e.g. programmed via an SPI or other I/O bus). The programmed value is fed into a summing device or counter, known as a phase accumulator. This is just responsible for repeatedly adding the programmed value to the existing sum, on each clock cycle. So, if the desired frequency is a low value then the phase accumulator will increment in low values too. If the desired frequency is higher, then the phase accumulator will increment in larger chunks The phase accumulator loops back to zero once it reaches its maximum. Each possible value that the output of the accumulator can take represents a different point on a sinewave. A look-up table is used to convert from the phase accumulator output to an amplitude on the curve of a sine wave. This then drives a DAC and and external filter.

 

Some of the benefits are:

  • Extremely low noise close to the oscillation frequency
  • High granularity (sub-Hz is possible)
  • On-board RAM and instruction set allow for very fast frequency hopping or ramping (it is possible to achieve FM and FSK modulation using this method)

 

A disadvantage of DDS is that there can be some spurious content (usually relatively far away from the selected output frequency) that may need filtering for very demanding applications. Since filters can be expensive, often just a fixed low-pass filter is used, as in the project described here.

 

DDS boards are available from ebay, with a digital input interface, and an RF connector ready for providing the signal output. All that is required is to configure the DDS board to output the desired frequency, using a microcontroller for example.

 

For the project described here, a FRDM-KL25Z microcontroller boardmicrocontroller board is used. It is very low cost (about $15) and easy to program using a USB cable. For more detail about the board and the programming process, see here: Working with FRDM Boards and ARM mbed 

 

The board has 128 kbyte Flash and 16 kbyte RAM, and lots of input/output pins, on a near-credit-card-sized board around 5mm thick - it's really great!

(image source: NXP website)image

 

 

The easiest implementation was to not have any buttons or display on the device, and just enable the USB connection on the FRDM board to become a USB Serial interface. Thus whenever the user wishes to modify the frequency output, all that needs to be done is to connect the board to a PC via USB, and run terminal software such as PuTTY on Windows or ‘screen’ on Mac or Linux. A text-based menu system becomes the user interface.

image

 

With this method, the project can be constructed for about $30 or a bit more, depending on which DDS board is used. I tried two boards; a 0-10 MHz one, and a 0.05-160 MHz board.

 

If a permanent display is desired, an LCD screen can be attached. It adds another $20 to the cost. If buttons are needed, they can be added too. A rotary encoder or even a keypad could also be attached. There are plenty of free pins available on the FRDM board. Although I didn’t do it for this project, for information on how to attach a keypad, see here: Building a USB Keypad: A Mini-Project

 

In summary there’s a lot of flexibility concerning implementation. The core functionality uses the USB Serial menu system however. Code can be added to make use of the display, and buttons/keypad/encoder. I'd also like to incorporate a USB based SCPI interface (based on Jan Cumps SCPI project on element14) at some stage. This blog post is just to give ideas, not all combinations are implemented today so if you modify the code to implement a new combination, please do share the code.

 

The current code implements the text menu system, and rotary encoder for frequency selection, and display update indication of the menu selections and frequency. The plan is to extend rotary encoder usage so that it works with the menu system. So, if the text menu has the options such as sine and ramp at a particular menu level for instance, then the rotary encoder should also allow for selection of these two options before going into the next menu level in the hierarchy.

 

For this project I decided to develop my own menu system called picocli (I originally planned to take a Linux shell’s source code and run it Linux-kernel-less since the FRDM board has just a microcontroller). I may still revert to that, but for now I’m using custom code). It is at proof-of-concept level but functions reliably enough for now to use in this project, and it implements things like help, tab completion and a last-command history. It will be explored more in Part 2.

 

I also had to write a custom rotary encoder library rather than use an existing one, because I wanted to integrate things like velocity based modification of behaviour. Anyway, this was a short exercise compared to writing the menu system.

 

Making the Basic Configuration

The basic implementation (using a DDS board and the FRDM-KL25Z board connected to the PC for control via a USB serial interfaced menu) takes about five minutes to assemble. One or two boards are purchased and wired together with jumper cables.

image

 

For the DC to 10 MHz range, AD9834 boards are purchased. I have only tested a single AD9834 board, but two could be connected in theory if desired, for dual output, but there is no way to synchronise the two board outputs with the AD9834 chip.

 

For approx. 50 kHz to 160 MHz, AD9954 boards are used.

 

Nearly all the wiring throughout the project relied on jumper wires. To make these to custom lengths, this crimp toolthis crimp tool is great. It works with the crimpscrimps and then the result is inserted into SIL and DIL header socket shells. Standard pre-assembled jumper wires could be used too.

image

 

Here is a table of the specific wiring shown in the diagram above:

 

AD9834 DDS board markingFRDM-KL25Z board marking (conn. J9)
FSY  (fsync)B11 (PTB11) J9 pin 7
PS (phase select)B9 (PTB9)   J9 pin 3
SCK (clk)E3 (PTE3)   J9 pin 11
FS (freq select)B10 (PTB10) J9 pin 5
SDA (data)E2 (PTE2)   J9 pin 9
RST (reset)B8 (PTB8)   J9 pin 1
GND (0V)GND           J9 pin 12
5V5V              J9 pin 10

 

 

For using the 160 MHz boards, the connection diagram is below. Please note that I believe this diagram is correct, but I don’t have these actual boards to verify. I used some custom boards (based on the same chip) that I created a while back. However I see no reason why the ebay boards wouldn’t work.

image

 

With a bit of effort, it will be possible to have phase locked and phase adjustable outputs with these 160 MHz boards, since the AD9954 chip supports this capability. I have not tried it yet, because I’m still considering the optimal way to do that (I didn’t originally design my custom boards with that capability in mind : (

 

Still, there is plenty of room in the enclosure to add this capability at a future date once I’ve figured it out.

image

 

Building the Software

Instructions on how to use the development environment and how to push the compiled code into the board are described at the location mentioned earlier: Working with FRDM Boards and ARM mbed 

 

The code can be compiled and then programmed into the board via the USB cable. The next blog post will cover the software, but if you wish to use it now (it won’t be pretty code, it still needs tidying) then please let me know.

 

Using It

Connect up the output of the DDS board to an oscilloscope or spectrum analyzer, plug in the USB connection into the PC and the project should power up! Open up a serial terminal and connect to the board. Hit the Enter key and a command prompt (‘$’) should appear. You can type help or ? for assistance. Generally the menu structure has been designed to accept a command, or a command followed by parameters. Some commands will drop you into a new level in the menu, and you can exit that level by typing exit.

 

So, to output a sinewave at 1.2 MHz, type the following to enter the sinewave mode and invoke the signal output at the desired frequency:

 

$ sine
sine$ frequency 1.2M 
sine$ on

 

Here is another example, to generate a frequency sweep from 2.1 MHz to 2.2 MHz. Here the sweep command will drop you into the sweep mode, so type exit afterwards if you want to go into a different mode. You can type help or ? at any time to get help for the mode that you’re in:

 

sweep
range 2.1M 2.3M
on

 

There are extra parameters that can be configured (press ‘?’ to see the commands to do so) for adjusting the sweep steps and so on. I'd like to add a trigger output on the rear panel, so that the project can be used for basic scalar analysis of things like filters.

image

 

Adding a Display and User Controls

I decided to use an enclosure and front panel similar to what I’ve used before for this project: Building a SMT Pick-and-Place Buddy and so both projects rely on a Hammond instrument case and LCD on the front, and FRDM board stuck at the back so that the USB connector is accessible. The two signal outputs will also be at the back (using SMA connectors) because the front panel ended up becoming too full. It's not very convenient, but I can live with it.

image

 

This time I used a parallel mode LCD which is more inconvenient to use than the I2C displays, but I wanted to use it for the high quality output. The display uses ‘VATN’ LCD technology, which looks very close to Organic LED (OLED) in terms of contrast, when viewed at the right angle. So, it has near-OLED looks, but with LCD display lifetime, which seemed ideal for a test instrument. For the user input, I used a rotary encoder. An optical encoder with no detents is quite good for setting frequency, because it can be rapidly spun for getting from one end of the spectrum to the other in a short time. I used a Marquardt switch too. These almost feel like a keyboard switch, so they are light to press.

 

The Hammond case comes with aluminium plates, but plastic is easier to machine so I replaced the front panel with a black ABS plastic sheet instead, and cut a few other bits of plastic to hold the switch and rotary encoder at a convenient depth. A 3D printer could be used to make these, although I did it manually with sheet plastic.

image

 

After lots of epoxying, the front panel was semi-complete.

image

 

Sanding parts makes them easier to epoxy together. Thread-lock glue was used to hold some of the screwed bits together.

image

 

The particular rotary encoder I had operated at 5V whereas the FRDM-KL25Z board has 3.3V logic inputs, so a couple of potential divider resistor pairs were used on the quadrature encoder output lines, to drop from 5V to 3.3V (I used 1.8k and 3.3k resistors); the resistors can be seen attached to the header socket that will be connected to the rotary encoder in the photo below.

image

 

The LCD screen was a couple of millimetres taller than the inside of the case! : ( so I had to cut a shallow groove in the top and bottom of the case, to accommodate it. A piece of wood was glued to hold the display in the correct position. Jumper cables were used everywhere in case things ever need disassembly.

image

 

Performance

The performance is quite good, but that’s to be expected from DDS technology.

 

Here is what it looks like on an oscilloscope, using the AD9834 board; the output extends down to DC incidentally, because there is no output capacitor on the board.

image

 

The AD9954 board provides for up to 160 MHz output although at the low end it is limited; much lower than 50 kHz results in reduced amplitude, because my board has a transformer on the output. The ebay versions do not have this according to the photos on ebay, so they should extend down to DC.

image

 

It is hard to tell how good or bad a signal is from the ‘scope trace, so the FPC1500 spectrum analyzer was used. A span of 2MHz was examined when the DDS was set to 9.55MHz, and also 134MHz in the case of the AD9954. The result was good. The close-in noise is almost entirely due to the crystal oscillator module. The module on the AD9954 board for example contains an internal phase locked loop (PLL) to generate a 100MHz clock. Another PLL inside the AD9954 multiplies this by 4 to generate a 400MHz internal clock. I have a 400MHz oscillator module (which still uses a PLL) that I may try at some point; it has worse jitter than the 100MHz module, but it means that I can then disable the PLL inside the AD9954. Or I could try to source a better module, but it could get expensive.

 

The AD9834 board uses a similar style of oscillator module, with a PLL inside it too I suspect.

image

 

To see how this compared with a commercial signal generator, I connected a Rigol DG1022Z to the FPC1500. The DG1022Z has a 14-bit DAC internally, as does the AD9954 DDS chip.

 

The result is fairly similar when set to approximately the same power level. At higher output level this situation can change! - see the second spectrum trace below.

image

 

The DG1022Z operates to 25MHz, and I only tested at 10MHz. The AD9954 can go to 160MHz. Of course the DG1022Z is more flexible since it has arbitrary waveform capability too, but if just a sine wave and a few frequency modulation based schemes are required, then the AD9834 or AD9954 are great options.

 

Summary

A simple design has been presented to create a fairly usable signal generator. It costs less than $30 and perhaps half an hour of time to build and program it all. The full enclosure version takes longer of course.

 

It could be extended with an amplifier circuit if desired. If you build this project as-is or extend or modify it, it would be great to hear about it to bounce off ideas.

 

image

  • Sign in to reply
Parents
  • jc2048
    jc2048 over 8 years ago

    Thanks for posting this. It looks like a good route to getting a reasonable low-cost rf signal generator.

     

    It's got very good resolution but the accuracy is just that of the xtal. Got me wondering about the possibilities of locking it to an external source (like, maybe, radio time transmissions, where I vaguely seem to remember the carrier is derived from the atomic clock. Might suffer from atmospheric effects, though.)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 8 years ago in reply to jc2048

    Hi Jon, although MSF is locked to an Atomic clock at the transmitter the problem as you point out is that the  multipath and other variances in propagation are many times the error in a crystal.

    In order to average them out you would need a very large integration time to be useful. GPS modules are down to £3-4 and say less than £10 for units who's 1PPS output is really reliable so really they are better to lock up to altogether!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Problemchild

    This is an application note for TI's GPS receiver chips. It shows jitter of up to about 60nS on the 1PPS output.

     

    http://processors.wiki.ti.com/images/f/f1/TI_GPS_PPS_Timing_AppNote.pdf

     

    Long term it's very, very accurate because, like the off-air signals it goes back to an atomic clock, but short term it will have the same problems, won't it?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 8 years ago in reply to jc2048

    Jon that isnt that good for example the Neo8 chipset is around 25ns and variants designed for time reference have variences of 5 ish ns.

    That said it offers  better stability given long enough sample time!!

    I may note you can get OXCOs with a precision of 0.2 PPB at that point do you need to bother locking your source for most purposes!!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to michaelkellett

    I've just realized, that chip provides each output in phase, since there are programmable dividers taking the output from the common PLL in there. That would solve the current limitation and allow each DDS to be clocked identically : )

    I'm tempted to rip off the oscillators on the two boards, and fit that silabs dev-board in there!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to michaelkellett

    Silabs always has interesting parts. That one seems very handy.

    The xtal oscillator I'm currently using is On Semi NBXSBA010LN1TAGNBXSBA010LN1TAG of similar performance from what I can tell (they all specify it in different ways), i.e. as good as anything in low-midrange test equipment perhaps, without venturing into expensive module territory. For sub-£10 that was as best as I could find.

     

    I spent quite a while at the time figuring out how to get the oscillator signal into the DDS, and discussed with AD since there wasn't much information on clocking for that particular chip. That was about 4 years ago.

     

    However the silabs one is very interesting. It's more versatile and adjustable, is a fraction of the cost and a lot smaller. So would be the better choice now I think, although I have not done the sums, just looked at ballpark values. The fact that it goes to 333MHz would mean there is the possibility of just clocking at that rate and totally switching off the additional PLL inside the DDS (and just using the project up to say 130MHz, and re-do the filter on the output accordingly).

     

    I used this excellent website to convert the silabls jitter value into dBc/Hz values that I could loosely compare with the xtal osc on my board: https://www.changpuak.ch/electronics/phase_noise_jitter_conversion_reverse.php

     

    AD had a PDF that explained how to work out the overall phase noise here (on page 41): http://www.analog.com/media/en/training-seminars/design-handbooks/Technical-Tutorial-DDS/Section5.pdf

    When I did that with the On Semi part, I had no way to measure it at the time, but I was able to get a value using the FPC1500, at 10.7MHz, using a xtal filter, during the FPC1500 review. It was in an almost similar ballpark (well, still maybe 6dB out, but I didn't do it accurately, I was more curious if it was possible).

     

    The ebay boards would definitely need work done. They're possibly feeding in the oscillator single-ended, whereas it's worth putting in the effort to feed it in better (e.g. LVPECL) but then that needs termination resistors and there probably won't be space for those on the ebay board.

    (I don't have the ebay board, but I'm guessing what they've done is the go the low-cost route).

    Also, the output is using a single-ended output, whereas with the AD9954 and other DDSs it's possible to use a transformer on the balanced outputs. That would be too difficult to mod on the ebay board too : (

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to jc2048

    What about one of these:

     

    https://www.silabs.com/products/timing/clocks/low-jitter-clock-generators/device.si5332e-gm1

     

    And so long as you are happy with making those cables you don't even need to go down to chip level:

     

    https://www.silabs.com/products/development-tools/timing/clock/si5332-6ix-evb-development-kit

     

    The chips are cheap (sub £10) Arrow have stock but Mouser and DigiKey both list them but not in stock yet - it's a new part but very suitable for low volume applications because the crystal is built in - but is only 20ppm basic accuracy

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to shabaz

    I was thinking of something more modest than trying to compete with the very best that the large companies could do. Just going for something that was perhaps a bit better than the 20ppm or 30ppm accuracy you'd get with an off-the-shelf oscillator, maybe bringing it down to an accuracy of 1ppm, or something like that.

     

    In the old days, radio amateurs producing transmitters for 144Mz or 433MHz would use a crystal (often running third overtone) and then feed it to a 'multiplier'. The multiplier was an amplifier stage designed to deliberately generate a lot of second or third harmonic distortion that could then be filtered out (transistors are good at generating harmonic distortion). I've got a copy of Jessop's VHF-UHF Manual, published by the RSGB, here. One of the transmitter designs, for instance, used a 24MHz crystal running third overtone at 72MHz which was then doubled to 144MHz (I won't reproduce the circuit because it's copyright and not 'public' in the same way as a datasheet). If you find a copy of an old RSGB handbook or one of the ARRL ones you should find similar circuits. I don't know what such a scheme would be like for phase noise - to be honest, I haven't got a clue what I'm talking about here, really, just trying to add to the ideas - but you're better set up to look at these things than I am (if you're interested, that is).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to Problemchild

    I wish I knew more on this topic in general : ( I really don't : (

    I think Jon's referring to knowledge of the actual frequency, which needs calibration (even with an OCXO, the drift may be in parts per billion, but the actual frequency could be sufficiently different to be several Hertz off).

    For that, I don't think there's an easier/practical way than just counting over a long time, whether that's by GPS or terrestrial time signal, and then storing the offset for the DDS, and possibly some adjustment of the oscillator. I could be totally wrong. : (

     

    Personally I don't mind being several Hertz off, but there could be scenarios (e.g. if calibrating other gear, or for some radio or astronomy apps maybe, or for long term counters) where that isn't good.

     

    What I care about more is low jitter on the output signal. The OCXO isn't a full solution for me : ( cos most OCXO's are 10MHz, and then I need a PLL to get to a 400MHz clock (or higher for the newer DDSs). And when I do that, I get the PLL shape phase noise. The solution would be a discrete oscillator, which can have super low phase noise - but needs to be built with a lot of design and care, and hard to measure with readily accessible test equipment, or mega expensive to purchase. The actual frequency could be off by a lot, so would need still need temp compensation or ovenization, and calibration.

    I need a training course in timing : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to Problemchild

    I wish I knew more on this topic in general : ( I really don't : (

    I think Jon's referring to knowledge of the actual frequency, which needs calibration (even with an OCXO, the drift may be in parts per billion, but the actual frequency could be sufficiently different to be several Hertz off).

    For that, I don't think there's an easier/practical way than just counting over a long time, whether that's by GPS or terrestrial time signal, and then storing the offset for the DDS, and possibly some adjustment of the oscillator. I could be totally wrong. : (

     

    Personally I don't mind being several Hertz off, but there could be scenarios (e.g. if calibrating other gear, or for some radio or astronomy apps maybe, or for long term counters) where that isn't good.

     

    What I care about more is low jitter on the output signal. The OCXO isn't a full solution for me : ( cos most OCXO's are 10MHz, and then I need a PLL to get to a 400MHz clock (or higher for the newer DDSs). And when I do that, I get the PLL shape phase noise. The solution would be a discrete oscillator, which can have super low phase noise - but needs to be built with a lot of design and care, and hard to measure with readily accessible test equipment, or mega expensive to purchase. The actual frequency could be off by a lot, so would need still need temp compensation or ovenization, and calibration.

    I need a training course in timing : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Problemchild
    Problemchild over 7 years ago in reply to jc2048

    Jon, a TCXO or something similar in the firmware (especially if you have calibrated that source vs temperature) would get you in the the 1ppm range.

    Also that measurement is usually the basic accuracy which can simply be measured out beforehand. The unknown element is drift due to temperature change which is harder to deal with but a tempsensor and somecalibration could easily sort that out!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to shabaz

    I'm glad it looks useful - I'll be interested to hear which way you jump.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to michaelkellett

    I've just realized, that chip provides each output in phase, since there are programmable dividers taking the output from the common PLL in there. That would solve the current limitation and allow each DDS to be clocked identically : )

    I'm tempted to rip off the oscillators on the two boards, and fit that silabs dev-board in there!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to michaelkellett

    Silabs always has interesting parts. That one seems very handy.

    The xtal oscillator I'm currently using is On Semi NBXSBA010LN1TAGNBXSBA010LN1TAG of similar performance from what I can tell (they all specify it in different ways), i.e. as good as anything in low-midrange test equipment perhaps, without venturing into expensive module territory. For sub-£10 that was as best as I could find.

     

    I spent quite a while at the time figuring out how to get the oscillator signal into the DDS, and discussed with AD since there wasn't much information on clocking for that particular chip. That was about 4 years ago.

     

    However the silabs one is very interesting. It's more versatile and adjustable, is a fraction of the cost and a lot smaller. So would be the better choice now I think, although I have not done the sums, just looked at ballpark values. The fact that it goes to 333MHz would mean there is the possibility of just clocking at that rate and totally switching off the additional PLL inside the DDS (and just using the project up to say 130MHz, and re-do the filter on the output accordingly).

     

    I used this excellent website to convert the silabls jitter value into dBc/Hz values that I could loosely compare with the xtal osc on my board: https://www.changpuak.ch/electronics/phase_noise_jitter_conversion_reverse.php

     

    AD had a PDF that explained how to work out the overall phase noise here (on page 41): http://www.analog.com/media/en/training-seminars/design-handbooks/Technical-Tutorial-DDS/Section5.pdf

    When I did that with the On Semi part, I had no way to measure it at the time, but I was able to get a value using the FPC1500, at 10.7MHz, using a xtal filter, during the FPC1500 review. It was in an almost similar ballpark (well, still maybe 6dB out, but I didn't do it accurately, I was more curious if it was possible).

     

    The ebay boards would definitely need work done. They're possibly feeding in the oscillator single-ended, whereas it's worth putting in the effort to feed it in better (e.g. LVPECL) but then that needs termination resistors and there probably won't be space for those on the ebay board.

    (I don't have the ebay board, but I'm guessing what they've done is the go the low-cost route).

    Also, the output is using a single-ended output, whereas with the AD9954 and other DDSs it's possible to use a transformer on the balanced outputs. That would be too difficult to mod on the ebay board too : (

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to jc2048

    What about one of these:

     

    https://www.silabs.com/products/timing/clocks/low-jitter-clock-generators/device.si5332e-gm1

     

    And so long as you are happy with making those cables you don't even need to go down to chip level:

     

    https://www.silabs.com/products/development-tools/timing/clock/si5332-6ix-evb-development-kit

     

    The chips are cheap (sub £10) Arrow have stock but Mouser and DigiKey both list them but not in stock yet - it's a new part but very suitable for low volume applications because the crystal is built in - but is only 20ppm basic accuracy

     

    MK