Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building A Direct Digital Synthesis Dual-Channel Signal Generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Aug 2018 6:37 AM Date Created
  • Views 29004 views
  • Likes 17 likes
  • Comments 148 comments
  • mbed enabled
  • ad9834
  • signal generator
  • direct digital synthesis (dds)
  • arm mbed
  • freescale
  • mbed os 5
  • dds
  • kinetis
  • direct digital synthesizer
  • ad9954
  • frdm
  • frdm-kl25z
  • radiofrequencych
  • mbed
  • frdm-family
  • frequency synthesizer
  • mbed-os
  • nxp
Related
Recommended

Building A Direct Digital Synthesis Dual-Channel Signal Generator

shabaz
shabaz
11 Aug 2018

Introduction

This blog post discusses some practical implementations of super-low-cost ($30 upward) direct digital synthesis (DDS) based signal generator for home use. To save effort and time, they can all be built around an off-the-shelf microcontroller board, and an off-the-shelf direct digital synthesis (DDS) board.

image

There are several different ideas discussed in this blog post, and all are similar – the principles are exactly the same, just that frequency range and desired control/monitoring capabilities can be chosen to suit needs. They are all be lumped together since they are all so similar.

 

There is a three-minute demo of the user interface here:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What Does it Do?

This project allows for the creation of controlled sine waves, at a desired frequency. This has uses for testing radio receivers, measuring the frequency response of filters, creating a radio transmission, creating a stimulus for testing amplifiers, and so on.

 

Manipulations such as frequency sweeping, frequency modulation and frequency shift keying (FSK) is possible with this project.

 

This project relies on an external amplifier or attenuator to adjust the signal level, although some limited adjustment is possible without additional hardware.

 

How Does it Work?

For a more in-depth look at DDS, see the blog post here Building a Frequency Synthesiser but briefly, the DDS board constructs a sine wave digitally by sending a table of numbers to a digital to analog converter (DAC). DDS devices allow a desired frequency to be programmed using an internal register (e.g. programmed via an SPI or other I/O bus). The programmed value is fed into a summing device or counter, known as a phase accumulator. This is just responsible for repeatedly adding the programmed value to the existing sum, on each clock cycle. So, if the desired frequency is a low value then the phase accumulator will increment in low values too. If the desired frequency is higher, then the phase accumulator will increment in larger chunks The phase accumulator loops back to zero once it reaches its maximum. Each possible value that the output of the accumulator can take represents a different point on a sinewave. A look-up table is used to convert from the phase accumulator output to an amplitude on the curve of a sine wave. This then drives a DAC and and external filter.

 

Some of the benefits are:

  • Extremely low noise close to the oscillation frequency
  • High granularity (sub-Hz is possible)
  • On-board RAM and instruction set allow for very fast frequency hopping or ramping (it is possible to achieve FM and FSK modulation using this method)

 

A disadvantage of DDS is that there can be some spurious content (usually relatively far away from the selected output frequency) that may need filtering for very demanding applications. Since filters can be expensive, often just a fixed low-pass filter is used, as in the project described here.

 

DDS boards are available from ebay, with a digital input interface, and an RF connector ready for providing the signal output. All that is required is to configure the DDS board to output the desired frequency, using a microcontroller for example.

 

For the project described here, a FRDM-KL25Z microcontroller boardmicrocontroller board is used. It is very low cost (about $15) and easy to program using a USB cable. For more detail about the board and the programming process, see here: Working with FRDM Boards and ARM mbed 

 

The board has 128 kbyte Flash and 16 kbyte RAM, and lots of input/output pins, on a near-credit-card-sized board around 5mm thick - it's really great!

(image source: NXP website)image

 

 

The easiest implementation was to not have any buttons or display on the device, and just enable the USB connection on the FRDM board to become a USB Serial interface. Thus whenever the user wishes to modify the frequency output, all that needs to be done is to connect the board to a PC via USB, and run terminal software such as PuTTY on Windows or ‘screen’ on Mac or Linux. A text-based menu system becomes the user interface.

image

 

With this method, the project can be constructed for about $30 or a bit more, depending on which DDS board is used. I tried two boards; a 0-10 MHz one, and a 0.05-160 MHz board.

 

If a permanent display is desired, an LCD screen can be attached. It adds another $20 to the cost. If buttons are needed, they can be added too. A rotary encoder or even a keypad could also be attached. There are plenty of free pins available on the FRDM board. Although I didn’t do it for this project, for information on how to attach a keypad, see here: Building a USB Keypad: A Mini-Project

 

In summary there’s a lot of flexibility concerning implementation. The core functionality uses the USB Serial menu system however. Code can be added to make use of the display, and buttons/keypad/encoder. I'd also like to incorporate a USB based SCPI interface (based on Jan Cumps SCPI project on element14) at some stage. This blog post is just to give ideas, not all combinations are implemented today so if you modify the code to implement a new combination, please do share the code.

 

The current code implements the text menu system, and rotary encoder for frequency selection, and display update indication of the menu selections and frequency. The plan is to extend rotary encoder usage so that it works with the menu system. So, if the text menu has the options such as sine and ramp at a particular menu level for instance, then the rotary encoder should also allow for selection of these two options before going into the next menu level in the hierarchy.

 

For this project I decided to develop my own menu system called picocli (I originally planned to take a Linux shell’s source code and run it Linux-kernel-less since the FRDM board has just a microcontroller). I may still revert to that, but for now I’m using custom code). It is at proof-of-concept level but functions reliably enough for now to use in this project, and it implements things like help, tab completion and a last-command history. It will be explored more in Part 2.

 

I also had to write a custom rotary encoder library rather than use an existing one, because I wanted to integrate things like velocity based modification of behaviour. Anyway, this was a short exercise compared to writing the menu system.

 

Making the Basic Configuration

The basic implementation (using a DDS board and the FRDM-KL25Z board connected to the PC for control via a USB serial interfaced menu) takes about five minutes to assemble. One or two boards are purchased and wired together with jumper cables.

image

 

For the DC to 10 MHz range, AD9834 boards are purchased. I have only tested a single AD9834 board, but two could be connected in theory if desired, for dual output, but there is no way to synchronise the two board outputs with the AD9834 chip.

 

For approx. 50 kHz to 160 MHz, AD9954 boards are used.

 

Nearly all the wiring throughout the project relied on jumper wires. To make these to custom lengths, this crimp toolthis crimp tool is great. It works with the crimpscrimps and then the result is inserted into SIL and DIL header socket shells. Standard pre-assembled jumper wires could be used too.

image

 

Here is a table of the specific wiring shown in the diagram above:

 

AD9834 DDS board markingFRDM-KL25Z board marking (conn. J9)
FSY  (fsync)B11 (PTB11) J9 pin 7
PS (phase select)B9 (PTB9)   J9 pin 3
SCK (clk)E3 (PTE3)   J9 pin 11
FS (freq select)B10 (PTB10) J9 pin 5
SDA (data)E2 (PTE2)   J9 pin 9
RST (reset)B8 (PTB8)   J9 pin 1
GND (0V)GND           J9 pin 12
5V5V              J9 pin 10

 

 

For using the 160 MHz boards, the connection diagram is below. Please note that I believe this diagram is correct, but I don’t have these actual boards to verify. I used some custom boards (based on the same chip) that I created a while back. However I see no reason why the ebay boards wouldn’t work.

image

 

With a bit of effort, it will be possible to have phase locked and phase adjustable outputs with these 160 MHz boards, since the AD9954 chip supports this capability. I have not tried it yet, because I’m still considering the optimal way to do that (I didn’t originally design my custom boards with that capability in mind : (

 

Still, there is plenty of room in the enclosure to add this capability at a future date once I’ve figured it out.

image

 

Building the Software

Instructions on how to use the development environment and how to push the compiled code into the board are described at the location mentioned earlier: Working with FRDM Boards and ARM mbed 

 

The code can be compiled and then programmed into the board via the USB cable. The next blog post will cover the software, but if you wish to use it now (it won’t be pretty code, it still needs tidying) then please let me know.

 

Using It

Connect up the output of the DDS board to an oscilloscope or spectrum analyzer, plug in the USB connection into the PC and the project should power up! Open up a serial terminal and connect to the board. Hit the Enter key and a command prompt (‘$’) should appear. You can type help or ? for assistance. Generally the menu structure has been designed to accept a command, or a command followed by parameters. Some commands will drop you into a new level in the menu, and you can exit that level by typing exit.

 

So, to output a sinewave at 1.2 MHz, type the following to enter the sinewave mode and invoke the signal output at the desired frequency:

 

$ sine
sine$ frequency 1.2M 
sine$ on

 

Here is another example, to generate a frequency sweep from 2.1 MHz to 2.2 MHz. Here the sweep command will drop you into the sweep mode, so type exit afterwards if you want to go into a different mode. You can type help or ? at any time to get help for the mode that you’re in:

 

sweep
range 2.1M 2.3M
on

 

There are extra parameters that can be configured (press ‘?’ to see the commands to do so) for adjusting the sweep steps and so on. I'd like to add a trigger output on the rear panel, so that the project can be used for basic scalar analysis of things like filters.

image

 

Adding a Display and User Controls

I decided to use an enclosure and front panel similar to what I’ve used before for this project: Building a SMT Pick-and-Place Buddy and so both projects rely on a Hammond instrument case and LCD on the front, and FRDM board stuck at the back so that the USB connector is accessible. The two signal outputs will also be at the back (using SMA connectors) because the front panel ended up becoming too full. It's not very convenient, but I can live with it.

image

 

This time I used a parallel mode LCD which is more inconvenient to use than the I2C displays, but I wanted to use it for the high quality output. The display uses ‘VATN’ LCD technology, which looks very close to Organic LED (OLED) in terms of contrast, when viewed at the right angle. So, it has near-OLED looks, but with LCD display lifetime, which seemed ideal for a test instrument. For the user input, I used a rotary encoder. An optical encoder with no detents is quite good for setting frequency, because it can be rapidly spun for getting from one end of the spectrum to the other in a short time. I used a Marquardt switch too. These almost feel like a keyboard switch, so they are light to press.

 

The Hammond case comes with aluminium plates, but plastic is easier to machine so I replaced the front panel with a black ABS plastic sheet instead, and cut a few other bits of plastic to hold the switch and rotary encoder at a convenient depth. A 3D printer could be used to make these, although I did it manually with sheet plastic.

image

 

After lots of epoxying, the front panel was semi-complete.

image

 

Sanding parts makes them easier to epoxy together. Thread-lock glue was used to hold some of the screwed bits together.

image

 

The particular rotary encoder I had operated at 5V whereas the FRDM-KL25Z board has 3.3V logic inputs, so a couple of potential divider resistor pairs were used on the quadrature encoder output lines, to drop from 5V to 3.3V (I used 1.8k and 3.3k resistors); the resistors can be seen attached to the header socket that will be connected to the rotary encoder in the photo below.

image

 

The LCD screen was a couple of millimetres taller than the inside of the case! : ( so I had to cut a shallow groove in the top and bottom of the case, to accommodate it. A piece of wood was glued to hold the display in the correct position. Jumper cables were used everywhere in case things ever need disassembly.

image

 

Performance

The performance is quite good, but that’s to be expected from DDS technology.

 

Here is what it looks like on an oscilloscope, using the AD9834 board; the output extends down to DC incidentally, because there is no output capacitor on the board.

image

 

The AD9954 board provides for up to 160 MHz output although at the low end it is limited; much lower than 50 kHz results in reduced amplitude, because my board has a transformer on the output. The ebay versions do not have this according to the photos on ebay, so they should extend down to DC.

image

 

It is hard to tell how good or bad a signal is from the ‘scope trace, so the FPC1500 spectrum analyzer was used. A span of 2MHz was examined when the DDS was set to 9.55MHz, and also 134MHz in the case of the AD9954. The result was good. The close-in noise is almost entirely due to the crystal oscillator module. The module on the AD9954 board for example contains an internal phase locked loop (PLL) to generate a 100MHz clock. Another PLL inside the AD9954 multiplies this by 4 to generate a 400MHz internal clock. I have a 400MHz oscillator module (which still uses a PLL) that I may try at some point; it has worse jitter than the 100MHz module, but it means that I can then disable the PLL inside the AD9954. Or I could try to source a better module, but it could get expensive.

 

The AD9834 board uses a similar style of oscillator module, with a PLL inside it too I suspect.

image

 

To see how this compared with a commercial signal generator, I connected a Rigol DG1022Z to the FPC1500. The DG1022Z has a 14-bit DAC internally, as does the AD9954 DDS chip.

 

The result is fairly similar when set to approximately the same power level. At higher output level this situation can change! - see the second spectrum trace below.

image

 

The DG1022Z operates to 25MHz, and I only tested at 10MHz. The AD9954 can go to 160MHz. Of course the DG1022Z is more flexible since it has arbitrary waveform capability too, but if just a sine wave and a few frequency modulation based schemes are required, then the AD9834 or AD9954 are great options.

 

Summary

A simple design has been presented to create a fairly usable signal generator. It costs less than $30 and perhaps half an hour of time to build and program it all. The full enclosure version takes longer of course.

 

It could be extended with an amplifier circuit if desired. If you build this project as-is or extend or modify it, it would be great to hear about it to bounce off ideas.

 

image

  • Sign in to reply
Parents
  • derick007
    derick007 over 7 years ago

    Hi Shabaz,

     

    Took your advice and purchased the Arduino MKR zero.

     

    I am a novice SIMULINK user and i was hoping to use it to learn a bit about the Arduino board. However I am not exactly sure how to program the arduino board to control the AD9954.

     

    I can only imagine it is programed in coded in C / assembler  and the coded is detailed, complex and quite long ?

     

    I have never used the C programming language, but am willing to learn. Not sure if the whole task is a bit much but I would like to find out.

     

    Any pointers / suggestions would be welcome. In the end, making some adjustments to your code may be the solution.

     

    SIMULINK will communicate with the Arduino and control i/o, not sure if it will provide enough programming functionality to allow it to control the AD9954 board.

     

    If at all possible I will like to connect the AD9954 board to a pc to learn a bit about it. Analog Devices seem to suggest a parallel port is required to do this ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to derick007

    Hi Derek,

     

    The parallel port cannot be easily used, without additional hardware, since the parallel port is 5V only.

    There's no need to use a parallel port, you can communicate to a PC using the Arduino. There are many possibilities, it all depends on what you want to do, and what hardware you wish to use.

    To get you started, since you have a MKR ZERO board, you could try the code here, which should generate a 10MHz signal. It could be a basis for a more advanced program later, that could accept input from the PC via USB (as an example).

    I do not have a MKR ZERO, nor am I very familiar with Arduino, so there's no guarantee the code will work. It most likely will not work and will need some tweaks. It does compile.

    This is what the code does (so you can compare with the AD9954 datasheet). You may need to modify the code if the crystal is not 100MHz (my custom DDS board used a 100MHz crystal, but yours may have a different value).

     

    image

     

    Regarding connections, see lines 10-19 in the code, which indicate that the MKRZERO pins A0 to A4 are to be connected. The GND pin will also need connecting. Your AD9954 board will need powering from 3.3V or 5V or some other value, but hopefully this is marked on the board (or can be reverse-engineered by seeing what voltage regulator is on the board).

     

    Here is the code (hopefully it is possible to follow it in conjunction with the flow diagram above, to make adjustments). There's a couple of places in the code where the processor endian matters (there are comments in the code there), I think I've set it right for MKR ZERO, but I could be wrong.

     

     

    //************************************************
    //* dds test code for MKRZERO
    //* rev 0.1 June 2019
    //************************************************
    
    
    
    
    // ************** definitions ******************** 
    #define IO_UPD_LOW digitalWrite(A0, LOW)
    #define IO_UPD_HIGH digitalWrite(A0, HIGH)
    #define SCLK_LOW digitalWrite(A1, LOW)
    #define SCLK_HIGH digitalWrite(A1, HIGH)
    #define SDIO_LOW digitalWrite(A2, LOW)
    #define SDIO_HIGH digitalWrite(A2, HIGH)
    #define CS_BAR_LOW digitalWrite(A3, LOW)
    #define CS_BAR_HIGH digitalWrite(A3, HIGH)
    #define RESET_LOW digitalWrite(A4, LOW)
    #define RESET_HIGH digitalWrite(A4, HIGH)
    // DDS registers
    #define CFR1 0
    #define CFR2 1
    #define ASF 2
    #define ARR 3
    #define FTW0 4
    #define FTW1 6
    #define RSCW0 7
    #define RAM 0x0b
    
    
    #define SYSFREQ 400E6
    #define TWLEN 4294967296
    #define FOREVER 1
    
    
    // This disables the comparator. Set this to zero if
    // square wave output is required!
    #define COMPDIS 1
    
    
    // ********** function prototypes *******************
    void set_sysfreq(void); // set SYSFREQ
    void set_amplitude(unsigned int amp); // set amplitude register
    void freq2ftw(double freq, unsigned char* data); // convert freq into 4 bytes that represent it
    void write_bytes(unsigned char instr, unsigned char* data, int len); // write instruction and data to AD9954
    
    
    // ************** initialization code ***************
    void setup() {
      pinMode(A0, OUTPUT);
      pinMode(A1, OUTPUT);
      pinMode(A2, OUTPUT);
      pinMode(A3, OUTPUT);
      pinMode(A4, OUTPUT);
    
    
      // Reset the AD9954 and get the pins into a known state
      RESET_HIGH;
      CS_BAR_HIGH; // initialize *CS to be high
      IO_UPD_LOW; // initialise IO_UPD to be low
      SCLK_LOW; // initialise SCLK to be low (data is toggled in on the rising edge)
      RESET_LOW; // bring the DDS board out of reset
    
    
    }
    
    
    // *************** main loop ************************
    void loop() {
      unsigned int asf;
      double freq; // desired frequency
      unsigned char data[12];
      
      asf=16383; // max amplitude is (2^14)-1 i.e. 16383
      freq=10000000; // default to a 10MHz signal
    
    
      data[0]=0x06; // OSK Enable; we need this to have amplitude control
      data[1]=0; data[2]=0x02; data[3]=0x00; // We always stick to MSB first mode. 0x42
      if (COMPDIS) data[3]|=0x40; // disable comparator
      write_bytes(CFR1, data, 4);
        
      data[0]=255;
      write_bytes(ARR, data, 1); // set amplitude ramp rate register
        
      set_sysfreq();
      set_amplitude(asf); // 0x3fff is max amplitude
        
      freq2ftw(freq, data); // convert frequency into 4 data bytes (frequency tuning word)
      write_bytes(FTW0, data, 4);
      
      // done! loop forever.
      while(FOREVER)
      {
        delay(1000); // 1000 millisecond delay
      }
      
    }
    
    
    // ************** set SYSFREQ *************************
    // Sets SYSFREQ to 400MHz
    void
    set_sysfreq(void)
    {
      unsigned char data[3];
      data[0]=0x18; data[1]=0; data[2]=0x24; // 100MHz external oscillator, multiplied by 4 for 400MHz SYSFREQ
      write_bytes(CFR2, data, 3);
    }
    
    
    // *********Set the amplitude register *****************
    // Range is 0 (lowest) to 0x3fff (highest)
    void
    set_amplitude(unsigned int amp)
    {
      unsigned char data[2];
      unsigned char* aptr;
      aptr=(unsigned char*)&
      if (amp>0x3fff)
      {
        // error
        exit(1);
      }
      data[0]=*aptr; // adjust these lines for endian'ness
      data[1]=*(aptr+1);
      write_bytes(ASF, data, 2);
    }
    
    
    // ******* convert freq into 4 data bytes that represent it *****
    void
    freq2ftw(double freq, unsigned char* data)
    {
      unsigned char* tptr;
      unsigned int tword; // 32-bit tuning word
      
      tptr=(unsigned char*)&tword;
      tword=(unsigned int)((freq)*TWLEN/(SYSFREQ));
      data[0]=*tptr; // adjust these lines for endian'ness
      data[1]=*(tptr+1);
      data[2]=*(tptr+2);
      data[3]=*(tptr+3);
    }
    
    
    // **** Write instruction and data to the AD9954 *****************
    void
    write_bytes(unsigned char instr, unsigned char* data, int len)
    {
      int i, j;
      unsigned char dbyte, ibyte;
      
      ibyte=instr;
      CS_BAR_LOW;
      // transmit instruction byte
      for (i=0; i<8; i++)
      {
        if (ibyte & 0x80)
        {
          SDIO_HIGH;
        }
        else
        {
          SDIO_LOW;
        }
        ibyte=ibyte<<1;
        SCLK_HIGH;    
        SCLK_LOW;
      }
      
      // transmit data byte(s)
      for (j=0; j<len; j++)
      {
        dbyte=data[j];
        for (i=0; i<8; i++)
        {
          if (dbyte & 0x80)
          {
            SDIO_HIGH;
          }
          else
          {
            SDIO_LOW;
          }
          dbyte=dbyte<<1;
          SCLK_HIGH;
          SCLK_LOW;
        }
      }
    
    
      IO_UPD_HIGH; // toggle IO_UPD to transfer the data into the registers
      delay(1); // delay 1 millisec
      IO_UPD_LOW;
    }

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    Thank you for the code and the reply.

     

    I have just found out the AD9954 evaluation board is substantially different from the AD9954 board I purchased.

     

    The board I purchased does not include a few connectors such as the DB25 connector for the parallel port.

     

    Looks like I will have to dive straight in and try and use your code to program the Arduino board which in turn will control the AD9954 board to produce a 10 MHz signal.

     

    I might be gone awhile.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to derick007

    Hi Shabaz,

     

    I am not really sure of the difference between Linear Sweep Mode of Operation and RAM mode.

     

    Presumably with the AD9954, the Linear Sweep Mode is where all you have to do is program AD9954 with the START & STOP frequencies and how fast they transition ? Advantages – little to do in the way of programming, but limited to sinewaves only ?

     

    Whereas the RAM mode, is where you calculate exact values of the waveform you want and store the values in RAM ? Can generate any desired waveform, but requires relatively more programming effort ?

     

    Therefore in order to generate a BFSK signal, it would be better to use the Linear Sweep Mode ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to derick007

    Hi Derek,

     

    As Frank says, the 20MHz thing is unusual. The SCLK pin doesn't need to be generating a 20MHz signal.

    SCLK is only toggled (at a slower rate) as data is shifted into the chip. Otherwise, SCLK is idle.

    I don't have a way of testing the code, but the code I pasted earlier does compile in the Arduino window. It may not function though, but it should be close. It sends instructions to the DDS to generate a frequency, and then it idles. Once you can get that working, then you can rewrite it to do whatever you intend it to do.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to derick007

    If you pull the window with the error message in it more fully open it may give further detail.  Try not commenting out setup() as I believeArduino expects to always see it.  Calling tone continuously in a loop is probably not what you want to do - it is calling a function that generates a square wave with unlimited duration over and over.   Also I don’t know for sure but doubt it can generate a 20 MHz square wave.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    Trying to toggle the SCLK line (A1 on the MKRZERO board) using the code attached.

    Unfortunately when I try to compile, I get an error message telling me I have a complie error for the MKRZERO board ?

    {gallery} My Gallery Title

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to derick007

    Hi Derek,

     

    For toggling the SCLK line, I'm suggesting eventually doing away with all delays, i.e. just let it toggle out at its highest speed, if the Arduino cannot output at a rate higher than 25MHz anyway.

    (But slowed down with delays for initial testing).

    For anywhere else that you need timing of data, you'll likely need to use delays or timers.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to shabaz

    Hi Shabaz, thanks for getting back.

     

    1. Frequency of the SCLK line.

     

    From your comments, I will definitely slow the toggling down, however the following has me thinking,

     

    "  If you don't use the delay function, it will likely be fine, "

     

    Is there another function / way to generate a clock signal on the Arduino board ?

     

    Regards, Derek

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • derick007
    derick007 over 7 years ago in reply to shabaz

    Hi Shabaz, thanks for getting back.

     

    1. Frequency of the SCLK line.

     

    From your comments, I will definitely slow the toggling down, however the following has me thinking,

     

    "  If you don't use the delay function, it will likely be fine, "

     

    Is there another function / way to generate a clock signal on the Arduino board ?

     

    Regards, Derek

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 7 years ago in reply to derick007

    When you generate an analogue signal from a DAC you need a low pass filter after the DAC. If you could design a filter with infinite slope you would get a perfect sine wave, after infinite time, with a sample rate equal to twice the frequency of a sine wave output.

    In practice you might use a 4th order filter (24dB/Octave) and you would need at least 2 octaves to get a decent signal, so the filter cut off frequency would need to be at 1/8th of the sample rate - so your 400MHz clock will allow you to get a decent 50MHz sine wave.

    With better filters you can push this up to maybe 100MHz - but designing an 8th order filter to work at 100MHz may well be out of you comfort zone image

     

    Try Googling "reconstruction filters"

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to shabaz

    Hi Shabaz, still struggling with the DDS project.

     

    I was hoping you could give me some help re. DDS theory.

     

    If the ref. clock is 400 MHz and I want to produce a sinewave of 40 MHz, then I will have 10 samples to send to the DAC ?

    If I want to produce a sinewave of 80 MHz, then I will only have 5 samples to send to the DAC ?

     

    If my understanding above is correct, then in order to produce an accurate sinewave we are limited to a maximum frequency ?

    In this case could you advise what this maximum frequency would be ?

     

     

    Many thanks, Derek

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to fmilburn

    Hi Frank,

     

    I think I have solved the uploading problem by simply hitting the RESET button twice.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to derick007

    I am not an Arduino expert but are you able to upload other sketches and have them work - e.g. the blink example?  What have you tried doing to get the upload to work - e.g. shutting down and restarting. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 7 years ago in reply to shabaz

    Hi Shabaz, Frank

     

    I have changed the sketch drammatically and have compiled it successfully.

     

    Unfortunately I have problems uploading to the MKRZERO, which seems to happen quite alot according to some of the Forums I have read.

     

    I uploaded the first sketch a few days ago and it worked fine. I put my scope on the board and was able to see a square wave.

     

    However when I tried changing the frequency by altering the tone() function and uploading again I got an error message "An error occurred while uploading the sketch"

     

    The board still retains and executes the original sketch, outputting a square wave.

     

    The problem now is uploading the sketch and not so much the actual sketch ?

     

    Derek