Test & Tools
  • Technologies
  • More
Test & Tools
Blog Keithley DMM6500 Scanner Card - first impressions
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 7 Feb 2023 9:45 PM Date Created
  • Views 5897 views
  • Likes 11 likes
  • Comments 16 comments
  • 88ad1490-a97d-11ed-afa1-0242ac120002
  • 2000-scan
  • dmm6500
  • keithley
  • scan-2000
Related
Recommended

Keithley DMM6500 Scanner Card - first impressions

Jan Cumps
Jan Cumps
7 Feb 2023
Keithley DMM6500 Scanner Card - first impressions

I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This is my fist little test after receiving it.

image

I bought a 2nd hand card. 250€ on eBay. It's the relay version (there's also a solid-state version).
It can switch 10 2-wire inputs. For low resistance measurements, you can make 5 4-wire measurements. 

Photos

At the top of the post, you see the front side with the lid closed. Here is the same view with that lid open.

image

This is the unspectacular underside:

image

Wiring it up

I've wired channel 1 and 6 up. So that I can do 2 2-wire measurements or one 4-wire one.

image

Then plugged the card into the DMM dock:

image

I connected the 2 channels to a power supply. Channel 1 to a 1V dc output. Channel 2 to 1.5V dc.

Specs

image

Setting up a simple scan

I defined a DC Volt scan for both, taking 1 sample on each channel

image

image

Then I used the Channel App, and ran the scan:

image

Simple start, but it worked as expected.

link to all posts

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Gough Lui +1
    I'm surprised you didn't actually build one Look here: DC switching board . neuromodulator made one. I've been thinking (and procrastinating) about it too. Then this one popped up in my eBay search…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Gough Lui +1
    One hesitation I would have buying second hand is simply the amount of wear on the relays. It was a gamble. That's why I never bought 2nd hand ones that were going for a higher price. 250 € is still…
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    What I'm trying to do:

    @ghoug had a question about how often the relays were used before I bought the card.
    The DAQ6510 has an app to check the click counts. That app doesn't run on the DMM6500, and doesn't know the SCAN-2000 card. I try to port it.

    Current status: I can detect the card,

    image

    And get its specifications, but not (yet?) the click count.

    image

    I didn't read docs or check anything. I try to wing it by just looking at the code and massage it. I haven't checked if my card actually stores the click counts per relay...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    I got it working. Unfortunately, this card doesn't persist the click count (it's supported on some counts for the 7xxx series, but not for this one). I can use it to see how many times the relays were used until power cycle.

    Here is the output after I ran 1 scan on channel 1 and 6:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    I got it working. Unfortunately, this card doesn't persist the click count (it's supported on some counts for the 7xxx series, but not for this one). I can use it to see how many times the relays were used until power cycle.

    Here is the output after I ran 1 scan on channel 1 and 6:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • neuromodulator
    neuromodulator over 3 years ago in reply to Jan Cumps

    The reference manual states:

    "The DMM6500 keeps an internal count of the number of times each relay has been closed. This count can help you determine when relays require replacement. Refer to the card documentation for the contact life specifications for the relays."

    It's not like it would have increased the price that much to keep the count in the board itself.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to neuromodulator

    > It's not like it would have increased the price that much to keep the count in the board itself.

    That is true. But this is the basic card. They have ones that keep count, but they cost more.

    This one is capable but bare-bones. All logic comes from the DMM.