Test & Tools
  • Technologies
  • More
Test & Tools
Blog Keithley DMM6500 Scanner Card - first impressions
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 7 Feb 2023 9:45 PM Date Created
  • Views 5908 views
  • Likes 11 likes
  • Comments 16 comments
  • 88ad1490-a97d-11ed-afa1-0242ac120002
  • 2000-scan
  • dmm6500
  • keithley
  • scan-2000
Related
Recommended

Keithley DMM6500 Scanner Card - first impressions

Jan Cumps
Jan Cumps
7 Feb 2023
Keithley DMM6500 Scanner Card - first impressions

I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This is my fist little test after receiving it.

image

I bought a 2nd hand card. 250€ on eBay. It's the relay version (there's also a solid-state version).
It can switch 10 2-wire inputs. For low resistance measurements, you can make 5 4-wire measurements. 

Photos

At the top of the post, you see the front side with the lid closed. Here is the same view with that lid open.

image

This is the unspectacular underside:

image

Wiring it up

I've wired channel 1 and 6 up. So that I can do 2 2-wire measurements or one 4-wire one.

image

Then plugged the card into the DMM dock:

image

I connected the 2 channels to a power supply. Channel 1 to a 1V dc output. Channel 2 to 1.5V dc.

Specs

image

Setting up a simple scan

I defined a DC Volt scan for both, taking 1 sample on each channel

image

image

Then I used the Channel App, and ran the scan:

image

Simple start, but it worked as expected.

link to all posts

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Gough Lui +1
    I'm surprised you didn't actually build one Look here: DC switching board . neuromodulator made one. I've been thinking (and procrastinating) about it too. Then this one popped up in my eBay search…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Gough Lui +1
    One hesitation I would have buying second hand is simply the amount of wear on the relays. It was a gamble. That's why I never bought 2nd hand ones that were going for a higher price. 250 € is still…
Parents
  • dougw
    dougw over 3 years ago

    That meter can no doubt measure the contact resistance of the relays....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 3 years ago

    That meter can no doubt measure the contact resistance of the relays....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to dougw

    Yes, it would be able to measure itself, with some wit and wiring. 

    Contact Life: >105 operations at maximum signal level; >108 operations cold switching.

    Contact Resistance: < 1 Ohm at end of life