Test & Tools
  • Technologies
  • More
Test & Tools
Forum Ti LDC1000EVM A Question on Inductance
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 2 answers
  • Subscribers 386 subscribers
  • Views 7630 views
  • Users 0 members are here
  • ldc1000evm
  • inductors
Related

Ti LDC1000EVM A Question on Inductance

jw0752
jw0752 over 11 years ago

Inspired by shabaz I purchased a TI  LDC1000EVMLDC1000EVM Evaluation Kit and set it up If you want more information on the kit itself check out Shabaz's blog as it is very interesting Getting Started with the LDC1000 - Small Metal Detection!

 

After setting up the board I wanted to confirm some of the things I thought I understood about inductors and so I performed a couple of experiments and my results leave me with a question that I am hoping you can help me with.

 

My first experiment was to look at the inductor in free air.

 

image

 

The GUI for the Evaluation board was reading 19.496 uH with an open air core.

 

image

 

For my next experiment I inserted a small ferrite core into the inductor.

 

image

 

My expectation was that this ferrite core would increase the inductance of the coil. I was not disappointed as the inductance rose to 30 uH.

 

image

 

My next experiment was to replace the ferrite core with a soft steel rod of similar length to the ferrite one.

 

image

 

To my surprise and confusion the inductance of the coil dropped to 16.811 uH which was almost 3 uH lower than open air. I am hoping that someone can explain this behavior to me. I did not expect the steel core to do as well as the ferrite but I did expect it to do better than open air.

 

image

 

I have my physics book open right now and I am reviewing inductors to see if I can better understand why a steel core would lower the inductance of a coil instead of raising it.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago in reply to jw0752 +3
    I snapped off that resonant circuit and applied it to the VNA, this is the result I get (it could be inaccurate, the VNA is freshly built and could have issues. I'm still learning how to use it). I've…
  • DAB
    DAB over 11 years ago +2
    Hi John, After reading your post I remembered something I wrote in my book about how the crystalline structure of iron behaves under a magnetic field. The ferrite core is a very homogeneous material, so…
  • shabaz
    shabaz over 11 years ago +2 verified
    Hi John and Everyone, Chris Oberhauser from TI replied : At the higher frequencies (>500kHz) that LDC devices typically operate, the eddy currents on the target surface overwhelm the permeability and…
Parents
  • michaelwylie
    0 michaelwylie over 11 years ago

    John;

     

    Any chance that it's stainless steel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to michaelwylie

    Hi Michael,

    It is really good to hear from you. I used a magnet on all my test pieces and the piece in question is definitely regular soft steel. I did not try stainless steel but I will later on tonight when I am back in the shop. What is your prediction for the effect of stainless? I did use some other coils and an Inductance meter to verify that in fact the steel core does increase the inductance of a coil. The effect I was seeing has to be the result of the energy losses introduced by the steel into the field of the EVM test coil and the algorithm being used by the evaluation module to determine the inductance. While the evaluation kit does read out the inductance of the test coil I do not believe that it is really designed as an inductance tester as much as a sensitive inductive proximity sensor. I have yet to read the Data Sheet so I hope to have a better understanding soon.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to michaelwylie

    Hi Michael,

    It is really good to hear from you. I used a magnet on all my test pieces and the piece in question is definitely regular soft steel. I did not try stainless steel but I will later on tonight when I am back in the shop. What is your prediction for the effect of stainless? I did use some other coils and an Inductance meter to verify that in fact the steel core does increase the inductance of a coil. The effect I was seeing has to be the result of the energy losses introduced by the steel into the field of the EVM test coil and the algorithm being used by the evaluation module to determine the inductance. While the evaluation kit does read out the inductance of the test coil I do not believe that it is really designed as an inductance tester as much as a sensitive inductive proximity sensor. I have yet to read the Data Sheet so I hope to have a better understanding soon.

    John