Test & Tools
  • Technologies
  • More
Test & Tools
Forum MULTICOMP PRO MP750065 Function Generator - Programming Pt3: LabVIEW tryout (b)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 386 subscribers
  • Views 2607 views
  • Users 0 members are here
  • MP750065
  • function_generator
  • labview
  • scpi
Related

MULTICOMP PRO MP750065 Function Generator - Programming Pt3: LabVIEW tryout (b)

Jan Cumps
Jan Cumps over 4 years ago

The 3rd post in this Program the Device series talks about initial LabVIEW integration. An unstructured test to see if I can set up a meaningful conversation with the instrument.
It's the follow up of Programming Pt2: LabVIEW tryout (a).
For the MP750668, UTG900C-II, UTG1010 owners: this will very likely work for you too.

image
image: 2nd half of the functional flow. Click to enlarge

In this I resume where the previous one ended, showing how to read the current frequency and close the session. 

In a next post, I'll break this flow up in the traditional LabVIEW Virual Instrument blocks (Init, Close, basic Read and Write, and some advanced blocks to set and get favourite values, e.g. Set Freq, Get Freq, Set Waveform, ...)

Full LabVIEW Flow (part b)

You can see the full process in the header of the previous post. There are two remaining activities

Read Current Frequency

API function: uci_ReadX()

image
image: read the frequency that the instrument is currently set to

The left block is again a Call Library Function block on the right side, now configured for dll function uci_ReadX(). I will not repeat the inputs and outputs we see in each block.
The two parameters I want to highlight are the command string and return value size.
The command is a literal constant now. The same one I used in post 1, to read channel 0's frequency. When I build the driver, I will parameterise the channel number. Some UCI capable instruments have two channels.
The response size is set to 8. That's the number of bytes returned by this call, in the documentation.

On the output side, you see a construct to translate the 8 bytes reply array to a double.
First the array is flattened, so that it becomes a 4 byte string. Then the byte order is swapped for endianness.
Finally, this reversed byte string is type-cast into a double that you can show on the LabVIEW front panel.

image
image: front panel, with the frequency that we just read in orange

Close the Session

API function: uci_Close()

image

image: session and resource cleanup

The tail end of this test flow closes the session. This releases the USB handle we're using.
DLL resources are freed, and other programs can now access the instrument again.
The only input is the active session, that's been passed through the flow from the very first block on.
The session is no longer valid  after this call. If you want to submit new commands, you need to reopen the instrument.

In action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Related blog:

MULTICOMP PRO MP750065 Function Generator - 1st impressions
Programming Pt1: SDK Demo
Programming Pt2: LabVIEW tryout (a)
Programming Pt3: LabVIEW tryout (b)
Programming Pt4: LabVIEW Driver Lib Init block
Programming Pt5: LabVIEW Driver Lib Read, Write and Close blocks
Programming Pt6: LabVIEW Driver Lib: High Level Functional blocks
  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    next post creates the first Virtual Instrument blocks:  MULTICOMP PRO MP750065 Function Generator - Programming Pt4: LabVIEW Driver Lib Init block

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 4 years ago

    next post creates the first Virtual Instrument blocks:  MULTICOMP PRO MP750065 Function Generator - Programming Pt4: LabVIEW Driver Lib Init block