Test & Tools
  • Technologies
  • More
Test & Tools
Forum Solder station selection
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 388 subscribers
  • Views 3954 views
  • Users 0 members are here
Related

Solder station selection

davebullockmbe
davebullockmbe over 7 years ago

Hi everyone,

Having worked for many years with an ERSA  Analog 60A and then an ERSA  Digital 2000A both equipped with the TechTool iron I am spoiled when it comes to choosing a similar machine.

My son is getting interested in electronic construction and a solder station for Christmas seems like a great present.

However to set him up with a full ERSA kit with spare tips and maybe a replacement heating element would be well over £500.

I love the ERSA ease of tip change and the instant availability of continuous heat when soldering large components (you can solder a washer to a battleship..LOL) but how do less expensive setups perform?

Each alternative I follow up has both glowing praise and dire reviews in equal measure, it's so confusing!

So what are you you all using, and can I have some recommendations/warnings of what to choose/avoid from the Farnell range please?

Thanks in anticipation.....

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5
    I have several irons, but the one I use all the time is an old Hakko 936 - it has worked consistently well for many years. There seem to be other companies either cloning or licensing Hakko designs. This…
  • Jan Cumps
    Jan Cumps over 7 years ago +4
    I'd keep it very simple for a kid. It's not the gear that counts, but the pleasure of soldering.
  • michaelkellett
    michaelkellett over 7 years ago +3
    I've been using i-con picos for years (since ERSA stopped supporting the big expensive station I had.) I've found them to be pretty good. I also have an RS Pr Ds90 which is good for heavier work and has…
Parents
  • hlipka
    hlipka over 7 years ago

    I'm using a ERSA i-con pico for several years now, and I really like it. Heats up quite fast, and has no problems controlling the temperature. Only drawback: its non-antistatic (its not grounded), you would need the i-con nano for that.

    For someone starting in electronics one of the cheaper T12 soldering stations might be better, though. I have one as replacement (should the pico ever fail), and it also works quite well (though the hand-set is not as nice as the one from the ERSA).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hlipka
    hlipka over 7 years ago

    I'm using a ERSA i-con pico for several years now, and I really like it. Heats up quite fast, and has no problems controlling the temperature. Only drawback: its non-antistatic (its not grounded), you would need the i-con nano for that.

    For someone starting in electronics one of the cheaper T12 soldering stations might be better, though. I have one as replacement (should the pico ever fail), and it also works quite well (though the hand-set is not as nice as the one from the ERSA).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • davebullockmbe
    davebullockmbe over 7 years ago in reply to hlipka

    Thanks Hendrik,

    That's just the sort of operational insight I needed, I will check out the ERSA icon-pico now.

    Dave