Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need help with some measurements.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 387 subscribers
  • Views 5419 views
  • Users 0 members are here
  • non_slip_probes
Related

Need help with some measurements.

jw0752
jw0752 over 7 years ago

I need some help collecting data about Oscilloscope Probes. I am thinking of making some low frequency Non-Slip probe tip adapters for Oscilloscope probes. With the limited number of Oscilloscope probes with in my reach it does not look like there is any standardization.

 

image

As you can see the two probes that I own each have different diameter probe tips. It would help me plan my project if I could find out what the diameter and length of oscilloscope probes from as many of you as possible. Please measure length of the consistent diameter of the tip and also the diameter itself. I can accept measurement in inches or millimeters. Here is what I hope to be able to build without having to custom make each one.

 

image

 

Your help would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago in reply to dougw +9
    I have 3 types of probe: pin diameter = PD pin length = PL ground ferule diameter = GD ground ferule length = GL plastic barrel diameter = BD plastic barrel length = BL all dimensions in mm
  • Gough Lui
    Gough Lui over 7 years ago in reply to Gough Lui +7
    jw0752 - I decided to give my improvised method a go - I grabbed a piece of foil and corrugated cardboard, punched the probe tip through the foil into the cardboard and scanned the foil at 4800dpi to judge…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jw0752 +7
    w2aew - a field engineer of Tektronix - has made nice videos on (among other interesting subjects) probing techniques. I use this one at times when direct probing with the pig tail ground is not enough…
  • 14rhb
    14rhb over 7 years ago in reply to jw0752

    Not a problem, you must be amassing the greatest data survey of oscilloscope probes ever undertaken. I took the photo using my mobile phone camera whilst using an eyeglass/loupe.

     

    Rod

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi John.

     

    Sorry for the delay on this, I took a look at the probes here, and I wasn't sure what level of detail you needed, so sketched this up, so that we're using the same terminology (I took Doug's naming convention : ):

    image

     

    For the three probes I have, these are the measurements:

    Tektronix TPP0200TPP0200:

    PD1 = 0.73mm

    PD2 = 1.12mm

    GD = 3.80mm

    BD = 4.93mm

    PL1 = 4.0mm approx

    PL2 = 4.5mm approx

    PL3 = 0.5mm approx

    PGL = 4.5mm approx

    GL = 3.0mm approx

    BL = 20.8mm approx

     

    Tektronix TPP1000TPP1000:

    PD1 = PD2 = 0.65mm

    GD = 3.85mm

    BD = 4.95mm

    PL1 = 2.0mm approx

    PL2 = 3.5mm approx

    PL3 = 2mm approx

    PGL = 5.0mm approx

    GL = 3.0mm approx

    BL = 14.5mm approx

     

    Picoscope TA375:

    PD1 = 0.91mm

    PD2 = 1.34mm

    GD = 4.82mm

    BD = 6.20mm

    PL1 = 5.0mm approx

    PL2 = 6.0mm approx

    PL3 = 0.00mm

    PGL = 5.0mm approx

    GL = 3.6mm approx

    BL = 26.0mm approx

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    Can I say Wow!  That is a really nice collection of data. Thank you for all the time you put into helping me.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jw0752

    No problem at all! Thanks for all the valuable information you share, and also the nice test probes you sent me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 7 years ago

    Hi John

     

    I'd like to help, but all my probes are the spring loaded "hooky" type. I'm afraid if I want to probe a socket, I usually poke a patch lead in and then hook on to the other end of the patch.

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to neilk

    can you remove the spring loaded hook tip?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 7 years ago in reply to Jan Cumps

    Wow - why didn't I think of that!!!!!!! image

     

    I have 3 probes - all appear to be made by RS Components

     

    All 2 are similar, 3rd quite different

    All measurements in mm

     

    Pin Diameter          1.4     1.4     0.7

    Pin Length              4.8     3.8     3.8

    Ground Dia             7.6     6.5     4.8

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to neilk

    Hi Neil,

    Thanks for taking the time to get the measurements for me. It is amazing that in a little over a week I have amassed data on probe tip sizes from all over the world.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<