• Products and Partners
    Products and Partners
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
Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - ADC and DAC BoosterPack test
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Nov 2017 11:12 AM Date Created
  • Last Updated Last Updated: 2 Dec 2017 10:04 AM
  • Views 5874 views
  • Likes 7 likes
  • Comments 35 comments
Related
Recommended

Programmable Electronic Load - ADC and DAC BoosterPack test

WIP

 

This blog documents the characteristics of the DAC/ADC BoosterPack of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

We have the same DAC/ADC BoosterPacks so we can compare the measurements of each ADC and DAC channel. Check the main document for anything related to hardware and firmware.image

 

Test Setup

 

Peter has created a GUI that we can use to shoot SCPI commands. We can control the DACs and read the ADCs.

Measurements are performed with and without the power driver BoosterPack installed. We'll use 5V to power the DACs and ADCs in both situations.

 

image P1 and P2 on the bottom of the DAC/ADC BoosterPack have to be open. Else you'll inject 5V onto the LaunchPad 3V3 rail and you'll damage components.

 

It's not critical if you switch on the power supply before or after you connect the LaunchPad to your computer. The circuits are isolated.

All measurements use P3.10 as GND reference and P3.1 as reference voltage.

 

image

 

Setup without the power driver BoosterPack:

Mount the DAC/ADC BoosterPack on the LaunchPad.

Use a +5V power supply. It should be a decent one, current is approximately 5 mA.

Connect image with DAC/ADC BoosterPack P4.2  and image with P4.1.

 

Setup with the power driver BoosterPack:

Mount the DAC/ADC BoosterPack on the LaunchPad and the Power Driver BoosterPack on top of that.

On the Power Driver BoosterPack, bridge pins P2.4, P2.5 and P2.6 to tie both opamp inputs of opamp 3D to ground.

Use a +12V power supply. It should be a decent one, current is approximately 50 mA.

Connect image  with Power Driver BoosterPack P1.1 image  and with P1.2.

 

image

 

Measurements

 

In the table, the first column shows what we're measuring, the second column the SCPI command to execute with Peter's GUI.

The next columns are the measurements for Peter, Jon or Jan with and without the Power Driver BoosterPack.

The last column is for comments. We can indicate odds, errors, learnings.

 

JonPeterJan
Data PointSCPIWithoutWithWithoutWithWithoutWithMeasurement method
SupplyN/A4.989 V11.88 VDMM
DAC/ADC V+N/A4.989 V5.035 VDMM
VREFN/A2.046 V2.046 VDMM
ADC A GNDDEVE:ADC1?2SCPI output
ADC A VREFDEVE:ADC1?10918SCPI output
ADC ADEVE:ADC1?1138SCPI output
ADC B GNDDEVE:ADC2?12SCPI output
ADC B VREFDEVE:ADC2?10920SCPI output
ADC BDEVE:ADC2?1
SCPI output
ADC C GNDDEVE:ADC3?22SCPI output
ADC C VREFDEVE:ADC3?1092010919SCPI output
ADC CDEVE:ADC3?26868SCPI output
ADC D GNDDEVE:ADC4?83SCPI output
ADC D VREFDEVE:ADC4?1091910919SCPI output
DAC A 0DEVE:DAC1 00.000 V0.001 VDMM
DAC A maxDEVE:DAC1 655352.040 V2.040 VDMM
DAC B 0DEVE:DAC2 00.005 V0.005 VDMM
DAC B maxDEVE:DAC2 655352.046 V2.046 VDMM
DAC C 0DEVE:DAC3 00.000 V0.000 VDMM
DAC C maxDEVE:DAC3 655352.039 V V2.039 VDMM
DAC D 0DEVE:DAC4 00.000 V0.000 VDMM
DAC D maxDEVE:DAC4 655352.039 V2.039 VDMM

 

 

To resolve

With the power driver installed, ADC C and D act strange (probably also A and B, but I didn't inject a voltage in them because they are connected to opamp pins).

In particular strange for ADC D, because that one isn't routed. Strange.

I will try to decrease the frequency of the sample speed and the i²c speed to see if it's related to that ...

 

Follow up: the cause is that OPAMP 3C injects -0.8V into ADC A. All measurements are off when that happens. As soon as I force ADC A positive (by tying it to ground or a positive voltage) all measurements are correct.

 

image

 

We have a separate document to analyse the summing node at zero.

  • metrology
  • boosterpack
  • msp432
  • ti-rtos
  • launchpad
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +3
    Hi Jan, I was wondering, what are the expected values, is it reading a value representing 1.602V when it should read a value representing 2.048V? I'm wondering if it could be due to conversion time (i…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz +3
    yes, Shabaz, I have a controlled value of 2.040 V. Once I mount my additional driver board (self-designed so many things can be wrong ) the ADC says it’s 1.6 V. I checked signals with my scope to see if…
  • jc2048
    jc2048 over 6 years ago in reply to Andrew J +3
    Andrew J , have you read the blog I did when building Jan and Peter's load? That has some material on the low end of the DAC. Long story short, I adapted the analogue stuff after the DAC so the output…
Parents
  • Andrew J
    Andrew J over 6 years ago

    Test data results.  I've only measured the first 30 input codes in the graph but I will do more.  Having added the DC/DC Isolated converter to power Side A of the i2c and digital isolators (the Arduino input side) it has impacted the DAC output quite a lot, even though that is powered from a REF5040 (4.096) supply which I have measured at 4.096V.  That is used as the reference point for generating the DAC output.  My first conclusion is that noise is getting on to Side B ground from the DC/DC convertor although that is powered from a regulated 12V supply.

     

    I need to have a look at that but this is all on a breadboard right now so I'm only looking at (a) making sure my circuit works; and (b) working out an approach for tuning the DAC and ADC readings so that I can do it for real once I have a PCB.

     

    Nonetheless, I'm showing here an Ideal, Actual and Compensated DAC output with the derivation for the compensation calculation.  It's looking a lot more linear than I first thought and it has the same look as the graphs Jan and Jon produced!  It's also worth mentioning that the readings fluctuated by +/- 500uV around the value captured (e.g. at 0x000 input, I was reading anything from 0.0203 to 0.01998) but what I logged was the most stable - i.e. the reading that stayed steady the longest:

     

    EDIT: I've just noticed that the DAC input code runs from 1 to 31 - I should have edited these labels to read 0 to 30 so please read it on that basis.

     

    image

    image

     

    I don't intend to post more updates here unless Jan requests it as this is only related to the extent it's about DAC output.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Andrew J
    Andrew J over 6 years ago

    Test data results.  I've only measured the first 30 input codes in the graph but I will do more.  Having added the DC/DC Isolated converter to power Side A of the i2c and digital isolators (the Arduino input side) it has impacted the DAC output quite a lot, even though that is powered from a REF5040 (4.096) supply which I have measured at 4.096V.  That is used as the reference point for generating the DAC output.  My first conclusion is that noise is getting on to Side B ground from the DC/DC convertor although that is powered from a regulated 12V supply.

     

    I need to have a look at that but this is all on a breadboard right now so I'm only looking at (a) making sure my circuit works; and (b) working out an approach for tuning the DAC and ADC readings so that I can do it for real once I have a PCB.

     

    Nonetheless, I'm showing here an Ideal, Actual and Compensated DAC output with the derivation for the compensation calculation.  It's looking a lot more linear than I first thought and it has the same look as the graphs Jan and Jon produced!  It's also worth mentioning that the readings fluctuated by +/- 500uV around the value captured (e.g. at 0x000 input, I was reading anything from 0.0203 to 0.01998) but what I logged was the most stable - i.e. the reading that stayed steady the longest:

     

    EDIT: I've just noticed that the DAC input code runs from 1 to 31 - I should have edited these labels to read 0 to 30 so please read it on that basis.

     

    image

    image

     

    I don't intend to post more updates here unless Jan requests it as this is only related to the extent it's about DAC output.