1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Envidrawer 5 - Piping and pumping - water and liquid fertiliser delivery system
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
  • Author Author: jduchniewicz
  • Date Created: 29 Dec 2020 4:41 PM Date Created
  • Views 827 views
  • Likes 4 likes
  • Comments 1 comment
  • 1meterofpi
  • raspberrypi4
  • pimoroni
  • 1 meter of pi
  • envidrawer
  • urban farming
  • climate crisis
  • farming
  • smart farming
Related
Recommended

Envidrawer 5 - Piping and pumping - water and liquid fertiliser delivery system

jduchniewicz
jduchniewicz
29 Dec 2020

Previous blogs

Description

#1 - Introduction, the plan and materials preparationIn this blog post we describe the project's main concept and some initial high-level design of it.
#2 - Materials and casing assembly

Our journey with selecting proper materials, cutting and assembling the drawer and its casing!

#3 - Modelling, cutting, planting!The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables!
#4 - Plants, harvests, and fertilisersFirst harvest, problems with plants and used fertilisers. All that went off-script for our plants in the artificial environment.



Next blogsDescription
#6 - Mix of fixesFinal touches to water supply system and small redesigns/fixes.
#7 - Ride the lightning - Wiring diagram, pinout and components discussionDiagram of the circuit, pinout for most components, wire choices and their connections
#8 - Pulling the stringsLED and Fan control circuit, overview of BJTs and MOSFETs with a handful of useful general information

#9 - 3D printing

Detailed description of 3D printed components, their presentation and some tips
#10 - Software, architecture and the benefits of good preparationBig explanation of the software and its architecture
#11 - SummaryOur final post before the end of the challenge!

      • Intro
      • Tubing
      • Water container and pump
      • Gross structure
      • Water calculations
      • Summary

Intro

Our water supply system was based upon simple plant watering mechanism adapted for enclosed space design. It is fitted with additional features that can be regulated, most importantly the 5V aquarium pump which enables us to automate the process. Water will have to be refilled manually, but we plan on having a large container holding enough for several watering cycles. Each bout of water can be fitted with any water soluble/liquid fertiliser.

 

This post consists of:

  • Tubing
  • Water container and pump
  • Gross structure
  • Water calculations

 

Tubing

The main tube is 16 mm in diameter and 140 cm in length. This comes to around 1.2 liters in volume. There are 18 drippers in total attached in pairs every 13.3 cm, that give off 2 liters of water per hour each. A short (10 cm) piece of 3mm tubing is attached to each dripper and ran horizontally in the ground.

image

Picture 1: Piece of the main tube with its terminal seal and 4 last branching out 3mm tubes at the end

 

Each one of these tubes was pierced 20 times with a thick needle and the end was sealed using hot glue.

imageimage

Picture 2&3: Seal at the end of the 3mm black tubes and wide holes in the tube

 

This allows us for slow and even distribution of water across the Envidrawer.

 

Water container and pump

The water container is printed to a dimension of 20x20x10 cm. It can hold 4 liters, enough to fill up the tubes required 1.2 liters and for additional 2.8 liters - enough for at least 2 watering cycles. The drippers are all placed on the bottom half of the main pipe, making sure there is as little as possible water left after watering the plants. Any stale liquid would soon start to smell foul and with potentially added fertilisers grow bacterial colonies.

 

The container is being designed and printed at the moment. It is supposed to fit inside the tight space of Envidrawer and accommodate electronics thus it cannot be installed right away. Inside, a 5V submersible water pump will be installed. We will need to isolate the pump cable from the water container - it will be left out of the submersed part and encased separately to prevent accidental water leaks and spillage.

 

Water pump and tubing attachment is designed using original parts of the water supply system as well as custom seals and 3D printed components.

imageimage

Picture 4&5: Model of water connection and described elements of the system including the hole puncher for dripper montage

 

Gross structure

The main tube is attached to the bottom of the Envidrawer by printed and screwed on clamps. The tube is sealed at the end, and it will almost empty after watering the plants. The water container is placed at the end of the drawer, where the tube will be lead at an angle to be supplied by the water pump.

 

Water calculations

1.2 liters of water is needed to fill the pipe, however, less than that is required to start the watering process as drippers are on the lower half. To fill the pipe, we need to calculate how much water escapes the pipe per minute and how much our pump is capable of supplying. It can give off 80 liters per hour (1.3 liters per minute). It is important to maintain the tube's water levels at 70% to ensure all drippers provide water at equal flow rates. We can match the filling of the tube by the pump with the rate of emptying (0.6 l per minute - 18 2l/h drippers => 36 l/h - 0.6 l/min)  by cranking down the current on the pump and slowing down the water flow.

 

To provide 1.2 liters of water we need to fill our pipe once or keep it filled for 2 minutes. To approximate this value we should first fill it up to half of its volume and keep the pump running for an additional volume. Of course, all of this will be tested out as we near the completion of our project.

 

Summary

Overall, the setup is ready to be filled with water and soak our 30 liters of soil for the next plant growth. The setup is simple enough, but any problems will come out during testing and programming so we will need to address them accordingly. We aim at finishing the main design before 31.12 and then, only software will hold us back image

Michał & Jakub & Szymon

 

Previous postNext post
#4 - Plants, harvests, and fertilisers#6 - Mix of fixes
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +1
    Nice update. It will be interesting to see how well you can distribute the water evenly. DAB
Parents
  • DAB
    DAB over 5 years ago

    Nice update.

     

    It will be interesting to see how well you can distribute the water evenly.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Nice update.

     

    It will be interesting to see how well you can distribute the water evenly.

     

    DAB